CANFD Rx Buffer used in DMA mode.
This structure defines the Rx buffer format used in DMA mode. This matches with the Rx Buffer format in message ram. The Dma will be configured to read the full Rx buffer with header from message ram.
Data Fields | |
uint32_t | header1 |
uint32_t | header2 |
uint8_t | data [64] |
uint32_t CANFDLLD_DmaRxBuf::header1 |
uint32_t CANFDLLD_DmaRxBuf::header2 |
uint8_t CANFDLLD_DmaRxBuf::data[64] |