CANFD DMA message configuration used for Tx.
Data Fields | |
uint32_t | dataLengthPerMsg |
data length in Bytes for every message. More... | |
uint32_t | numMsgs |
Number of messages. More... | |
const void * | data |
pointer to the data buffer. This should a 2d array of uint8[numMsgs][dataLengthPerMsg] More... | |
uint32_t | currentMsgNum |
Used by driver to store current message count out of the numMsgs already processed. More... | |
uint32_t CANFDLLD_DmaMsgConfig::dataLengthPerMsg |
data length in Bytes for every message.
uint32_t CANFDLLD_DmaMsgConfig::numMsgs |
Number of messages.
const void* CANFDLLD_DmaMsgConfig::data |
pointer to the data buffer. This should a 2d array of uint8[numMsgs][dataLengthPerMsg]
uint32_t CANFDLLD_DmaMsgConfig::currentMsgNum |
Used by driver to store current message count out of the numMsgs already processed.