xWRL6432 MMWAVE-L-SDK  05.04.00.01

Detailed Description

Region config structure, this is used by SysConfig and not to be used by end-users directly.

Data Fields

uint64_t systemAddr
 
uint32_t localAddr
 
uint32_t size
 

Field Documentation

◆ systemAddr

uint64_t AddrTranslateP_RegionConfig::systemAddr

translated 48b system addr as seen by the SOC, MUST align to region size

◆ localAddr

uint32_t AddrTranslateP_RegionConfig::localAddr

region start address as seen by the CPU, MUST align to region size

◆ size

uint32_t AddrTranslateP_RegionConfig::size

region size, see AddrTranslateP_RegionSize