This module contains APIs to program and use DMA drivers available in the SoC with MCSPI.
|
MCSPI_DmaHandle | MCSPI_dmaOpen (int32_t index) |
| API to open an MCSPI DMA channel. More...
|
|
int32_t | MCSPI_dmaClose (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg) |
| API to close an MCSPI DMA channel. More...
|
|
int32_t | MCSPI_dmaChInit (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg) |
| API to init a DMA Channel opened. More...
|
|
int32_t | MCSPI_dmaTransfer (MCSPI_Object *obj, MCSPI_ChObject *chObj, const MCSPI_Attrs *attrs, MCSPI_Transaction *transaction) |
| API to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc. More...
|
|
int32_t | MCSPI_dmaStop (MCSPI_Object *obj, const MCSPI_Attrs *attrs, MCSPI_ChObject *chObj, uint32_t chNum) |
| API to Stop DMA using a specific DMA driver - UDMA, EDMA etc. More...
|
|
|
typedef void * | MCSPI_DmaHandle |
| Handle to the MCSPI DMA Config Object returned by MCSPI_dmaOpen. More...
|
|
typedef int32_t(* | MCSPI_dmaOpenFxn) (void *mcspiDmaArgs) |
| Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc. More...
|
|
typedef int32_t(* | MCSPI_dmaCloseFxn) (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg) |
| Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc. More...
|
|
typedef int32_t(* | MCSPI_dmaChInitFxn) (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg) |
| Driver implementation to init a DMA channel params using a specific DMA driver - UDMA, EDMA etc. More...
|
|
typedef int32_t(* | MCSPI_dmaTransferControllerFxn) (MCSPI_Object *obj, MCSPI_ChObject *chObj, const MCSPI_Attrs *attrs, MCSPI_Transaction *transaction) |
| Driver implementation to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc. More...
|
|
typedef int32_t(* | MCSPI_dmaStopFxn) (MCSPI_Object *obj, const MCSPI_Attrs *attrs, MCSPI_ChObject *chObj, uint32_t chNum) |
| Driver implementation to Stop DMA using a specific DMA driver - UDMA, EDMA etc. More...
|
|
◆ MCSPI_DmaHandle
◆ MCSPI_dmaOpenFxn
typedef int32_t(* MCSPI_dmaOpenFxn) (void *mcspiDmaArgs) |
Driver implementation to open a specific DMA driver channel - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
mcspiDmaArgs | [in] DMA specific arguments, obtained from the config |
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaCloseFxn
Driver implementation to close a specific DMA driver channel - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
MCSPI_DmaHandle | [in] MCSPI DMA Object handle returned from MCSPI_dmaOpen |
mcspiDmaArgs | [in] DMA specific arguments, obtained from the config |
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaChInitFxn
Driver implementation to init a DMA channel params using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaTransferControllerFxn
Driver implementation to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
obj | [in] Pointer to MCSPI object |
chObj | [in] Pointer to MCSPI_ChObject. This parameter can't be NULL |
attrs | [in] Pointer to MCSPI_Attrs. This parameter can't be NULL |
transaction | [in] Pointer to MCSPI_Transaction. This parameter can't be NULL |
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaStopFxn
Driver implementation to Stop DMA using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
obj | [in] Pointer to MCSPI object |
attrs | [in] Pointer to MCSPI_Attrs. This parameter can't be NULL |
chObj | [in] Pointer to MCSPI_ChObject. This parameter can't be NULL |
chNum | [in] Channel number |
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaOpen()
API to open an MCSPI DMA channel.
This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig
- Parameters
-
index | [in] Index of the DMA Config selected for this particular MCSPI driver instance |
- Returns
- Handle to the MCSPI DMA Config Object
◆ MCSPI_dmaClose()
API to close an MCSPI DMA channel.
This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig
- Parameters
-
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaChInit()
API to init a DMA Channel opened.
This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig
- Parameters
-
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaTransfer()
API to do a DMA transfer using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
obj | [in] Pointer to MCSPI object |
chObj | [in] Pointer to MCSPI_ChObject. This parameter can't be NULL |
attrs | [in] Pointer to MCSPI_Attrs. This parameter can't be NULL |
transaction | [in] Pointer to MCSPI_Transaction. This parameter can't be NULL |
- Returns
- SystemP_SUCCESS on success, else failure
◆ MCSPI_dmaStop()
API to Stop DMA using a specific DMA driver - UDMA, EDMA etc.
Typically this callback is hidden from the end application and is implemented when a new DMA driver needs to be supported.
- Parameters
-
obj | [in] Pointer to MCSPI object |
attrs | [in] Pointer to MCSPI_Attrs. This parameter can't be NULL |
chObj | [in] Pointer to MCSPI_ChObject. This parameter can't be NULL |
chNum | [in] Channel number |
- Returns
- SystemP_SUCCESS on success, else failure
◆ gMcspiDmaEdmaFxns