This module contains APIs to program and use the pinmux module.
◆ POWER_DISALLOW_LPDS
#define POWER_DISALLOW_LPDS 0 |
Constraint: Disallow entry to Low Power Deep Sleep (LPDS)
◆ POWER_DISALLOW_SLEEP
#define POWER_DISALLOW_SLEEP 1 |
Constraint: Disallow entry to Sleep
◆ POWER_DISALLOW_IDLE
#define POWER_DISALLOW_IDLE 2 |
Constraint: Disallow entry to Idle
◆ POWER_ENTERING_LPDS
#define POWER_ENTERING_LPDS 0x1 |
Power event: The device is entering the LPDS sleep state
◆ POWER_ENTERING_SLEEP
#define POWER_ENTERING_SLEEP 0x2 |
Power event: The device is entering the device sleep state
◆ POWER_ENTERING_IDLE
#define POWER_ENTERING_IDLE 0x4 |
Power event: The device is entering the idle state
◆ POWER_AWAKE_LPDS
#define POWER_AWAKE_LPDS 0x8 |
Power event: The device is waking from the LPDS sleep state
◆ POWER_AWAKE_SLEEP
#define POWER_AWAKE_SLEEP 0x10 |
Power event: The device is waking from the device sleep state
◆ POWER_AWAKE_IDLE
#define POWER_AWAKE_IDLE 0x20 |
Power event: The device is waking from the device idle state
◆ Power_GPIO_SYNCIO_Wakeup_Enable
Source of Wake-up can be either GPIO (WU_REQIN) or SYNC_IN.
Enumerator |
---|
POWER_GPIO_WAKEUP_LPDS | |
POWER_SYNCIN_IO_WAKEUP_LPDS | |
◆ Power_ParkState
Enumeration of states a pin can be parked in.
Enumerator |
---|
POWER_PARK | No pull resistor, leave pin in a HIZ state
|
POWER_DONT_PARK | Take no action; do not park the pin
|
◆ Power_configureWakeup()
Function configures wakeup for LPDS and shutdown.
This function allows the app to configure the type for waking up from LPDS This overwrites any previous wakeup settings.
- Parameters
-
[in] | wakeup | Settings applied to wakeup configuration |
◆ Power_initPolicy()
void Power_initPolicy |
( |
void |
| ) |
|
OS-specific power policy initialization function
◆ Power_getWakeup()
Function to get wakeup configuration settings.
This function allows an app to query the current LPDS and shutdown wakeup configuration settings.
- Parameters
-
◆ Power_sleepPolicy()
void Power_sleepPolicy |
( |
unsigned long long |
sleepTimeus | ) |
|
A reference power policy is provided which can transition the MCU from the active state to one of two sleep states: Low-Power Deep Sleep (LPDS) or Idle state. (Sleep will be supported in future releases)
The policy looks at the estimated idle time remaining, and the active constraints, and determine which sleep state to transition to. The policy will give first preference to choosing LPDS, but if that is not appropriate (e.g., not enough time), it will choose Idle.
◆ Power_Idle3()
Device Idle mode.
This function brings the device to Idle3 mode. Idle3 is TI defined idle state where,
- All Peripherals are clock gated
- HWA and Frontend are powered Down
- Core is kept in Deep Sleep State
- TOPSS is driven by OSC/16 clock
- Core is brought out of deep sleep using RTI timer interrupt (mapped to WIC)