Macros | |
#define | DPU_CFARPROCHWA_DET_MATRIX_BYTE_ALIGNMENT (sizeof(uint16_t)) |
Alignment for memory allocation purpose of detection matrix. There is CPU access of detection matrix in the implementation. More... | |
#define | DPU_CFARPROCHWA_CFAR_DET_LIST_BYTE_ALIGNMENT DPIF_CFAR_DET_LIST_CPU_BYTE_ALIGNMENT |
Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation. More... | |
#define | DPU_CFARPROCHWA_HWA_MEM_OUT_DOPPLER_BYTE_ALIGNMENT (sizeof(uint32_t)) |
Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation. This is the maximum field size of the DPU_CFARProcHWA_CfarDetOutput structure. More... | |
#define | DPU_CFARPROCHWA_HWA_MEM_OUT_RANGE_BYTE_ALIGNMENT (sizeof(uint32_t)) |
Alignment for memory allocation purpose. There is CPU access of thi buffers in the implementation. This is the maximum field size of the DPU_CFARProcHWA_CfarDetOutput structure. More... | |
#define | DPU_CFARPROCHWA_DOPPLER_DET_OUT_BIT_MASK_BYTE_ALIGNMENT (sizeof(uint32_t)) |
Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation. More... | |
#define DPU_CFARPROCHWA_DET_MATRIX_BYTE_ALIGNMENT (sizeof(uint16_t)) |
Alignment for memory allocation purpose of detection matrix. There is CPU access of detection matrix in the implementation.
#define DPU_CFARPROCHWA_CFAR_DET_LIST_BYTE_ALIGNMENT DPIF_CFAR_DET_LIST_CPU_BYTE_ALIGNMENT |
Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation.
#define DPU_CFARPROCHWA_HWA_MEM_OUT_DOPPLER_BYTE_ALIGNMENT (sizeof(uint32_t)) |
Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation. This is the maximum field size of the DPU_CFARProcHWA_CfarDetOutput structure.
#define DPU_CFARPROCHWA_HWA_MEM_OUT_RANGE_BYTE_ALIGNMENT (sizeof(uint32_t)) |
Alignment for memory allocation purpose. There is CPU access of thi buffers in the implementation. This is the maximum field size of the DPU_CFARProcHWA_CfarDetOutput structure.
#define DPU_CFARPROCHWA_DOPPLER_DET_OUT_BIT_MASK_BYTE_ALIGNMENT (sizeof(uint32_t)) |
Alignment for memory allocation purpose. There is CPU access of this buffer in the implementation.