Go to the source code of this file.
Data Structures | |
struct | SemaphoreP_Object |
Opaque semaphore object used with the semaphore APIs. More... | |
struct | SemaphoreP_Params |
Parameters passed during SemaphoreP_construct. More... | |
Macros | |
#define | SemaphoreP_OBJECT_SIZE_MAX (96u) |
Max size of semaphore object across no-RTOS and all OS's. More... | |
Enumerations | |
enum | SemaphoreP_Type { SemaphoreP_TYPE_BINARY, SemaphoreP_TYPE_COUNTING, SemaphoreP_TYPE_MUTEX } |
Semaphore type. More... | |
Functions | |
int32_t | SemaphoreP_constructMutex (SemaphoreP_Object *obj) |
Create a mutex semaphore object. More... | |
void | SemaphoreP_Params_init (SemaphoreP_Params *params) |
Set default values to SemaphoreP_Params. More... | |
int32_t | SemaphoreP_constructBinary (SemaphoreP_Object *obj, uint32_t initValue) |
Create a binary semaphore object. More... | |
int32_t | SemaphoreP_construct (SemaphoreP_Object *obj, SemaphoreP_Params *params) |
Create a semaphore object. More... | |
int32_t | SemaphoreP_constructCounting (SemaphoreP_Object *obj, uint32_t initValue, uint32_t maxValue) |
Create a counting semaphore object. More... | |
void | SemaphoreP_destruct (SemaphoreP_Object *obj) |
Cleanup, delete, destruct a semaphore object. More... | |
void | SemaphoreP_post (SemaphoreP_Object *obj) |
Post a semaphore object or unlock a mutex. More... | |
int32_t | SemaphoreP_pend (SemaphoreP_Object *obj, uint32_t timeToWaitInTicks) |
Pend on a semaphore object or lock a mutex. More... | |