xWRL1432 MMWAVE-L-SDK  05.03.00
DPU_AoAProc_stats Struct Reference

Detailed Description

Data processing Unit statistics.

The structure is used to hold the statistics of the DPU

Data Fields

uint32_t processingTime
 total processing time during all range gates in a frame excluding EDMA waiting time More...
 
uint32_t waitTime
 total wait time for EDMA data transfer during all range gates More...
 

Field Documentation

◆ processingTime

uint32_t DPU_AoAProc_stats::processingTime

total processing time during all range gates in a frame excluding EDMA waiting time

◆ waitTime

uint32_t DPU_AoAProc_stats::waitTime

total wait time for EDMA data transfer during all range gates