xWRL1432 MMWAVE-L-SDK  05.03.00
DPEDMA_ChanCfg Struct Reference

Detailed Description

EDMA channel configuration.

The structure is used to hold the EDMA channel configuration

Data Fields

uint32_t channel
 EDMA channel id. More...
 
uint32_t paramId
 EDMA ParamSet triggered by event on channel. More...
 
uint16_t channelShadow
 EDMA channel shadow id. More...
 
uint32_t shadowPramId
 EDMA shadow ParamSet id. More...
 
uint32_t eventQueue
 EDMA event Queue used for the transfer. More...
 
uint32_t tcc
 EDMA event Queue used for the transfer. More...
 

Field Documentation

◆ channel

uint32_t DPEDMA_ChanCfg::channel

EDMA channel id.

◆ paramId

uint32_t DPEDMA_ChanCfg::paramId

EDMA ParamSet triggered by event on channel.

◆ channelShadow

uint16_t DPEDMA_ChanCfg::channelShadow

EDMA channel shadow id.

◆ shadowPramId

uint32_t DPEDMA_ChanCfg::shadowPramId

EDMA shadow ParamSet id.

◆ eventQueue

uint32_t DPEDMA_ChanCfg::eventQueue

EDMA event Queue used for the transfer.

◆ tcc

uint32_t DPEDMA_ChanCfg::tcc

EDMA event Queue used for the transfer.