xWRL1432 MMWAVE-L-SDK  05.03.00
DPEDMA_3LinkChanCfg Struct Reference

Detailed Description

EDMA channel configuration with 3 shadow channels.

The structure is used to hold the EDMA channel configuration for 1 EDMA channel which is linked to 3 shadow channels.

Data Fields

uint32_t channel
 EDMA channel id. More...
 
uint32_t paramId
 EDMA ParamSet triggered by event on channel. More...
 
uint32_t ShadowPramId [3]
 EDMA channel shadow id. More...
 
uint32_t eventQueue
 EDMA event Queue used for the transfer. More...
 
uint32_t tcc
 EDMA event Queue used for the transfer. More...
 

Field Documentation

◆ channel

uint32_t DPEDMA_3LinkChanCfg::channel

EDMA channel id.

◆ paramId

uint32_t DPEDMA_3LinkChanCfg::paramId

EDMA ParamSet triggered by event on channel.

◆ ShadowPramId

uint32_t DPEDMA_3LinkChanCfg::ShadowPramId[3]

EDMA channel shadow id.

◆ eventQueue

uint32_t DPEDMA_3LinkChanCfg::eventQueue

EDMA event Queue used for the transfer.

◆ tcc

uint32_t DPEDMA_3LinkChanCfg::tcc

EDMA event Queue used for the transfer.