xWRL1432 MMWAVE-L-SDK  05.03.00
DPEDMA_2LinkChanCfg Struct Reference

Detailed Description

EDMA channel configuration with 2 shadow channels.

The structure is used to hold the EDMA channel configuration for 1 EDMA channel which is linked to 2 shadow channels.

Data Fields

uint8_t channel
 EDMA channel id. More...
 
uint16_t channelShadow [2]
 EDMA channel shadow id. More...
 
uint8_t eventQueue
 EDMA event Queue used for the transfer. More...
 

Field Documentation

◆ channel

uint8_t DPEDMA_2LinkChanCfg::channel

EDMA channel id.

◆ channelShadow

uint16_t DPEDMA_2LinkChanCfg::channelShadow[2]

EDMA channel shadow id.

◆ eventQueue

uint8_t DPEDMA_2LinkChanCfg::eventQueue

EDMA event Queue used for the transfer.