xWRL1432 MMWAVE-L-SDK  05.03.00
CANFDLLD_MCANProtocolStatus Struct Reference

Detailed Description

Data structure defines the MCAN protocol status.

Data Fields

uint32_t lastErrCode
 
uint32_t act
 
uint32_t errPassive
 
uint32_t warningStatus
 
uint32_t busOffStatus
 
uint32_t dlec
 
uint32_t resi
 
uint32_t rbrs
 
uint32_t rfdf
 
uint32_t pxe
 
uint32_t tdcv
 

Field Documentation

◆ lastErrCode

uint32_t CANFDLLD_MCANProtocolStatus::lastErrCode

Last Error Code Refer enum CANFDLLD_MCANErrCode

◆ act

uint32_t CANFDLLD_MCANProtocolStatus::act

Activity - Monitors the module's CAN communication state. refer enum CANFDLLD_MCANCommState

◆ errPassive

uint32_t CANFDLLD_MCANProtocolStatus::errPassive

Error Passive 0 = The M_CAN is in the Error_Active state 1 = The M_CAN is in the Error_Passive state

◆ warningStatus

uint32_t CANFDLLD_MCANProtocolStatus::warningStatus

Warning Status 0 = Both error counters are below the Error_Warning limit of 96 1 = At least one of error counter has reached the Error_Warning limit of 96

◆ busOffStatus

uint32_t CANFDLLD_MCANProtocolStatus::busOffStatus

Bus_Off Status 0 = The M_CAN is not Bus_Off 1 = The M_CAN is in Bus_Off state

◆ dlec

uint32_t CANFDLLD_MCANProtocolStatus::dlec

Data Phase Last Error Code Refer enum CANFDLLD_MCANErrCode

◆ resi

uint32_t CANFDLLD_MCANProtocolStatus::resi

ESI flag of last received CAN FD Message 0 = Last received CAN FD message did not have its ESI flag set 1 = Last received CAN FD message had its ESI flag set

◆ rbrs

uint32_t CANFDLLD_MCANProtocolStatus::rbrs

BRS flag of last received CAN FD Message 0 = Last received CAN FD message did not have its BRS flag set 1 = TLast received CAN FD message had its BRS flag set

◆ rfdf

uint32_t CANFDLLD_MCANProtocolStatus::rfdf

Received a CAN FD Message 0 = Since this bit was reset by the CPU, no CAN FD message has been received 1 = Message in CAN FD format with FDF flag set has been received

◆ pxe

uint32_t CANFDLLD_MCANProtocolStatus::pxe

Protocol Exception Event 0 = No protocol exception event occurred since last read access 1 = Protocol exception event occurred

◆ tdcv

uint32_t CANFDLLD_MCANProtocolStatus::tdcv

Transmitter Delay Compensation Value