Go to the source code of this file.
Macros | |
SOC Domain ID | |
#define | SOC_DOMAIN_ID_TOPSS_CTRL (0U) |
#define | SOC_DOMAIN_ID_APP_RCM (1U) |
#define | SOC_DOMAIN_ID_APP_CTRL (2U) |
#define | SOC_DOMAIN_ID_TOP_IO_MUX (3U) |
#define | SOC_DOMAIN_ID_TOP_PRCM (4U) |
Enumerations | |
enum | SOC_SysRstReason { SOC_SYS_RESET_REASON_PORZ = 0x01U, SOC_SYS_RESET_REASON_SR = 0x02U, SOC_SYS_RESET_REASON_WDG = 0x04U } |
SOC System Reset Reason. More... | |
enum | SOC_RstReason { SOC_RESET_REASON_PORZ = 0x01U, SOC_RESET_REASON_WARM, SOC_RESET_REASON_DEEPSLEEP, SOC_RESET_REASON_SOFT, SOC_RESET_REASON_STC_WARM, SOC_RESET_REASON_STC_PORZ } |
SOC Reset Reason. More... | |
Functions | |
int32_t | SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable) |
Enable clock to specified module. More... | |
int32_t | SOC_clocksEnable (void) |
Enables ADPLL. More... | |
int32_t | SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate) |
Set module clock to specified frequency. More... | |
const char * | SOC_getCoreName (uint16_t coreId) |
Convert a core ID to a user readable name. More... | |
void | SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition) |
Lock control module partition to prevent writes into control MMRs. More... | |
void | SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition) |
Unlock control module partition to allow writes into control MMRs. More... | |
void | SOC_logAllClockHz (void) |
Print's module clock info to the console. More... | |
uint64_t | SOC_virtToPhy (void *virtAddr) |
SOC Virtual (CPU) to Physical address translation function. More... | |
void | SOC_memoryInit (void) |
Initializes APPSS shared RAM0, RAM1 and HWASS Shared RAM. More... | |
void | SOC_enableMDLLClock (void) |
Enables MDLL Clock. More... | |
void | SOC_triggerWarmReset (void) |
Software Warm reset request. Generates warm reset for entire device. More... | |
void | SOC_triggerSoftReset (void) |
Soft reset request. More... | |
SOC_RstReason | SOC_getRstReason (void) |
Retrieves the reset reason. More... | |
SOC_SysRstReason | SOC_getSysRstReason (void) |
Retrieves the system reset reason from SYS_RST_CAUSE. All the reset registers will be cleared by the bootloader. The reset register values will be stored in BOOT_INFO_REG0[23:0] The TOP_PRCM:SYS_RST_CAUSE[2:0] is stored in APP_CTRL:APPSS_BOOT_INFO_REG0[7:4]. More... | |
void | SOC_setEpwmTbClk (uint32_t enable) |
Enable or disable ePWM time base clock from Control MMR. More... | |