For more details and example usage, see Event
|
int32_t | EventP_construct (EventP_Object *obj) |
| Create an Event object. More...
|
|
void | EventP_destruct (EventP_Object *obj) |
| Cleanup, delete, destruct an Event object. More...
|
|
int32_t | EventP_waitBits (EventP_Object *obj, uint32_t bitsToWaitFor, uint8_t clearOnExit, uint8_t waitForAll, uint32_t timeToWaitInTicks, uint32_t *eventBits) |
| Read the Event bits, after optionally waiting for a bit or multiple bits to be set. More...
|
|
int32_t | EventP_setBits (EventP_Object *obj, uint32_t bitsToSet) |
| Setting a bit or multiple bits in the Event bits. More...
|
|
int32_t | EventP_clearBits (EventP_Object *obj, uint32_t bitsToClear) |
| Clear a bit or multiple bits in the Event bits. More...
|
|
int32_t | EventP_getBits (EventP_Object *obj, uint32_t *eventBits) |
| Getting the current value of Event bits. More...
|
|
◆ EventP_OBJECT_SIZE_MAX
#define EventP_OBJECT_SIZE_MAX (48u) |
Max size of Event object across no-RTOS and all OS's.
◆ EventP_construct()
◆ EventP_destruct()
Cleanup, delete, destruct an Event object.
- Parameters
-
◆ EventP_waitBits()
int32_t EventP_waitBits |
( |
EventP_Object * |
obj, |
|
|
uint32_t |
bitsToWaitFor, |
|
|
uint8_t |
clearOnExit, |
|
|
uint8_t |
waitForAll, |
|
|
uint32_t |
timeToWaitInTicks, |
|
|
uint32_t * |
eventBits |
|
) |
| |
Read the Event bits, after optionally waiting for a bit or multiple bits to be set.
- Parameters
-
obj | [in] Event object |
bitsToWaitFor | [in] Bitwise value indicating the bits to be tested |
clearOnExit | [in] If this parameter is 1, then any bits set in the value passed in bitsToWaitFor will be cleared before this API returns. If there is a time-out based on timeToWaitInTicks parameter, it will not be cleared.
If this parameter is 0, then none of the bits are altered. |
waitForAll | [in] This parameter is used to specify if the test of bits should be logical AND or logical OR.
If this parameter is 1, then this API will return when ALL the bits set in bitsToWaitFor are set in the Event bits, or if there is a time-out.
If this parameter is 0, then this API will return when ANY of the bits set in bitsToWaitFor is set in the Event bits, or if there is a time-out.
|
timeToWaitInTicks | [in] Amount of time to wait for one or all bits from bitsToWaitFor to be set, in units of system ticks (see Clock) |
eventBits | [out]Value of the Event bits when the bits being waited for were set, or the time-out occured. |
- Returns
- SystemP_SUCCESS on success or time-out
-
SystemP_FAILURE on failure.
- Note
- This function should not be called from an interrupt.
-
The actual current value of Event bits can be different from returned value if an interrupt or a higher priority task modifies the value between the calling task leaving blocked state and exiting this API.
◆ EventP_setBits()
int32_t EventP_setBits |
( |
EventP_Object * |
obj, |
|
|
uint32_t |
bitsToSet |
|
) |
| |
Setting a bit or multiple bits in the Event bits.
- Parameters
-
obj | [in] Event object |
bitsToSet | [in] Bitwise value indicating the bits to be set |
- Returns
- SystemP_SUCCESS on success
-
SystemP_FAILURE on failure
◆ EventP_clearBits()
int32_t EventP_clearBits |
( |
EventP_Object * |
obj, |
|
|
uint32_t |
bitsToClear |
|
) |
| |
Clear a bit or multiple bits in the Event bits.
- Parameters
-
obj | [in] Event object |
bitsToClear | [in] Bitwise value indicating the bits to be cleared |
- Returns
- SystemP_SUCCESS on success
-
SystemP_FAILURE on failure
◆ EventP_getBits()
int32_t EventP_getBits |
( |
EventP_Object * |
obj, |
|
|
uint32_t * |
eventBits |
|
) |
| |
Getting the current value of Event bits.
- Parameters
-
obj | [in] Event object |
eventBits | [out]Value of the Event bits when the bits being waited for were set, or the time-out occured. |
- Returns
- SystemP_SUCCESS on success.
-
SystemP_FAILURE on failure.
- Note
- The actual current value of Event bits can be different from returned value if an interrupt or a higher priority task modifies the value between the calling task leaving blocked state and exiting this API.