xWRL1432 MMWAVE-L-SDK  05.03.00

Introduction

Macros

#define ESM_EINVAL   (ESM_ERRNO_BASE-1)
 Error Code: Invalid argument
More...
 
#define ESM_ENOINIT   (ESM_ERRNO_BASE-2)
 Error Code: Operation cannot be done as ESM_open is not done. More...
 
#define ESM_EREINIT   (ESM_ERRNO_BASE-3)
 Error Code: Operation cannot be done as ESM_open is already done and re-init is not permitted. More...
 
#define ESM_ENOMEM   (ESM_ERRNO_BASE-4)
 Error Code: Out of memory. More...
 

Macro Definition Documentation

◆ ESM_EINVAL

#define ESM_EINVAL   (ESM_ERRNO_BASE-1)

Error Code: Invalid argument

◆ ESM_ENOINIT

#define ESM_ENOINIT   (ESM_ERRNO_BASE-2)

Error Code: Operation cannot be done as ESM_open is not done.

◆ ESM_EREINIT

#define ESM_EREINIT   (ESM_ERRNO_BASE-3)

Error Code: Operation cannot be done as ESM_open is already done and re-init is not permitted.

◆ ESM_ENOMEM

#define ESM_ENOMEM   (ESM_ERRNO_BASE-4)

Error Code: Out of memory.