Base error code for the zoomProc DPU is defined in the dp_error.h
Macros | |
#define | DPU_ZOOMPROC_EINVAL (DP_ERRNO_ZOOM_PROC_BASE-1) |
Error Code: Invalid argument. More... | |
#define | DPU_ZOOMPROC_ENOMEM (DP_ERRNO_ZOOM_PROC_BASE-2) |
Error Code: Out of memory. More... | |
#define | DPU_ZOOMPROC_EINTERNAL (DP_ERRNO_ZOOM_PROC_BASE-3) |
Error Code: Internal error. More... | |
#define | DPU_ZOOMPROC_ENOTIMPL (DP_ERRNO_ZOOM_PROC_BASE-4) |
Error Code: Not implemented. More... | |
#define | DPU_ZOOMPROC_EINPROGRESS (DP_ERRNO_ZOOM_PROC_BASE-5) |
Error Code: In Progress. More... | |
#define | DPU_ZOOMPROC_ECMD (DP_ERRNO_ZOOM_PROC_BASE-6) |
Error Code: Invalid control command. More... | |
#define | DPU_ZOOMPROC_ESEMA (DP_ERRNO_ZOOM_PROC_BASE-7) |
Error Code: Semaphore error. More... | |
#define DPU_ZOOMPROC_EINVAL (DP_ERRNO_ZOOM_PROC_BASE-1) |
Error Code: Invalid argument.
#define DPU_ZOOMPROC_ENOMEM (DP_ERRNO_ZOOM_PROC_BASE-2) |
Error Code: Out of memory.
#define DPU_ZOOMPROC_EINTERNAL (DP_ERRNO_ZOOM_PROC_BASE-3) |
Error Code: Internal error.
#define DPU_ZOOMPROC_ENOTIMPL (DP_ERRNO_ZOOM_PROC_BASE-4) |
Error Code: Not implemented.
#define DPU_ZOOMPROC_EINPROGRESS (DP_ERRNO_ZOOM_PROC_BASE-5) |
Error Code: In Progress.
#define DPU_ZOOMPROC_ECMD (DP_ERRNO_ZOOM_PROC_BASE-6) |
Error Code: Invalid control command.
#define DPU_ZOOMPROC_ESEMA (DP_ERRNO_ZOOM_PROC_BASE-7) |
Error Code: Semaphore error.