Base error code for the dopplerProc DPU is defined in the
#define DPU_DOPPLERPROCHWA_EINVAL (DP_ERRNO_DOPPLER_PROC_BASE-1) |
Error Code: Invalid argument.
#define DPU_DOPPLERPROCHWA_ENOMEM (DP_ERRNO_DOPPLER_PROC_BASE-2) |
Error Code: Out of memory.
#define DPU_DOPPLERPROCHWA_EINPROGRESS (DP_ERRNO_DOPPLER_PROC_BASE-3) |
Error Code: DPU is in progress.
#define DPU_DOPPLERPROCHWA_EHWARES (DP_ERRNO_DOPPLER_PROC_BASE-4) |
Error Code: Out of HWA resources.
#define DPU_DOPPLERPROCHWA_ESEMA (DP_ERRNO_DOPPLER_PROC_BASE-5) |
Error Code: Semaphore creation failed.
#define DPU_DOPPLERPROCHWA_ESEMASTATUS (DP_ERRNO_DOPPLER_PROC_BASE-6) |
Error Code: Bad semaphore status.
#define DPU_DOPPLERPROCHWA_EEXCEEDHWAMEM (DP_ERRNO_DOPPLER_PROC_BASE-7) |
Error Code: Configure parameters exceed HWA memory bank size.
#define DPU_DOPPLERPROCHWA_ECUBEFORMAT (DP_ERRNO_DOPPLER_PROC_BASE-8) |
Error Code: Unsupported radar cube format.
#define DPU_DOPPLERPROCHWA_EDETMFORMAT (DP_ERRNO_DOPPLER_PROC_BASE-9) |
Error Code: Unsupported detection matrix format.
#define DPU_DOPPLERPROCHWA_EDETMSIZE (DP_ERRNO_DOPPLER_PROC_BASE-10) |
Error Code: Insufficient detection matrix size.
#define DPU_DOPPLERPROCHWA_EWINDSIZE (DP_ERRNO_DOPPLER_PROC_BASE-11) |
Error Code: Wrong window size.
#define DPU_AOAPROCHWA_EINVAL (DP_ERRNO_AOA_PROC_BASE-1) |
Error Code: Invalid argument.
#define DPU_AOAPROCHWA_ENOMEM (DP_ERRNO_AOA_PROC_BASE-2) |
Error Code: Out of memory.
#define DPU_AOAPROCHWA_EINPROGRESS (DP_ERRNO_AOA_PROC_BASE-3) |
Error Code: DPU is in progress.
#define DPU_AOAPROCHWA_EHWARES (DP_ERRNO_AOA_PROC_BASE-4) |
Error Code: Out of HWA resources.
#define DPU_AOAPROCHWA_ESEMA (DP_ERRNO_AOA_PROC_BASE-5) |
Error Code: Semaphore creation failed.
#define DPU_AOAPROCHWA_ESEMASTATUS (DP_ERRNO_AOA_PROC_BASE-6) |
Error Code: Bad semaphore status.
#define DPU_AOAPROCHWA_EEXCEEDHWAMEM (DP_ERRNO_AOA_PROC_BASE-7) |
Error Code: Configure parameters exceed HWA memory bank size.
#define DPU_AOAPROCHWA_ECUBEFORMAT (DP_ERRNO_AOA_PROC_BASE-8) |
Error Code: Unsupported radar cube format.
#define DPU_AOAPROCHWA_EDETMFORMAT (DP_ERRNO_AOA_PROC_BASE-9) |
Error Code: Unsupported detection matrix format.
#define DPU_AOAPROCHWA_EDETMSIZE (DP_ERRNO_AOA_PROC_BASE-10) |
Error Code: Insufficient detection matrix size.
#define DPU_AOAPROCHWA_EWINDSIZE (DP_ERRNO_AOA_PROC_BASE-11) |
Error Code: Wrong window size.