Introduction
This example application demonstrates the LIN message communication from external PC via PLIN-USB (from PEAK Systems -> IPEH-004052) using interrupts. Instance LIN1 is set in Responder Mode.
The PC via PLIN-USB initiates the transmission to the device, with the help of the PlinViewPro tool, by sending the LINID followed by the publisher or subscriber frames. A database consisting of which of the received ID's are to be responded to, received or ignored are maintained in the example application.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | xWRL1432-evm |
Example folder | examples/drivers/lin/lin_external_responder_interrupts |
Steps to Run the Example
- Board Configuration, change the switch 3 on S4 to OFF mode
LIN switch 3 on S4 set to OFF
- Hardware Connectivity, connect the PLIN-USB module to PC from USB and Serial Port to be connected as mentioned in the image below.
LIN Hardware Connectivity with PLIN USB.
- Software Setup, Download and Install the PLIN-View Pro from https://www.peak-system.com/PLIN-USB.485.0.html?&L=1
- Click on LIN in the menu bar and connect to PLIN-USB. Make sure the LINMode for PLIN is Commander with Baud Rate of 19200.
LIN Hardware Connectivity with PLIN USB.
- After successful connection with PLIN-USB, the status of connection is shown at the bottom of the screen.
PLIN Connectivity status.
- Once connection is established, Create the subscriber and publisher frames in the Transmit section with the ID's and configurations as shown in the below image.
Commander Configurations.
- Now send the publisher or subscriber frames created above by selecting the same in the Transmit tab and pressing the space bar to send the frame to the xWRL1432-evm. The response messages will then be visible in the upper Receive section as shown in the output section(see Sample Output).
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
LIN
Sample Output
Shown below is a sample output when the application is run,
[ LIN RESPONDER ] LIN External Responder Interrupts, application started ...
[ LIN RESPONDER ]
[ LIN RESPONDER ] Request 0x23h(ID) response frame sent 12 34 56 78
[ LIN RESPONDER ]
[ LIN RESPONDER ] Request 0x15h(ID) response frame sent 15 76 98 45 FA FE
[ LIN RESPONDER ]
[ LIN RESPONDER ] Request 0x30h(ID) response frame sent 30 A4 D3 CC F4 67 FF 7D
[ LIN RESPONDER ]
[ LIN RESPONDER ] New Frame Received 0x3C(ID) 00 FF FF FF FF FF FF 7D
[ LIN RESPONDER ] Sleep Frame Received. Going to sleep ...
[ LIN RESPONDER ]
[ LIN RESPONDER ] Wakeup detected. Lin now active.
[ LIN RESPONDER ] New Frame Received 0x1A(ID) 45 45 56
[ LIN RESPONDER ]
[ LIN RESPONDER ] New Frame Received 0x1E(ID) D0 AC FE DC BA FD FF FF
[ LIN RESPONDER ]
[ LIN RESPONDER ] New Frame Received 0x2F(ID) D7 83 99 F6 73
[ LIN RESPONDER ]
[ LIN RESPONDER ] New Frame Received 0x12(ID) F2 3B
[ LIN RESPONDER ]
[ LIN RESPONDER ] All tests have PASSED!!
Shown below is a sample output on PLIN-View Pro
Output on PLIN-View Pro