UART driver object.
Data Fields | |
UART_Handle | handle |
UART_Params | prms |
const void * | writeBuf |
uint32_t | writeCount |
uint32_t | writeSizeRemaining |
void * | readBuf |
uint32_t | readCount |
uint32_t | readSizeRemaining |
uint32_t | rxTimeoutCnt |
uint32_t | readErrorCnt |
UART_Transaction * | readTrans |
UART_Transaction * | writeTrans |
uint32_t | isOpen |
void * | lock |
SemaphoreP_Object | lockObj |
void * | readTransferSem |
SemaphoreP_Object | readTransferSemObj |
void * | writeTransferSem |
SemaphoreP_Object | writeTransferSemObj |
void * | hwiHandle |
HwiP_Object | hwiObj |
UART_EdmaParams | rxEdmaParams |
UART_EdmaParams | txEdmaParams |
EDMA_Handle | uartEdmaHandle |
CSL_app_uartRegs * | pSCIRegs |
uint8_t | shiftJustification |
UART_Handle UART_Object::handle |
Instance handle to which this object belongs
UART_Params UART_Object::prms |
Open parameter as provided by user
const void* UART_Object::writeBuf |
Buffer data pointer
uint32_t UART_Object::writeCount |
Number of Chars sent
uint32_t UART_Object::writeSizeRemaining |
Chars remaining in buffer
void* UART_Object::readBuf |
Buffer data pointer
uint32_t UART_Object::readCount |
Number of Chars read
uint32_t UART_Object::readSizeRemaining |
Chars remaining in buffer
uint32_t UART_Object::rxTimeoutCnt |
Receive timeout error count
uint32_t UART_Object::readErrorCnt |
Line status error count
UART_Transaction* UART_Object::readTrans |
Pointer to the current read transaction
UART_Transaction* UART_Object::writeTrans |
Pointer to the current write transaction
uint32_t UART_Object::isOpen |
Flag to indicate whether the instance is opened already
void* UART_Object::lock |
Instance lock - to protect across transfers
SemaphoreP_Object UART_Object::lockObj |
Driver lock object
void* UART_Object::readTransferSem |
Read Transfer Sync Sempahore - to sync between transfer completion ISR and task
SemaphoreP_Object UART_Object::readTransferSemObj |
Read Transfer Sync Sempahore object
void* UART_Object::writeTransferSem |
Write Transfer Sync Sempahore - to sync between transfer completion ISR and task
SemaphoreP_Object UART_Object::writeTransferSemObj |
Write Transfer Sync Sempahore object
void* UART_Object::hwiHandle |
Interrupt handle for master ISR
HwiP_Object UART_Object::hwiObj |
Interrupt object
UART_EdmaParams UART_Object::rxEdmaParams |
EDMA parameters for the UART Rx
UART_EdmaParams UART_Object::txEdmaParams |
EDMA parameters for the UART Tx
EDMA_Handle UART_Object::uartEdmaHandle |
CSL_app_uartRegs* UART_Object::pSCIRegs |
Pointer to register overlay
uint8_t UART_Object::shiftJustification |
This is the number of bits the read data needs to be shifted. This is calculated using the data length. When data of fewer than eight bits in length is received, it is left-justified in SCIRD and padded with trailing zeros. Data read from the SCIRD should be shifted by software to make the received data rightjustified.