Go to the source code of this file.
Macros | |
SOC Domain ID | |
#define | SOC_DOMAIN_ID_TOPSS_CTRL (0U) |
#define | SOC_DOMAIN_ID_APP_RCM (1U) |
#define | SOC_DOMAIN_ID_APP_CTRL (2U) |
#define | SOC_DOMAIN_ID_TOP_IO_MUX (3U) |
Functions | |
int32_t | SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable) |
Enable clock to specified module. More... | |
int32_t | SOC_clocksEnable (void) |
Enables ADPLL. More... | |
int32_t | SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate) |
Set module clock to specified frequency. More... | |
const char * | SOC_getCoreName (uint16_t coreId) |
Convert a core ID to a user readable name. More... | |
void | SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition) |
Lock control module partition to prevent writes into control MMRs. More... | |
void | SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition) |
Unlock control module partition to allow writes into control MMRs. More... | |
void | SOC_logAllClockHz (void) |
Print's module clock info to the console. More... | |
uint64_t | SOC_virtToPhy (void *virtAddr) |
SOC Virtual (CPU) to Physical address translation function. More... | |
void | SOC_memoryInit (void) |
Initializes HWA shared RAM0, RAM1. More... | |
void | SOC_enableMDLLClock (void) |
Enables MDLL Clock. More... | |