Power manager interface for the 64XX/14xx.
This module defines the power resources, constraints, events, sleep states and transition latencies for 64XX.
A reference power policy is provided which can transition the MCU from the active state to one of two sleep states: Low-Power Deep Sleep (LPDS) or Sleep. The policy looks at the estimated idle time remaining, and the active constraints, and determine which sleep state to transition to. The policy will give first preference to choosing LPDS, but if that is not appropriate (e.g., not enough idle time), it will choose Sleep.
Go to the source code of this file.
Data Structures | |
struct | Power_ParkInfo |
Used to specify parking of a pin during LPDS. More... | |
struct | Power_ConfigV1 |
Power global configuration. More... | |
struct | syncinpadcfg |
struct | Power_Wakeup |
Specify the wakeup sources for LPDS and Shutdown. More... | |
Macros | |
#define | POWER_RESUMETIMELPDS 2500 |
#define | POWER_PERIPH_CAN 0 |
#define | POWER_PERIPH_SPI 1 |
#define | POWER_PERIPH_QSPI 2 |
#define | POWER_PERIPH_TOPSS 3 |
#define | POWER_PERIPH_APP_RTI 4 |
#define | POWER_PERIPH_WD 5 |
#define | POWER_PERIPH_UART0 6 |
#define | POWER_PERIPH_UART1 7 |
#define | POWER_PERIPH_I2C 8 |
#define | POWER_PERIPH_LIN 9 |
#define | POWER_PERIPH_ESM 10 |
#define | POWER_PERIPH_EDMA 11 |
#define | POWER_PERIPH_CRC 12 |
#define | POWER_PERIPH_PWM 13 |
#define | POWER_PERIPH_GIO 14 |
#define | POWER_PERIPH_HWASS 15 |
#define | POWER_DISALLOW_LPDS 0 |
#define | POWER_DISALLOW_SLEEP 1 |
#define | POWER_DISALLOW_IDLE 2 |
#define | POWER_ENTERING_LPDS 0x1 |
#define | POWER_ENTERING_SLEEP 0x2 |
#define | POWER_ENTERING_IDLE 0x4 |
#define | POWER_AWAKE_LPDS 0x8 |
#define | POWER_AWAKE_SLEEP 0x10 |
#define | POWER_AWAKE_IDLE 0x20 |
Functions | |
void | Power_configureWakeup (Power_Wakeup *wakeup) |
Function configures wakeup for LPDS and shutdown. More... | |
void | Power_initPolicy (void) |
void | Power_getWakeup (Power_Wakeup *wakeup) |
Function to get wakeup configuration settings. More... | |
Power_ParkState | Power_getParkState (Power_Pin pin) |
void | Power_restoreParkState (Power_Pin pin, Power_ParkState state) |
void | Power_setParkState (Power_Pin pin, uint32_t level) |
void | Power_sleepPolicy (unsigned long long sleepTimeus) |
A reference power policy is provided which can transition the MCU from the active state to one of two sleep states: Low-Power Deep Sleep (LPDS) or Sleep. More... | |
int_fast16_t | Power_reset (uint_fast16_t resourceId) |
Software reset of a resource. More... | |
void | Power_Idle3 () |
Device Idle mode. More... | |
void | Power_afterLPDS (void) |