![]() |
PDK API Guide for AM64x
|
Functions | |
| uint32_t | CSL_pktdmaGetRevision (const CSL_PktdmaCfg *pCfg) |
| Return revision of the PKTDMA module. More... | |
| int32_t | CSL_pktdmaGetRevisionInfo (const CSL_PktdmaCfg *pCfg, CSL_PktdmaRevision *pRev) |
| Return revision information of the PKTDMA module. More... | |
| void | CSL_pktdmaInitCfg (CSL_PktdmaCfg *pCfg) |
| Initialize contents of a PKTDMA configuration structure. More... | |
| void | CSL_pktdmaGetCfg (CSL_PktdmaCfg *pCfg) |
| Return PKTDMA configuration information. More... | |
| void | CSL_pktdmaInitTxChanCfg (CSL_PktdmaTxChanCfg *pTxChanCfg) |
| Initialize a CSL_PktdmaTxChanCfg structure. More... | |
| void | CSL_pktdmaInitRxChanCfg (CSL_PktdmaRxChanCfg *pRxChanCfg) |
| Initialize a CSL_PktdmaRxChanCfg structure. More... | |
| void | CSL_pktdmaInitRxFlowCfg (CSL_PktdmaRxFlowCfg *pFlow) |
| Initialize a CSL_PktdmaRxFlowCfg structure. More... | |
| void | CSL_pktdmaSetPerfCtrl (CSL_PktdmaCfg *pCfg, uint32_t rxRetryTimeoutCnt) |
| Set performance control parmeters. More... | |
| void | CSL_pktdmaSetUtcCtrl (CSL_PktdmaCfg *pCfg, uint32_t startingThreadNum) |
| [udmap_only] Set UTC control parmeters More... | |
| int32_t | CSL_pktdmaRxFlowCfg (CSL_PktdmaCfg *pCfg, uint32_t flow, const CSL_PktdmaRxFlowCfg *pFlow) |
| Configure an RX flow. More... | |
| int32_t | CSL_pktdmaRxChanCfg (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, const CSL_PktdmaRxChanCfg *pRxChanCfg) |
| Configure an RX channel. More... | |
| int32_t | CSL_pktdmaTxChanCfg (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, const CSL_PktdmaTxChanCfg *pTxChanCfg) |
| Configure a TX channel. More... | |
| int32_t | CSL_pktdmaRxChanSetTrEvent (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, uint32_t trEventNum) |
| [udmap_only] Configure an RX channel TR event More... | |
| int32_t | CSL_pktdmaTxChanSetTrEvent (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, uint32_t trEventNum) |
| [udmap_only]Configure an TX channel TR event More... | |
| int32_t | CSL_pktdmaRxChanSetBurstSize (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanBurstSize burstSize) |
| Configure RX channel burst size. More... | |
| int32_t | CSL_pktdmaTxChanSetBurstSize (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanBurstSize burstSize) |
| Configure TX channel burst size. More... | |
| int32_t | CSL_pktdmaGetRxRT (const CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaRT *pRT) |
| Get an RX channel's real-time register values. More... | |
| int32_t | CSL_pktdmaGetTxRT (const CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaRT *pRT) |
| Get a TX channel's real-time register values. More... | |
| int32_t | CSL_pktdmaSetRxRT (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, const CSL_PktdmaRT *pRT) |
| Set an RX channel's real-time register values. More... | |
| int32_t | CSL_pktdmaSetTxRT (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, const CSL_PktdmaRT *pRT) |
| Set a TX channel's real-time register values. More... | |
| int32_t | CSL_pktdmaEnableTxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Enable a transmit channel. More... | |
| int32_t | CSL_pktdmaDisableTxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Disable a transmit channel. More... | |
| int32_t | CSL_pktdmaTeardownTxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, bool bForce, bool bWait) |
| Teardown a transmit channel. More... | |
| int32_t | CSL_pktdmaPauseTxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Pause a transmit channel. More... | |
| int32_t | CSL_pktdmaUnpauseTxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Un-pause a transmit channel. More... | |
| int32_t | CSL_pktdmaTriggerTxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| [udmap_only] Send a trigger event to a TX channel More... | |
| void | CSL_pktdmaClearTxChanError (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Clear error indication in a transmit channel. More... | |
| int32_t | CSL_pktdmaEnableRxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Enable a receive channel. More... | |
| int32_t | CSL_pktdmaDisableRxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Disable a receive channel. More... | |
| int32_t | CSL_pktdmaTeardownRxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, bool bForce, bool bWait) |
| Teardown a receive channel. More... | |
| int32_t | CSL_pktdmaPauseRxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Pause a receive channel. More... | |
| int32_t | CSL_pktdmaUnpauseRxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Un-pause a receive channel. More... | |
| int32_t | CSL_pktdmaTriggerRxChan (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| [udmap_only] Send a trigger event to an RX channel More... | |
| void | CSL_pktdmaClearRxChanError (CSL_PktdmaCfg *pCfg, uint32_t chanIdx) |
| Clear error indication in a receive channel. More... | |
| void | CSL_pktdmaCfgRxFlowIdFirewall (CSL_PktdmaCfg *pCfg, uint32_t outEvtNum) |
| Configure the receive flow ID range firewall. More... | |
| bool | CSL_pktdmaGetRxFlowIdFirewallStatus (CSL_PktdmaCfg *pCfg, CSL_PktdmaRxFlowIdFirewallStatus *pRxFlowIdFwStatus) |
| Get receive flow ID range firewall status information. More... | |
| void | CSL_pktdmaGetChanStats (const CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanDir chanDir, CSL_PktdmaChanStats *pChanStats) |
| Get channel statistics. More... | |
| void | CSL_pktdmaDecChanStats (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanDir chanDir, const CSL_PktdmaChanStats *pChanStats) |
| Decrement channel statistics. More... | |
| int32_t | CSL_pktdmaGetChanPeerReg (const CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanDir chanDir, uint32_t regIdx, uint32_t *pVal) |
| Read a channel peer register. More... | |
| int32_t | CSL_pktdmaSetChanPeerReg (const CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanDir chanDir, uint32_t regIdx, uint32_t *pVal) |
| Write a channel peer register. More... | |
| int32_t | CSL_pktdmaEnableLink (CSL_PktdmaCfg *pCfg, uint32_t chanIdx, CSL_PktdmaChanDir chanDir) |
| Enable a directional data flow for a paired link. More... | |
| uint32_t CSL_pktdmaGetRevision | ( | const CSL_PktdmaCfg * | pCfg | ) |
Return revision of the PKTDMA module.
This function returns the contents of the PKTDMA revision register. Consult the PKTDMA module documentation for a description of the contents of the revision register.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| int32_t CSL_pktdmaGetRevisionInfo | ( | const CSL_PktdmaCfg * | pCfg, |
| CSL_PktdmaRevision * | pRev | ||
| ) |
Return revision information of the PKTDMA module.
This function returns revision information for the PKTDMA module.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| pRev | [OUT] Pointer to a CSL_PktdmaRevision structure where the revision information is returned |
| void CSL_pktdmaInitCfg | ( | CSL_PktdmaCfg * | pCfg | ) |
Initialize contents of a PKTDMA configuration structure.
This function initializes the contents of the specified PKTDMA configuration structure.
All elements of the CSL_PktdmaCfg structure are initialized to zero.
This function should not be called after calling CSL_pktdmaGetCfg as the PKTDMA module configuration stored in the PKTDMA configuration structure will be overwritten with zeros.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| void CSL_pktdmaGetCfg | ( | CSL_PktdmaCfg * | pCfg | ) |
Return PKTDMA configuration information.
This function returns configuration and capability information for the PKTDMA module. See the CSL_PktdmaCfg structure for details on the information that is returned.
| pCfg | [IN/OUT] Pointer to the PKTDMA configuration structure |
| void CSL_pktdmaInitTxChanCfg | ( | CSL_PktdmaTxChanCfg * | pTxChanCfg | ) |
Initialize a CSL_PktdmaTxChanCfg structure.
This function initializes the specified CSL_PktdmaTxChanCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_pktdmaTxChanCfg function.
All elements of the CSL_PktdmaTxChanCfg structure are initialized to zero except for the following:
chanType = CSL_PKTDMA_CHAN_TYPE_NORMAL; fetchWordSize = CSL_PKTDMA_FETCH_WORD_SIZE_16; trEventNum = CSL_PKTDMA_NO_EVENT; errEventNum = CSL_PKTDMA_NO_EVENT;
| pTxChanCfg | [OUT] Pointer to a CSL_PktdmaTxChanCfg structure |
| void CSL_pktdmaInitRxChanCfg | ( | CSL_PktdmaRxChanCfg * | pRxChanCfg | ) |
Initialize a CSL_PktdmaRxChanCfg structure.
This function initializes the specified CSL_PktdmaRxChanCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_pktdmaRxChanCfg function.
All elements of the CSL_PktdmaRxChanCfg structure are initialized to zero except for the following:
chanType = CSL_PKTDMA_CHAN_TYPE_NORMAL; fetchWordSize = CSL_PKTDMA_FETCH_WORD_SIZE_16; trEventNum = CSL_PKTDMA_NO_EVENT; errEventNum = CSL_PKTDMA_NO_EVENT; flowIdFwRangeCnt = CSL_PKTDMA_RXCCFG_CHAN_RFLOW_RNG_FLOWID_CNT_RESETVAL;
| pRxChanCfg | [OUT] Pointer to a CSL_PktdmaRxChanCfg structure |
| void CSL_pktdmaInitRxFlowCfg | ( | CSL_PktdmaRxFlowCfg * | pFlow | ) |
Initialize a CSL_PktdmaRxFlowCfg structure.
This function initializes the specified CSL_PktdmaRxFlowCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_pktdmaRxFlowCfg function.
All elements of the CSL_PktdmaRxFlowCfg structure are initialized to zero.
| pFlow | [OUT] Pointer to a CSL_PktdmaRxFlowCfg structure |
| void CSL_pktdmaSetPerfCtrl | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | rxRetryTimeoutCnt | ||
| ) |
Set performance control parmeters.
This function is used to set performance control paramaters available in the PKTDMA module.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| rxRetryTimeoutCnt | [IN] This parameter specifies the minimum amount of time (in clock cycles) that an Rx channel will be required to wait when it encounters a buffer starvation condition and the Rx error handling bit is set to 1 |
| void CSL_pktdmaSetUtcCtrl | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | startingThreadNum | ||
| ) |
[udmap_only] Set UTC control parmeters
This function is used to set UTC control paramaters available in the PKTDMA module.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| startingThreadNum | [IN] This parameter specifies the starting PSI-L thread number for the external UTC |
| int32_t CSL_pktdmaRxFlowCfg | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | flow, | ||
| const CSL_PktdmaRxFlowCfg * | pFlow | ||
| ) |
Configure an RX flow.
This function initializes a receive flow with values specified in the CSL_PktdmaRxFlowCfg structure.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| flow | [IN] Index of the receive flow to initialize |
| pFlow | [IN] Pointer to a CSL_PktdmaRxFlowCfg structure containing initialization values |
| int32_t CSL_pktdmaRxChanCfg | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| const CSL_PktdmaRxChanCfg * | pRxChanCfg | ||
| ) |
Configure an RX channel.
This function initializes a receive channel with values specified in the CSL_PktdmaRxChanCfg structure.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the receive channel to initialize |
| pRxChanCfg | [IN] Pointer to a CSL_PktdmaRxChanCfg structure containing initialization values |
| int32_t CSL_pktdmaTxChanCfg | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| const CSL_PktdmaTxChanCfg * | pTxChanCfg | ||
| ) |
Configure a TX channel.
This function initializes a transmit channel with values specified in the CSL_PktdmaTxChanCfg structure.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel to initialize |
| pTxChanCfg | [IN] Pointer to a CSL_PktdmaTxChanCfg structure containing initialization values |
| int32_t CSL_pktdmaRxChanSetTrEvent | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| uint32_t | trEventNum | ||
| ) |
[udmap_only] Configure an RX channel TR event
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the receive channel to initialize |
| trEventNum | [IN] Specifies a global event number to generate anytime the required event generation criteria specified in a TR are met Set to CSL_PKTDMA_NO_EVENT for no event generation. |
| int32_t CSL_pktdmaTxChanSetTrEvent | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| uint32_t | trEventNum | ||
| ) |
[udmap_only]Configure an TX channel TR event
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel to initialize |
| trEventNum | [IN] Specifies a global event number to generate anytime the required event generation criteria specified in a TR are met Set to CSL_PKTDMA_NO_EVENT for no event generation. |
| int32_t CSL_pktdmaRxChanSetBurstSize | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanBurstSize | burstSize | ||
| ) |
Configure RX channel burst size.
This function enables configuration of the nominal burst size and alignment for data transfers on the specified RX channel. The default burst size is 64 bytes (a value of CSL_PKTDMA_CHAN_BURST_SIZE_64_BYTES).
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the receive channel to initialize |
| burstSize | [IN] Burst size value. See CSL_PktdmaChanBurstSize for a list of valid burst size values. |
| int32_t CSL_pktdmaTxChanSetBurstSize | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanBurstSize | burstSize | ||
| ) |
Configure TX channel burst size.
This function enables configuration of the nominal burst size and alignment for data transfers on the specified TX channel. The default burst size is 64 bytes (a value of CSL_PKTDMA_CHAN_BURST_SIZE_64_BYTES).
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel to initialize |
| burstSize | [IN] Burst size value. See CSL_PktdmaChanBurstSize for a list of valid burst size values. |
| int32_t CSL_pktdmaGetRxRT | ( | const CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaRT * | pRT | ||
| ) |
Get an RX channel's real-time register values.
This function returns the real-time register values for the specified receive channel.
Note that no parameter error checking is performed by this function for performance reasons.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the receive channel |
| pRT | [OUT] Pointer to a CSL_PktdmaRT structure where values are returned |
| int32_t CSL_pktdmaGetTxRT | ( | const CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaRT * | pRT | ||
| ) |
Get a TX channel's real-time register values.
This function returns the real-time register values for the specified transmit channel.
Note that no parameter error checking is performed by this function for performance reasons.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel |
| pRT | [OUT] Pointer to a CSL_PktdmaRT structure where values are returned |
| int32_t CSL_pktdmaSetRxRT | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| const CSL_PktdmaRT * | pRT | ||
| ) |
Set an RX channel's real-time register values.
This function sets the real-time register values for the specified receive channel.
Note that no parameter error checking is performed by this function for performance reasons.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the receive channel |
| pRT | [IN] Pointer to a CSL_PktdmaRT structure containing initialization values |
| int32_t CSL_pktdmaSetTxRT | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| const CSL_PktdmaRT * | pRT | ||
| ) |
Set a TX channel's real-time register values.
This function sets the real-time register values for the specified transmit channel.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel |
| pRT | [IN] Pointer to a CSL_PktdmaRT structure containing initialization values |
Note that no parameter error checking is performed by this function for performance reasons.
| int32_t CSL_pktdmaEnableTxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Enable a transmit channel.
This function enables the transmit channel specified by 'chanIdx'.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| int32_t CSL_pktdmaDisableTxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Disable a transmit channel.
This function disables the transmit channel specified by 'chanIdx'.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| int32_t CSL_pktdmaTeardownTxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| bool | bForce, | ||
| bool | bWait | ||
| ) |
Teardown a transmit channel.
This function tears down the transmit channel specified by 'chanIdx' at the next packet boundary.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| bForce | [IN] If true, the channel is torn down without attempting to preserve data or wait for events (flushes the channel). If false, any packets in flight are completed prior to the channel being torn down. |
| bWait | [IN] If true, wait for the teardown operation to complete. Otherwise, return immediately. |
| int32_t CSL_pktdmaPauseTxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Pause a transmit channel.
This function pauses the transmit channel specified by 'chanIdx' at the next packet boundary. This is a more graceful method of halting processing than disabling the channel as it will not allow any current packets to underflow.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| int32_t CSL_pktdmaUnpauseTxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Un-pause a transmit channel.
This function un-pauses the transmit channel specified by 'chanIdx'.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| int32_t CSL_pktdmaTriggerTxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
[udmap_only] Send a trigger event to a TX channel
This function causes a trigger event to be sent to the specified transmit channel.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel |
| void CSL_pktdmaClearTxChanError | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Clear error indication in a transmit channel.
This function clears the error indication in the specified transmit channel.
Note that no parameter error checking is performed by this function for performance reasons.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| int32_t CSL_pktdmaEnableRxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Enable a receive channel.
This function enables the receive channel specified by 'chanIdx'.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the receive channel |
| int32_t CSL_pktdmaDisableRxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Disable a receive channel.
This function disables the receive channel specified by 'chanIdx'.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the receive channel |
| int32_t CSL_pktdmaTeardownRxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| bool | bForce, | ||
| bool | bWait | ||
| ) |
Teardown a receive channel.
This function tears down the receive channel specified by 'chanIdx' at the next packet boundary.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the receive channel |
| bForce | [IN] If true, the channel is torn down without attempting to preserve data or wait for events (flushes the channel). If false, any packets in flight are completed prior to the channel being torn down. |
| bWait | [IN] If true, wait for the teardown operation to complete. Otherwise, return immediately. |
| int32_t CSL_pktdmaPauseRxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Pause a receive channel.
This function pauses the receive channel specified by 'chanIdx' at the next packet boundary. This is a more graceful method of halting processing than disabling the channel as it will not allow any current packets to underflow.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the receive channel |
| int32_t CSL_pktdmaUnpauseRxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Un-pause a receive channel.
This function un-pauses the receive channel specified by 'chanIdx'.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the transmit channel |
| int32_t CSL_pktdmaTriggerRxChan | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
[udmap_only] Send a trigger event to an RX channel
This function causes a trigger event to be sent to the specified receive channel.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the receive channel |
| void CSL_pktdmaClearRxChanError | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx | ||
| ) |
Clear error indication in a receive channel.
This function clears the error indication in the specified receive channel.
Note that no parameter error checking is performed by this function for performance reasons.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] The index of the receive channel |
| void CSL_pktdmaCfgRxFlowIdFirewall | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | outEvtNum | ||
| ) |
Configure the receive flow ID range firewall.
This function is used to configure the receive flow ID range firewall.
Note: This function is provided for backwards compatibility with the udmap CSL-FL.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| outEvtNum | [IN] Output event number to use when the receive flow ID range firewall detects an error |
| bool CSL_pktdmaGetRxFlowIdFirewallStatus | ( | CSL_PktdmaCfg * | pCfg, |
| CSL_PktdmaRxFlowIdFirewallStatus * | pRxFlowIdFwStatus | ||
| ) |
Get receive flow ID range firewall status information.
This function returns information from the receive flow ID range firewall.
If the receive flow ID firewall has detected an out of range flow ID, the function returns true and the fields within the CSL_PktdmaRxFlowIdFirewallStatus structure contain error details. The function will automatically reset the receive flow ID firewall to capture the next error.
If the receive flow ID firewall has not detected an out of range flow ID, the function returns false and the fields within the CSL_PktdmaRxFlowIdFirewallStatus structure are not updated.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| pRxFlowIdFwStatus | [IN] Pointer to a CSL_PktdmaRxFlowIdFirewallStatus structure containing error details (valid only when true is returned) |
| void CSL_pktdmaGetChanStats | ( | const CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanDir | chanDir, | ||
| CSL_PktdmaChanStats * | pChanStats | ||
| ) |
Get channel statistics.
This function is used to read statistics for a transmit or receive channel.
Note that no parameter error checking is performed by this function for performance reasons.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the channel |
| chanDir | [IN] Channel direction (see CSL_PktdmaChanDir) |
| pChanStats | [OUT] Pointer to a CSL_PktdmaChanStats structure where the statistics are returned |
| void CSL_pktdmaDecChanStats | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanDir | chanDir, | ||
| const CSL_PktdmaChanStats * | pChanStats | ||
| ) |
Decrement channel statistics.
Note that no parameter error checking is performed by this function for performance reasons.
This function is used to decrement statistics for a transmit or receive channel by the counts contained in the specified CSL_PktdmaChanStats structure.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the channel |
| chanDir | [IN] Channel direction (see CSL_PktdmaChanDir) |
| pChanStats | [IN] Pointer to a CSL_PktdmaChanStats structure containing the counts to decrement each statistic by |
| int32_t CSL_pktdmaGetChanPeerReg | ( | const CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanDir | chanDir, | ||
| uint32_t | regIdx, | ||
| uint32_t * | pVal | ||
| ) |
Read a channel peer register.
This function is used to read the value from a peer register for the specified channel.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the channel |
| chanDir | [IN] Channel direction (see CSL_PktdmaChanDir) |
| regIdx | [IN] Peer register index (0..15) |
| pVal | [OUT] Pointer where the register value is returned |
| int32_t CSL_pktdmaSetChanPeerReg | ( | const CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanDir | chanDir, | ||
| uint32_t | regIdx, | ||
| uint32_t * | pVal | ||
| ) |
Write a channel peer register.
This function is used to write a value to a peer register for the specified transmit channel.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the transmit channel |
| chanDir | [IN] Channel direction (see CSL_PktdmaChanDir) |
| regIdx | [IN] Peer register index (0..15) |
| pVal | [IN] Pointer to the register value to be written |
| int32_t CSL_pktdmaEnableLink | ( | CSL_PktdmaCfg * | pCfg, |
| uint32_t | chanIdx, | ||
| CSL_PktdmaChanDir | chanDir | ||
| ) |
Enable a directional data flow for a paired link.
This function is used to enable a directional data flow for a given PKTDMA channel between PKTDMA and a paired PSIL peer.
| pCfg | [IN] Pointer to the PKTDMA configuration structure |
| chanIdx | [IN] Index of the PKTDMA channel (TX or RX) |
| chanDir | [IN] Channel direction (TX or RX, see CSL_PktdmaChanDir) |