![]() |
PDK API Guide for AM65xx
|
Multi-Channel SPI driver interface.
============================================================================
The MCSPI header file should be included in an application as follows:
Go to the source code of this file.
Data Structures | |
| struct | MCSPI_Params |
| MCSPI Parameters. More... | |
| struct | MCSPI_FxnTable |
| The definition of a MCSPI function table that contains the required set of functions to control a specific MCSPI driver implementation. More... | |
| struct | MCSPI_Config |
| MCSPI Global configuration. More... | |
Macros | |
| #define | MCSPI_MAX_NUM_INSTANCES (SPI_MAX_CONFIG_CNT) |
| Max number of MCSPI peripheral instances. More... | |
| #define | MCSPI_MAX_NUM_CHANNELS (4U) |
| Max number of channels of a MCSPI peripheral instance. More... | |
Typedefs | |
| typedef struct MCSPI_Config_s * | MCSPI_Handle |
| A handle that is returned from a MCSPI_open() call. More... | |
| typedef void(* | MCSPI_CallbackFxn) (MCSPI_Handle handle, SPI_Transaction *transaction) |
| The definition of a callback function used by the MCSPI driver when used in SPI_MODE_CALLBACK. More... | |
| typedef void(* | MCSPI_CloseFxn) (MCSPI_Handle handle) |
| A function pointer to a driver specific implementation of MCSPI_close(). More... | |
| typedef int32_t(* | MCSPI_ControlFxn) (MCSPI_Handle handle, uint32_t cmd, const void *arg) |
| A function pointer to a driver specific implementation of MCSPI_control(). More... | |
| typedef void(* | MCSPI_InitFxn) (MCSPI_Handle handle) |
| A function pointer to a driver specific implementation of MCSPI_init(). More... | |
| typedef MCSPI_Handle(* | MCSPI_OpenFxn) (MCSPI_Handle handle, const MCSPI_Params *params) |
| A function pointer to a driver specific implementation of MCSPI_open(). More... | |
| typedef bool(* | MCSPI_TransferFxn) (MCSPI_Handle handle, SPI_Transaction *transaction) |
| A function pointer to a driver specific implementation of MCSPI_transfer(). More... | |
| typedef void(* | MCSPI_TransferCancelFxn) (MCSPI_Handle handle) |
| A function pointer to a driver specific implementation of MCSPI_transferCancel(). More... | |
| typedef MCSPI_Config | MCSPI_config_list[MCSPI_MAX_NUM_INSTANCES][MCSPI_MAX_NUM_CHANNELS] |
Functions | |
| void | MCSPI_close (MCSPI_Handle handle) |
| Function to close a channel of a SPI peripheral specified by the MCSPI handle. More... | |
| int32_t | MCSPI_control (MCSPI_Handle handle, uint32_t cmd, void *arg) |
| Function performs implementation specific features on a channel of a SPI peripheral specified by the MCSPI handle. More... | |
| void | MCSPI_init (void) |
| This function initializes the MCSPI module. More... | |
| MCSPI_Handle | MCSPI_open (uint32_t idx, uint32_t channel, MCSPI_Params *params) |
| This function opens a given channel of a given MCSPI peripheral. More... | |
| void | MCSPI_Params_init (MCSPI_Params *params) |
| Function to initialize the MCSPI_Params struct to its defaults. More... | |
| bool | MCSPI_transfer (MCSPI_Handle handle, SPI_Transaction *spiTrans) |
| Function to perform SPI transactions on a channel of a SPI peripheral specified by the MCSPI handle. More... | |
| void | MCSPI_transferCancel (MCSPI_Handle handle) |
| Function to cancel SPI transactions on channel of a SPI peripheral specified by the MCSPI handle. More... | |