![]() |
PDK API Guide for AM65xx
|
HeapP interface
Files | |
file | HeapP.h |
Heap management module for the RTOS Porting Interface. | |
Data Structures | |
struct | HeapP_Params |
Basic HeapP Parameters. More... | |
struct | HeapP_MemStats |
Structure used to pass information about the heap out of HeapP_getHeapStats(). More... | |
Functions | |
void | HeapP_Params_init (HeapP_Params *params) |
Initialize params structure to default values. More... | |
HeapP_Handle | HeapP_create (const HeapP_Params *params) |
Create a user defined heap. More... | |
HeapP_Status | HeapP_delete (HeapP_Handle handle) |
Delete the user defined heap. More... | |
void * | HeapP_alloc (HeapP_Handle handle, uint32_t allocSize) |
Alloc memory from user defined heap. More... | |
HeapP_Status | HeapP_free (HeapP_Handle handle, void *ptr, uint32_t size) |
Free memory from user defined heap. More... | |
HeapP_Status | HeapP_getHeapStats (HeapP_Handle handle, HeapP_MemStats *stats) |
Get detailed heap statistics. More... | |
Typedefs | |
typedef void * | HeapP_Handle |
Opaque client reference to an instance of a HeapP. More... | |
Enumerations | |
enum | HeapP_Status { HeapP_OK = 0, HeapP_FAILURE = (-(int32_t)1) } |
Status codes for HeapP APIs. More... | |
Macros | |
#define | HeapP_BYTE_ALIGNMENT (256U) |
Minimum alignment for heap allocations, in units of bytes. More... | |
#define HeapP_BYTE_ALIGNMENT (256U) |
Minimum alignment for heap allocations, in units of bytes.
typedef void* HeapP_Handle |
Opaque client reference to an instance of a HeapP.
A HeapP_Handle returned from the HeapP_create represents that instance and is used in the other instance based functions
enum HeapP_Status |
void HeapP_Params_init | ( | HeapP_Params * | params | ) |
Initialize params structure to default values.
params | Pointer to the instance configuration parameters. |
HeapP_Handle HeapP_create | ( | const HeapP_Params * | params | ) |
Create a user defined heap.
The actual heap start address and size will be adjusted to satisfy HeapP_BYTE_ALIGNMENT.
params | Pointer to the instance configuration parameters. |
HeapP_Status HeapP_delete | ( | HeapP_Handle | handle | ) |
Delete the user defined heap.
handle | [in] Heap handle |
void* HeapP_alloc | ( | HeapP_Handle | handle, |
uint32_t | allocSize | ||
) |
Alloc memory from user defined heap.
handle | [in] Heap handle |
allocSize | [in] Size of memory to allocate |
HeapP_Status HeapP_free | ( | HeapP_Handle | handle, |
void * | ptr, | ||
uint32_t | size | ||
) |
Free memory from user defined heap.
handle | [in] Heap handle |
ptr | [in] Pointer to memory allocated using HeapP_alloc |
size | [in] Size of the block of memory to free |
HeapP_Status HeapP_getHeapStats | ( | HeapP_Handle | handle, |
HeapP_MemStats * | stats | ||
) |
Get detailed heap statistics.
handle | [in] Heap handle |
stats | [out] Returned heap statistics |