![]() |
PDK API Guide for AM65xx
|
Files | |
| file | csl_dssOverlay.h |
| DSS Overlay CSL FL interface file. | |
Data Structures | |
| struct | CSL_DssOverlayCfg |
| Configuration for DSS Overlay. More... | |
| struct | CSL_DssOverlayLayerCfg |
| Configuration for selecting overlay input layers. More... | |
| struct | CSL_DssOverlayPipePosCfg |
| Video Pipe Position Configuration in Overlay. More... | |
Functions | |
| void | CSL_dssOverlaySetConfig (CSL_dss_overlayRegs *overlayRegs, const CSL_DssOverlayCfg *overlayCfg) |
| Configure the Overlay Params. More... | |
| void | CSL_dssOverlayColorBarEnable (CSL_dss_overlayRegs *overlayRegs, uint32_t enable) |
| Enable the Color Bar in DSS Overlay. More... | |
| void | CSL_dssOverlaySetLayerConfig (CSL_dss_overlayRegs *overlayRegs, const CSL_DssOverlayLayerCfg *layerCfg) |
| Configure the Overlay input selection. More... | |
| void | CSL_dssOverlaySetPipePosConfig (CSL_dss_overlayRegs *overlayRegs, const CSL_DssOverlayPipePosCfg *pipePosCfg, uint32_t layerNum) |
| Configure the Video Pipe Position in Overlay. More... | |
| uint32_t | CSL_dssOverlayGetEnabledPipeLayerNum (const CSL_dss_overlayRegs *overlayRegs, uint32_t pipeId) |
| Get the layer number where a particular Video Pipe is connected. More... | |
| static void | CSL_dssOverlayCfgInit (CSL_DssOverlayCfg *overlayCfg) |
| CSL_DssOverlayCfg structure init function. More... | |
| static void | CSL_dssOverlayLayerCfgInit (CSL_DssOverlayLayerCfg *layerCfg) |
| CSL_DssOverlayLayerCfg structure init function. More... | |
| static void | CSL_dssOverlayPipePosCfgInit (CSL_DssOverlayPipePosCfg *pipePosCfg) |
| CSL_DssOverlayPipePosCfg structure init function. More... | |
Typedefs | |
| typedef CSL_dss_ovr1Regs | CSL_dss_overlayRegs |
| DSS Overlay Registers. More... | |
DSS Overlay Transparency Color Key Selection | |
| #define | CSL_DSS_OVERLAY_TRANS_COLOR_DEST ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_GDTK) |
| Destination transparency color key selected. More... | |
| #define | CSL_DSS_OVERLAY_TRANS_COLOR_SRC ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_VSTK) |
| Source transparency color key selected. More... | |
DSS Overlay Layer Number | |
| #define | CSL_DSS_OVERLAY_LAYER_NUM_0 ((uint32_t) 0x0U) |
| Overlay Layer 0. More... | |
| #define | CSL_DSS_OVERLAY_LAYER_NUM_1 ((uint32_t) 0x1U) |
| Overlay Layer 1. More... | |
| #define | CSL_DSS_OVERLAY_LAYER_MAX ((uint32_t) 0x2U) |
| Maximum overlay layers. More... | |
| #define | CSL_DSS_OVERLAY_LAYER_INVALID ((uint32_t) 0xFFU) |
| Invalid Overlay Layer. More... | |
| #define CSL_DSS_OVERLAY_TRANS_COLOR_DEST ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_GDTK) |
Destination transparency color key selected.
| #define CSL_DSS_OVERLAY_TRANS_COLOR_SRC ((uint32_t) CSL_DSS_OVR1_CONFIG_TCKLCDSELECTION_VAL_VSTK) |
Source transparency color key selected.
| #define CSL_DSS_OVERLAY_LAYER_NUM_0 ((uint32_t) 0x0U) |
Overlay Layer 0.
| #define CSL_DSS_OVERLAY_LAYER_NUM_1 ((uint32_t) 0x1U) |
Overlay Layer 1.
| #define CSL_DSS_OVERLAY_LAYER_MAX ((uint32_t) 0x2U) |
Maximum overlay layers.
| #define CSL_DSS_OVERLAY_LAYER_INVALID ((uint32_t) 0xFFU) |
Invalid Overlay Layer.
| typedef CSL_dss_ovr1Regs CSL_dss_overlayRegs |
DSS Overlay Registers.
DSS7 UL has two identical Overlay blocks, hence define a generic structure to have common APIs
| void CSL_dssOverlaySetConfig | ( | CSL_dss_overlayRegs * | overlayRegs, |
| const CSL_DssOverlayCfg * | overlayCfg | ||
| ) |
Configure the Overlay Params.
| overlayRegs | Pointer to a CSL_dss_overlayRegs structure containing the overlay configuration |
| overlayCfg | Pointer to the CSL_DssOverlayCfg structure. This parameter should not be NULL |
| void CSL_dssOverlayColorBarEnable | ( | CSL_dss_overlayRegs * | overlayRegs, |
| uint32_t | enable | ||
| ) |
Enable the Color Bar in DSS Overlay.
| overlayRegs | Pointer to a CSL_dss_overlayRegs structure containing the overlay configuration |
| enable | Enable or disable the color bar |
| void CSL_dssOverlaySetLayerConfig | ( | CSL_dss_overlayRegs * | overlayRegs, |
| const CSL_DssOverlayLayerCfg * | layerCfg | ||
| ) |
Configure the Overlay input selection.
| overlayRegs | Pointer to a CSL_dss_overlayRegs structure containing the overlay configuration |
| layerCfg | Pointer to CSL_DssOverlayLayerCfg structure. This parameter should not be NULL |
| void CSL_dssOverlaySetPipePosConfig | ( | CSL_dss_overlayRegs * | overlayRegs, |
| const CSL_DssOverlayPipePosCfg * | pipePosCfg, | ||
| uint32_t | layerNum | ||
| ) |
Configure the Video Pipe Position in Overlay.
| overlayRegs | Pointer to a CSL_dss_overlayRegs structure containing the overlay configuration |
| pipePosCfg | Pointer to CSL_DssOverlayPipePosCfg structure. This parameter should not be NULL |
| layerNum | Layer Number |
| uint32_t CSL_dssOverlayGetEnabledPipeLayerNum | ( | const CSL_dss_overlayRegs * | overlayRegs, |
| uint32_t | pipeId | ||
| ) |
Get the layer number where a particular Video Pipe is connected.
| overlayRegs | Pointer to a CSL_dss_overlayRegs structure containing the overlay configuration |
| pipeId | Pipe Id. Refer to CSL_DssVidPipeId for values |
|
inlinestatic |
CSL_DssOverlayCfg structure init function.
| overlayCfg | Pointer to CSL_DssOverlayCfg structure |
|
inlinestatic |
CSL_DssOverlayLayerCfg structure init function.
| layerCfg | Pointer to CSL_DssOverlayLayerCfg structure |
|
inlinestatic |
CSL_DssOverlayPipePosCfg structure init function.
| pipePosCfg | Pointer to CSL_DssOverlayPipePosCfg structure |