Interface file for LDC M2M FVID2 driver
|
| file | vhwa_m2mLdc.h |
| | Defines the structures / control operations that could be used to configure / control LDC M2M driver.
|
| |
| #define VHWA_M2M_LDC_DRV_INST_ID (0U) |
< Instance ID for the LDC M2m driver
| #define VHWA_M2M_LDC_MAX_HANDLES (8u) |
Max Number of handles supported by LDC M2M Driver.
IOCTL for setting LDC configuration. This IOCTL takes LDC Configuration Ldc_Config as input.
- Returns
- FVID2_SOK on success, else error code.
IOCTL for getting module's performance numbers for the last frame submitted.
- Returns
- FVID2_SOK on success, else error code.
| #define IOCTL_VHWA_M2M_LDC_GET_PSA_SIGN |
Value:#define IOCTL_VHWA_M2M_LDC_GET_PERFORMANCE
IOCTL for getting module's performance numbers for the last frame submitted.
Definition: vhwa_m2mLdc.h:122
IOCTL for getting LSE PSA Signature.
- Returns
- FVID2_SOK on success, else error code.
| #define IOCTL_VHWA_M2M_LDC_REGISTER_ERR_CB |
Value: 1U)
#define IOCTL_VHWA_M2M_LDC_GET_PSA_SIGN
IOCTL for getting LSE PSA Signature.
Definition: vhwa_m2mLdc.h:129
IOCTL for enabling error events and registering callbacks for the same. This IOCTL pointer to Ldc_ErrEventParams as input.
- Returns
- FVID2_SOK on success, else error code.
| #define IOCTL_VHWA_M2M_LDC_SET_RD_BW_LIMIT |
Value:#define IOCTL_VHWA_M2M_LDC_REGISTER_ERR_CB
IOCTL for enabling error events and registering callbacks for the same. This IOCTL pointer to Ldc_Err...
Definition: vhwa_m2mLdc.h:139
IOCTL for enabling and setting parameters for LDC Read bandwidth limiter. This ioctl sets the configurations directly in the registers, so it gets used for all open handles. This IOCTL takes pointer to Ldc_RdBwLimitConfig as input.
- Returns
- FVID2_SOK on success, else error code.
| #define IOCTL_VHWA_M2M_LDC_SET_HTS_LIMIT |
Value:#define IOCTL_VHWA_M2M_LDC_SET_RD_BW_LIMIT
IOCTL for enabling and setting parameters for LDC Read bandwidth limiter. This ioctl sets the configu...
Definition: vhwa_m2mLdc.h:150
IOCTL for enabling and setting HTS limiter. This is used to slowed down the HTS by introducing clock cycles between internal start signals. This IOCTL takes pointer to Vhwa_HtsLimiter as input.
- Returns
- FVID2_SOK on success, else error code.
| #define IOCTL_VHWA_M2M_LDC_SYNC_START |
Value:#define IOCTL_VHWA_M2M_LDC_SET_HTS_LIMIT
IOCTL for enabling and setting HTS limiter. This is used to slowed down the HTS by introducing clock ...
Definition: vhwa_m2mLdc.h:161
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing.
- Returns
- FVID2_SOK on success, else error code.
Initializes LDC Init Parameters.
- Parameters
-
| ldcInitPrms | LDC Init Parameters This parameter should not be 0. |
- Returns
- Returns 0 on success else returns error value
| void Vhwa_m2mLdcDeInit |
( |
void |
| ) |
|
DeInitializes LDC Init Parameters.
Function to allocate Sl2 memory for the output buffers.
- Parameters
-
- Returns
- FVID2_SOK if successful, else suitable error code
| void Vhwa_m2mLdcFreeSl2 |
( |
void |
| ) |
|
Function to free allocated SL2.
This function should be used to initialize variable of type Vhwa_M2mLdcInitParams.
VhwaM2mLdcCfg_Init
- Parameters
-
- Returns
- None
This function should be used to initialize variable of type Vhwa_M2mLdcCreateArgs.
Vhwa_M2mLdcCreateArgsInit
- Parameters
-
- Returns
- None