![]() |
MCUSW
|
This file contains interface header for WDG MCAL driver.
Go to the source code of this file.
Data Structures | |
| struct | Wdg_ModeInfoType |
| Mode info type. More... | |
| struct | Wdg_ConfigType |
| WDG config structure. More... | |
| struct | Wdg_ConfigType_PC |
| WDG pre-compile config structure. More... | |
| struct | Wdg_RegisterReadbackType |
Macros | |
WDG Driver Module SW Version Info | |
Defines for WDG Driver version used for compatibility checks | |
| #define | WDG_SW_MAJOR_VERSION (1U) |
| Driver Implementation Major Version. More... | |
| #define | WDG_SW_MINOR_VERSION (2U) |
| Driver Implementation Minor Version. More... | |
| #define | WDG_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
WDG Driver Module AUTOSAR Version Info | |
Defines for WDG Driver AUTOSAR version used for compatibility checks | |
| #define | WDG_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by WDG Driver. More... | |
| #define | WDG_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by WDG Driver. More... | |
| #define | WDG_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by WDG Driver. More... | |
WDG Driver ID Info | |
| #define | WDG_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. More... | |
| #define | WDG_MODULE_ID ((uint16) 102U) |
| WDG Driver Module ID. More... | |
| #define | WDG_INSTANCE_ID ((uint8) 0U) |
| WDG Driver Instance ID. More... | |
WDG Error Codes | |
Error codes returned by Driver functions | |
| #define | WDG_E_DRIVER_STATE ((uint8) 0x10U) |
| ERROR:Invalid driver state. More... | |
| #define | WDG_E_PARAM_MODE ((uint8) 0x11U) |
| ERROR:Invalid mode param. More... | |
| #define | WDG_E_PARAM_CONFIG ((uint8) 0x12U) |
| ERROR:Invalid config param. More... | |
| #define | WDG_E_PARAM_TIMEOUT ((uint8) 0x13U) |
| ERROR:Invalid timeout value. More... | |
| #define | WDG_E_PARAM_POINTER ((uint8) 0x14U) |
| ERROR:Invalid NULL ptr param. More... | |
| #define | WDG_E_INIT_FAILED ((uint8) 0x15U) |
| ERROR:Invalid configuration set selection. More... | |
WDG Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | WDG_API_INIT ((uint8) 0x00U) |
| Wdg_Init() More... | |
| #define | WDG_API_SET_MODE ((uint8) 0x01U) |
| Wdg_SetMode() More... | |
| #define | WDG_SET_TRIGGER_CONDITION ((uint8) 0x03U) |
| Wdg_SetTriggerCondition() More... | |
| #define | WDG_API_GET_VERSION_INFO ((uint8) 0x04U) |
| Wdg_GetVersionInfo() More... | |
| #define | WDG_API_TRIGGER ((uint8) 0x05U) |
| Wdg_Trigger() More... | |
| #define | WDG_API_REGISTER_READBACK ((uint8) 0x06U) |
| Wdg_RegisterReadback() More... | |
Watchdog Window Size | |
Windowed watchdog trigger window size define | |
| #define | WDG_WINDOW_100_PERCENT ((uint32) 0x00000005U) |
| Window open 100% of interval. More... | |
| #define | WDG_WINDOW_50_PERCENT ((uint32) 0x00000050U) |
| Window open 50% of interval. More... | |
| #define | WDG_WINDOW_25_PERCENT ((uint32) 0x00000500U) |
| Window open 25% of interval. More... | |
| #define | WDG_WINDOW_12P5_PERCENT ((uint32) 0x00005000U) |
| Window open 12.5% of interval. More... | |
| #define | WDG_WINDOW_6P25_PERCENT ((uint32) 0x00050000U) |
| Window open 6.25% of interval. More... | |
| #define | WDG_WINDOW_3P125_PERCENT ((uint32) 0x00500000U) |
| Window open 3.125% of interval. More... | |
Enumerations | |
| enum | Wdg_StatusType { WDG_UNINIT, WDG_IDLE, WDG_BUSY } |
| Watchdog driver state. More... | |
Functions | |
| void | Wdg_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. More... | |
| void | Wdg_Init (const Wdg_ConfigType *CfgPtr) |
| This service initializes the WDG driver. More... | |
| void | Wdg_SetTriggerCondition (uint16 timeout) |
| Sets the timeout value for the trigger counter. More... | |
| void | Wdg_Trigger (void) |
| This function triggers the servicing of the watchdog. More... | |
| Std_ReturnType | Wdg_RegisterReadback (Wdg_RegisterReadbackType *regRbPtr) |
| This function reads the important registers of the hardware unit and returns the value in the structure. More... | |