3.9.4. Arm NN and Arm Compute Library

3.9.4.1. Introduction

Arm NN and Arm Compute Library, as a set of machine learning software, tools and libraries, enable Machine Learning on Arm.

For Sitara devices without accelerators like C66x or EVE (AM3/4/6), one can use Arm provided libraries created for supporting inference only tasks on Arm CPUs. Arm NN and Arm Compute Library can also be used on AM57xx devices as well, as complementary approach to TIDL-API.

3.9.4.2. Supported versions

  • ARMNN 19.08
  • ARM Compute Library 19.08

3.9.4.3. Arm Compute Library

Arm Compute Library is a software library for computer vision and machine learning, optimized for NEON SIMD architecture (Mali GPU OpenCL is not applicable to TI devices). Exact list of functions can be found at https://developer.arm.com/technologies/compute-library. Arm Compute Libraries and sample executables are included in PLSDK filesystem. AM3/4/5/6 devices can utilize this library to unleash full potential of Arm CPUs.

Sample NN related executables (using Arm Compute Library only):

/usr/bin/graph2tree
/usr/bin/graph_alexnet
/usr/bin/graph_googlenet
/usr/bin/graph_inception_v3
/usr/bin/graph_inception_v4
/usr/bin/graph_lenet
/usr/bin/graph_mobilenet
/usr/bin/graph_mobilenet_qasymm8
/usr/bin/graph_resnet50
/usr/bin/graph_resnext50
/usr/bin/graph_squeezenet
/usr/bin/graph_squeezenet_v1_1
/usr/bin/graph_vgg16
/usr/bin/graph_vgg19

3.9.4.4. Arm NN

Arm NN is library built on top of Arm Compute Library leveraging its NEON optimized kernels. Importing of Caffe, ONNX, TensorFlow, and TensorFlow Lite inference models is significantly simplified. Library and executables are part of AM3/4/5/6 target filesystem. More information can be found at: https://developer.arm.com/products/processors/machine-learning/arm-nn

Sample Arm NN executables using Caffe models:

/usr/bin/CaffeAlexNet-Armnn
/usr/bin/CaffeCifar10AcrossChannels-Armnn
/usr/bin/CaffeInception_BN-Armnn
/usr/bin/CaffeMnist-Armnn
/usr/bin/CaffeResNet-Armnn
/usr/bin/CaffeVGG-Armnn
/usr/bin/CaffeYolo-Armnn

Sample executables using ONNX models:

/usr/bin/OnnxMnist-Armnn
/usr/bin/OnnxMobileNet-Armnn

Sample executables using TensorFlow models:

/usr/bin/TfCifar10-Armnn
/usr/bin/TfInceptionV3-Armnn
/usr/bin/TfMnist-Armnn
/usr/bin/TfMobileNet-Armnn
/usr/bin/TfResNext-Armnn

Sample executables using TensorFlow Lite models:

/usr/bin/TfLiteInceptionV3Quantized-Armnn
/usr/bin/TfLiteInceptionV4Quantized-Armnn
/usr/bin/TfLiteMnasNet-Armnn
/usr/bin/TfLiteMobileNetQuantizedSoftmax-Armnn
/usr/bin/TfLiteMobileNetSsd-Armnn
/usr/bin/TfLiteMobilenetQuantized-Armnn
/usr/bin/TfLiteMobilenetV2Quantized-Armnn
/usr/bin/TfLiteResNetV2-50-Quantized-Armnn
/usr/bin/TfLiteResNetV2-Armnn
/usr/bin/TfLiteVGG16Quantized-Armnn

3.9.4.5. Arm NN MobileNet Demo

Upon boot, Matrix-GUI is started with multiple icons that can start many out of box demos. Under sub-menu “Machine Learning”, there are two icons to start the Arm NN demos:

  • Arm NN MobileNet Real Common Objects
  • Arm NN MobileNet Camera Input

These examples demonstrate Deep Learning Imagenet classification (1000 classes) with MobileNet model on Arm. One example uses pre-recorded real-world video clip and the other uses live camera input. The pre-recorded video clip (320x320 resolution) and live camera input (default 640x480 resolution) are scaled down and central-cropped in run-time (using OpenCV API) to 224x224. Result of this processing is standard Imagenet classification output (1D vector with 1000 elements).

Executable invoked from the Matrix-GUI demos above is /usr/bin/ArmnnExamples, and the TensorFlow Lite parser is used.

Options of ArmnnExamples are listed below:

-f [ --model-format ] arg       caffe-binary, caffe-text, onnx-binary,
                                onnx-text, tflite-binary, tensorflow-binary
                                or tensorflow-text. E.g.: -f
                                tensorflow-binary
-m [ --model-path ] arg         Model Name w/ full path, e.g.of supported
                                model types: .caffemodel, .prototxt, .tflite,
                                .onnx. E.g.: -m /usr/share/arm/armnn/models/m
                                obilenet_v1_1.0_224_frozen.pb
-c [ --compute ] arg            The preferred order of devices to run layers
                                on by default. Possible choices: CpuAcc,
                                CpuRef, GpuAcc. E.g.: -c CpuAcc
-i [ --input-name ] arg         Identifier of the input tensor in the
                                network. E.g.: -i input
-s [ --input-tensor-shape ] arg The shape of the input tensor in the network
                                as a flat array of integers separated by
                                whitespace. This parameter is optional,
                                depending on the network. E.g.: -s '1 224 224 3'
-d [ --input-tensor-data ] arg  Input test file name. It can be image/video
                                clip file name or use 'camera_live_input' to
                                select camera input. E.g.: -d
                                /usr/share/arm/armnn/testvecs/camera_live_input
-o [ --output-name ] arg        Identifier of the output tensor in the
                                network. E.g.: -o MobilenetV1/Predictions/Reshape_1
--number_frame arg (=1)         Number of frames to process. E.g.:
                                --number_frame 100.

Here is an example of classification using live camera input - stop at any time with mouse right-click on output image window.

ArmnnExamples -f tflite-binary -i input -s '1 224 224 3' -o MobilenetV2/Predictions/Reshape_1 -d /usr/share/arm/armnn/testvecs/camera_live_input -m /usr/share/arm/armnn/models/mobilenet_v2_1.0_224.tflite -c CpuAcc --number_frame 100

Here is an example of classification using video clip - stop at any time with mouse right-click on output image window.

ArmnnExamples -f tflite-binary -i input -s '1 224 224 3' -o MobilenetV2/Predictions/Reshape_1 -d /usr/share/arm/armnn/testvecs/test2.mp4 -m /usr/share/arm/armnn/models/mobilenet_v2_1.0_224.tflite -c CpuAcc --number_frame 100

Here is an example of classification using JPG image - use “–number_frame” to select the number of runs.

root@am57xx-evm:/usr/bin# ArmnnExamples -f tflite-binary -i input -s '1 224 224 3' -o MobilenetV2/Predictions/Reshape_1 -d /usr/share/arm/armnn/testvecs/baseball.jpg -m /usr/share/arm/armnn/models/mobilenet_v2_1.0_224.tflite -c CpuAcc --number_frame 10
ArmNN v20190800

Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 7.57426
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.48181
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.46633
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.41803
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.3029
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.45797
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.45416
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.49093
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.33742
Top(1) prediction is 430:baseball with confidence: 69.5592%
Top(2) prediction is 575:golf ball with confidence:  0.307349%
Top(3) prediction is 474:can opener, tin opener with confidence:  0.248897%
Top(4) prediction is 884:vase with confidence:  0.196634%
Top(5) prediction is 130:spoonbill with confidence:  0.191194%
Performance (FPS): 9.4193