2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders & Filesystems
- SDK Installer
- Setup Scripts
- Makefiles
- Matrix Application Launcher
- Example Applications
- WLAN support (Wilink 8)
- Code Composer Studio
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see PLSDK GPLv3 Disclaimer
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 06.02.00¶
Released January 2020
What’s New
Processor SDK 6.2 Release is limited to AM5 and AM6 platforms w/ Linux OS, and has following new features:
- AM57x Networking:
- Support Standard Ethernet Switch over ICSS
- Support Rapid Spanning Tree Protocol (RSTP) w/ cut-through offloaded to ICSS Switch
- Support Telecomm profile (G.8275.2) Slave Mode on ICSS EMAC interface
- Support Early boot of IPUs, and late attach from ARM core. For more details see here
- AM65x:
- ICSSG PRUETH: Support 100M Link Speed full duplex operation, in addition to 1G
- Support SOC PRU PWM Interface
- Graphics
- Re-enable qtWebengine and Chromium browser support
- Upgrade SGX DDK to support all required EGL 1.5-based extensions with Mesa-EGL instead of the traditional IMG WSEGL.
- Both Wayland and GBM(DRM) window systems are supported by Mesa-based EGL while the nullDRM window system is dropped
- All the full-screen (EGLFS)-based applications have been updated to use GBM-based window system.
- Please refer to the Graphics and Display section at the developer guide for details. See here
SDK Components & Versions
| Component | Version |
|---|---|
| Linux Kernel | 4.19.79+ (2019 LTS) |
| U-Boot | 2019.01 |
| Yocto Project | 2.6 (thud) |
| ARM Toolchain (gcc) | 8.3 2019.03 hard-float |
| Qt | 5.11.3 |
| OpenCL | 1.1.19 |
| OpenCV | 3.1 |
| Wayland | 1.16 |
| GStreamer | 1.14.4 |
| TI PRU Compiler | 2.2.1 |
| TI C66x CGT Compiler | 8.3.2 |
2.1.5. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Generic Kernel Release Notes
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
| Record ID | Platform | Title |
|---|---|---|
| LCPD-16641 | am654x-evm, am654x-idk, am654x-hsevm, j721e-evm, j721e-evm-ivi | tidss: need to ensure the output width is divisible by 2 |
| LCPD-13587 | am57xx-evm | dwc3: g_audio can only record once |
| LCPD-16707 | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm, dra71x-evm, dra71x-hsevm, dra72x-evm, dra72x-hsevm, dra76x-evm, dra76x-hsevm, dra7xx-evm, dra7xx-hsevm | DRA7x: Off-by-one error while selecting OTV in tuning algorithm |
| LCPD-15821 | am654x-evm | AM6 tidss: 1680x1050 does not work with TC358767 |
| LCPD-17185 | am57xx-evm | U-Boot does not have Extended Mode Register support for the TI DP83867 PHY driver |
| LCPD-12470 | Analyze / fix klocwork warnings for TSCADC | |
| LCPD-15714 | [Klokworks uboot] Resolve or indicate false positives on drivers/usb/dwc3/gadget.c | |
| LCPD-15722 | [Klokworks uboot] Resolve or indicate false positives on drivers/usb/dwc3/core.c | |
| LCPD-16937 | am43xx-epos, am43xx-gpevm, am43xx-hsevm, am437x-idk, am437x-sk | U-Boot: usbhost boot failed on AM437x |
| LCPD-15241 | am437x-sk | am437x-sk failed boot to uboot prompt from QSPI |
| LCPD-16190 | am335x-evm, am43xx-gpevm, am57xx-evm, dra72x-evm, dra7xx-evm | NBench’s FP_Emulation benchmark is ~30% lower than expected |
| LCPD-15706 | [Klokworks] Resolve or indicate false positives on arch/arm/mach-omap2/omap_hwmod.c | |
| LCPD-15707 | [Klokworks] Resolve or indicate false positives on drivers/clk/ti/autoidle.c | |
| LCPD-15702 | [Klokworks] Resolve or indicate false positives on drivers/clk/ti/clockdomain.c | |
| LCPD-15727 | [Klokworks uboot] Resolve or indicate false positives on drivers/core/regmap.c | |
| LCPD-15717 | [Klokworks uboot] Resolve or indicate false positives on drivers/mtd/spi/spi-nor-core.c | |
| LCPD-15712 | [Klokworks uboot] Resolve or indicate false positives on drivers/net/ti/cpsw.c | |
| LCPD-15721 | [Klokworks uboot] Resolve or indicate false positives on drivers/thermal/ti-bandgap.c | |
| LCPD-16838 | am335x-ice, am437x-idk, am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am654x-idk | icss/icssg: prueth: PHY shouldn’t advertise flow control |
| PLSDK-3134 | am572x-evm | NEO-AI DLR cannot be imported on the target |
| PLSDK-2943 | am572x-evm | Browser app crashes if EVM is connected to Internet |
| PLSDK-3033 | am571x-idk,am572x-idk,am574x-idk | HSR mode PRP frames not forwarded |
| PLSDK-3150 | am654x-idk | icssg U-boot revert the interposer card related patches |
| PLSDK-3095 | am571x-idk,am572x-idk | If nsp_credit is set to 0 storm prevention should be disabled |
2.1.7.2. Issues found and closed on this release that may be applicable to prior releases¶
| Record ID | Platform | Title |
|---|---|---|
| PLSDK-3166 | am571x-idk | In switch mode ifconfig up then down of an interface causes kernel crash |
2.1.7.3. Errata Workarounds Available in this Release¶
| Record ID | Title |
|---|---|
| LCPD-5310 | i900: CTRL_CORE_MMR_LOCK_5 region after locking results in ctrl module inaccessible, recoverable only post a reset |
| LCPD-5311 | i893: DCAN ram init issues in HW AUTO and when traffic hitting CAN bus (open investigation) |
| LCPD-5309 | LCPD: i896: USB Port disable doesnt work |
| LCPD-7642 | MMC/SD: i832: return DLL to default reset state with CLK gated if not in SDR104/HS200 mode. |
| LCPD-4195 | J6: SATA: Investigate applicability of i807 |
| LCPD-4225 | J6: Errata: i834: Investigate possibility of software workaround |
| LCPD-976 | J6/J6eco: 32clk is psuedo (erratum i856) - clock source |
| LCPD-975 | J6/J6eco: 32clk is psuedo (erratum i856) - realtime counter |
| LCPD-1022 | J6: Errata: i694: System I2C hang due to miss of Bus Clear support @ OMAP level |
| LCPD-1188 | J6: Baseport: Errata i877: RGMII clocks must be enabled to avoid IO timing degradation due to Assymetric Aging |
| LCPD-9084 | i887: Software workaround to limit mmc3 speed to 64MHz |
| LCPD-16904 | PCIe: Unsupported request (UR) or Configuration Request Retry Status (CRS) in configuration completion response packets results in external abort |
| LCPD-5836 | CAL: Errata: i913: CSI2 LDO needs to be disabled when module is powered on |
| LCPD-5460 | Implement WA for Vayu errata i829 (Reusing Pipe Connected To Writeback Pipeline On The Fly To An Active Panel) |
| LCPD-5052 | Upstream: Post the dmtimer errata fix for i874 |
| LCPD-4910 | J6/OMAP5: errata i810 implementation |
| LCPD-4911 | DRA7: USB: Investigate applicability of Errata i897: StopEndpoint_issue |
| LCPD-4912 | DRA7: USB: Implement ErrataID_i896_PED_issue |
| LCPD-16363 | IO, MMCSD: Incorrect IO Power Supply Connectivity Prevent Dynamic Voltage Change on VDDSHV6 and VDDSHV7 |
| LCPD-16364 | MMCSD: Negative Current from UHS-I PHY May Create an Over-Voltage Condition on VDDS6 and VDDS7 which exposes the Device to a Significant Reliability Risk |
| LCPD-16538 | PCI-Express (PCIe) May Corrupt Inbound Data |
| LCPD-14184 | USB: SuperSpeed USB Non-Functional |
| LCPD-14187 | UDMA-P Real-time Remote Peer Registers not Functional Across UDMA-P Domains |
| LCPD-14185 | MSMC: Non-coherent memory access to coherent memory can cause invalidation of snoop filter |
| LCPD-14159 | The assertion of warm reset coinciding with a debug configuration access targeting the STM Subsystem may result in a hang of said debug configuration access |
| LCPD-13884 | CPTracer Bus Probes MAIN_CAL0_0 and MCU_SRAM_SLV_1 are not able to distinguish between secure and non-secure transactions |
| LCPD-13887 | DDR Controller ECC Scrubbing feature can cause DRAM data corruption |
| LCPD-4647 | [rpmsg 2015 LTS] Implement errata i879 - DSP MStandby requires CD_EMU in SW_WKUP |
| LCPD-4648 | [rpmsg 2014 LTS] Implement errata i879 - DSP MStandby requires CD_EMU in SW_WKUP |
| LCPD-4975 | DSS AM5/DRA7: implement WA for errata i886 |
| LCPD-14941 | RINGACC and UDMA ring state interoperability issue after channel teardown |
| LCPD-14579 | DSS : DSS Does Not Support YUV Pixel Data Formats |
| LCPD-14580 | DSS : DSS Does Not Support YUV Pixel Data Formats |
| LCPD-14578 | DSS : DSS DPI Interface does not support BT.656 and BT.1120 output modes |
| LCPD-14577 | CPSW does not support CPPI receive checksum (Host to Ethernet) offload feature |
| LCPD-8277 | u-boot: j6: SATA is not shutdown correctly as per errata i818 |
| LCPD-8294 | 37 pins + VOUT pins need slow slew enabled for timing and reliability respectively |
| LCPD-5308 | i897: USB Stop Endpoint doesnt work in certain circumstances |
| LCPD-6907 | Workaround errata i880 for RGMII2 is missing |
| LCPD-5931 | DRA7xx: AM57xx: mmc: upstream errata workaround for i834 |
| LCPD-5924 | ALL: CONNECTIVITY: CPSW: errata i877 workarround for cpsw |
| LCPD-4218 | Implement Workaround for Errata i813 - Spurious Thermal Alert Generation When Temperature Remains in Expected Range |
| LCPD-4217 | Implement Workaround for Errata i814 - Bandgap Temperature read Dtemp can be corrupted |
| LCPD-4184 | Implement workaround for errata i814 - Bandgap Temperature read Dtemp can be corrupted |
| LCPD-1146 | DMM hang: Errata VAYU-BUG02976 (i878) (register part) |
| LCPD-1087 | J6: MMC: Errata: i802: OMAP5430 MMCHS: DCRC errors during tuning procedure |
| LCPD-1108 | J6: Wrong Access In 1D Burst For YUV4:2:0-NV12 Format (Errata i631) |
| LCPD-876 | OMAP5: Errata i810: DPLL Controller Sticks when left clock requests are removed |
| LCPD-16605 | MMC: MMC1/2 Speed Issue |
| LCPD-17220 | U-Boot Hyperbus: Hyperflash reads limited to 125MHz max. frequency |
| LCPD-16643 | Hyperbus: Hyperflash reads limited to 125MHz max. frequency |
| LCPD-16350 | DSS: Frame Buffer Flip/Mirror Feature Using RGB24/BGR24 Packed Format can Result in Pixel Corruption |
| LCPD-9173 | i897: USB Stop Endpoint doesnt work in certain circumstances |
| LCPD-17333 | [CPTS] GENF (and ESTF) Reconfiguration Issue |
| LCPD-14186 | UDMA-P Host Packet Descriptors 0x3FFFFF Packet Length Mode not Functional |
| LCPD-1776 | [J6 SATA Adaptation] J6 - Errata i783, SATA Lockup After SATA DPLL Unlock/Relock |
| LCPD-941 | OMAP4,5: DSS: implement workaround for errata i740 |
| LCPD-1171 | DRA7: DMM errata i878 (framebuffer part) |
2.1.7.4. SDK Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-15810 | am335x-evm, am43xx-gpevm, k2g-evm | Illegal instruction reported when trying to decode h264 stream with gstreamer | None |
| PLSDK-1398 | k2e-evm, k2e-hsevm, k2g-hsevm, k2hk-hsevm | IPC demo hangs if run after OpenCL demos | Run IPC demo w/o running OpenCL first |
| PLSDK-1419 | k2l-evm | Intermittent-IP address display issue on LCD for K2L RT | Use ifconfig once Linux boots, to acquire IP address |
| PLSDK-2178 | am335x-ice, am437x-idk, am574x-idk | ICSS EMAC intermittent error in received acyclic packet content | None |
| PLSDK-2466 | am335x-ice, am437x-idk, am571x-idk, am572x-idk, k2g-ice | Fix Race condition in updating NSP credit value | None |
| PLSDK-2530 | am335x-ice, am437x-idk | AM3/4 PTP PPS fails intermittently | No complete workaround. Restarting the ethernet interface should reset PPS and likely resolve the issue temporarily. |
| PLSDK-2642 | am654x-idk | PRU Ethernet links on IDK Application board are unstable | IDK Limitation, requires re-work |
| PLSDK-2662 | am335x-ice, am437x-idk, am571x-idk, am572x-idk, am574x-idk, k2g-ice | HSR/PRP: Bringing down one slave port stops HSR/PRP interface | None |
| PLSDK-2861 | k2e-evm, k2g-evm, k2hk-evm, k2l-evm | Crypto is not functional on 2019 LTS | None |
| PLSDK-2873 | k2g-ice | K2G-ICE kernel warnings when removing PRUETH module | None |
| PLSDK-2895 | am571x-idk | AM571x-IDK: Icss Emac: TTS Port 1: Packet cyclic timestamp error. | None |
| PLSDK-2896 | k2e-evm, k2e-hsevm, k2hk-evm | mpm_transport_hyperlink_loopback: transport arm-loopback-hyplnk-0 failed (error: -114) retval -1001 | No workaround |
| PLSDK-2900 | am335x-evm, am437x-evm, k2e-evm, k2g-evm, k2hk-evm, k2l-evm | crypto examples are skipped from toplevel SDK Makefile, due to OpenSSL dependency | No workaround |
| PLSDK-2913 | am572x-idk | NetJury Test Failure: TC_PRP_4_3_4_____Reception_of_a_PRP_Supervision_frame_and_Nodes_Table - test_VLAN | No workaround |
| PLSDK-2936 | am572x-evm | jailhouse: failed in destroy cell | None |
| PLSDK-2937 | am572x-evm | jailhouse: ti-app demo doesn’t start | None |
| PLSDK-2960 | am571x-idk | HSR/PRP: Noticed 1 packet loss seen with UDP tests over 60 minute test | None |
| PLSDK-2989 | am335x-evm, am437x-evm, am437x-hsevm, am572x-evm, am572x-hsevm, k2e-evm, k2g-evm, k2l-evm, k2l-hsevm | defconfig build failure: reported diff | |
| PLSDK-3031 | am571x-idk, am572x-idk, am574x-idk | HSR: erroneous A-B forwarding of frames | |
| PLSDK-3032 | am571x-idk, am572x-idk, am574x-idk | HSR: forwarding of untagged frames in default mode H not according to IEC 62439-3:2016, 5.3.3 DANH receiving from an HSR port. | None |
| PLSDK-3057 | am335x-evm, am437x-evm, am572x-evm, am654x-evm, am654x-idk | ARMNN with TFLite parser: performance/accuracy issue with quantized mobilenet models | Patch from arm compute library https://review.mlplatform.org/c/ml/ComputeLibrary/+/1620/. |
| PLSDK-3071 | am571x-idk, am572x-evm, am572x-idk, am574x-idk | Dual camera demo: Overlapping of camera and stats panel due to big font size | None |
| PLSDK-3074 | am572x-idk | NetJury Test Failure: TC_PRP_4_2_4_____IP_addresses | None |
| PLSDK-3086 | am571x-idk, am572x-idk | Unable to handle kernel NULL pointer dereference when disabling HSR | None |
| PLSDK-3089 | am572x-evm, k2l-evm | openmpacc example test failed on am572x-evm and k2l-evm | |
| PLSDK-3091 | am572x-idk | Jailhouse: ICSS_EMAC_LLD test hangs during TTS tests on ICSS_EMAC_TEST_PRU2ETH0 and ICSS_EMAC_TEST_PRU2ETH1 | |
| PLSDK-3125 | am571x-idk, am572x-idk, am574x-idk | clean up timestamp queue when extts is disabled | |
| PLSDK-3128 | am572x-evm, am572x-hsevm, am572x-idk, am574x-hsidk, am574x-idk | SDK disk image for Windows users too large for 16GB SD card | |
| PLSDK-3138 | EtherCAT in Jailhouse inmate: instruction abort at 0x80013f00 | ||
| PLSDK-3143 | am335x-evm, am437x-evm, am437x-idk, am572x-evm, am572x-idk, am574x-idk | TVM inside PLSDK Linux devkit not working for code generation | |
| PLSDK-3147 | am654x-idk | ICSSG: < 0.01 packet loss at 3/4/4.5 Mbits/sec for 10M Half Duplex link | |
| PLSDK-3148 | am654x-idk | ICSSG: 10M/100M Half duplex doesn’t work with 10/100M Hub | |
| PLSDK-3151 | beagleboneblack | ArmnnExamples cannot run on BBB for usb camera input | |
| PLSDK-3152 | am654x-idk | 10M/100M EVM <——-> PC / H3C S5120V2: setup results in kernel errors and ping failures | |
| PLSDK-3157 | am654x-evm, am654x-idk, am654x-hsevm | ICSSG: Driver has to support changing of speed/duplex on the fly | |
| PLSDK-3171 | am335x-ice, am437x-idk, am571x-idk, am572x-idk, am574x-idk, k2g-ice | DualEMAC PTP IPv4/UDP transport does not support VLAN | |
| PLSDK-3172 | am335x-ice, am437x-idk, am571x-idk, am572x-idk, am574x-idk, k2g-ice | DualEMAC PTP IPv4/UDP transport does not drop SYNC messages from unknown PTP masters |
2.1.7.5. U-Boot Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-16524 | am654x-evm, am654x-idk, am654x-hsevm | Need to adjust RMW bit when using enabling ECC | None |
| LCPD-16103 | am654x-evm | AM6: MMC: Probe fail warning in bootloader | None |
| LCPD-15873 | am654x-evm | There is no dtbo in u-boot for PCIe x1 + usb3 daughter card | None |
| LCPD-15127 | am654x-evm | u-boot: net: Stop called even without start leading to crash | None |
| LCPD-15054 | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | [u-boot] AM57xx phy_ctrl structures must be board-specific | None |
| LCPD-14843 | am654x-evm, am654x-idk | U-boot should support default settings for netboot | None |
| LCPD-14638 | k2g-evm, k2g-ice | Invalid DDR_PHY_MR2 setting in K2G board library | None |
| LCPD-10726 | am572x-idk, am57xx-evm | Update DDR3 emif regs structure for EMIF2 for the beagle_x15 board in U-Boot board file | None |
| LCPD-10668 | k2g-evm | Ethernet boot: Sometimes the board could not boot uboot from Ethernet on k2g-evm | None |
| LCPD-7366 | am335x-evm | uboot McSPI driver drives multiple chip selects simultaneously | None |
2.1.7.6. Linux Kernel Known Issues¶
| Record ID | Priority | Title | Component | Subcomponent | Platform | Workaround | Impact |
|---|---|---|---|---|---|---|---|
| LCPD-17648 | P2-High | ICSSG: Periodic packet loss seen at as low as 30Mbits/sec over 100M Full Duplex Link | Connectivity | am654x-idk | Use rate of 20Mbits/sec for 0 packet loss | ||
| LCPD-17305 | P2-High | ICSSG PRUETH: kernel crash when eth1 & eth3 connected and ifconfig up/down | Connectivity | am654x-idk | |||
| LCPD-16877 | P3-Medium | ti-ipc-examples-linux intermittent build failure | IPC, System Integration | k2hk-evm | |||
| LCPD-17517 | P3-Medium | Platform can’t suspend due to IPU failing to suspend | IPC | am57xx-evm | |||
| LCPD-16534 | P3-Medium | remoteproc/k3-r5f: PDK IPC echo_test image fails to do IPC in remoteproc mode on second run | IPC | Firmware | am654x-evm, am654x-idk | None | |
| LCPD-17779 | P3-Medium | UART Read/Write tests fail | Connectivity | UART | am57xx-evm, am654x-evm, dra7xx-evm, k2g-evm | ||
| LCPD-17529 | P3-Medium | Could not access usbhost when booting from SD card | Connectivity | am43xx-gpevm | |||
| LCPD-17482 | P3-Medium | Linux spi-ti-qspi driver does not properly support multiple MTD devices | Connectivity | SPI | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm | ||
| LCPD-17475 | P3-Medium | Update PRUETH Single EMAC Bindings Documentation | Connectivity | am335x-ice, am437x-idk, am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am654x-idk, k2g-ice | |||
| LCPD-17472 | P3-Medium | Missing commit b5376be4f in kernel 4.19 for K2E/L system hung caused by ethernet cable unplugged | Connectivity | k2e-evm, k2l-evm | |||
| LCPD-17470 | P3-Medium | CPSW: Still seeing multicast packets with promisc and allmulti disabled | Connectivity | am654x-evm, j721e-idk-gw | |||
| LCPD-17441 | P3-Medium | TI_CPSW Module cannot be removed and reinserted | Connectivity | am57xx-evm | |||
| LCPD-17420 | P3-Medium | AM65x: MCU_UART lockup due to udma teardown timeout | Connectivity | UART | am654x-evm | ||
| LCPD-17329 | P3-Medium | K2E RT-Linux USB fails when using USB-Ethernet dongle to scp file (512MB) | Connectivity | USB | k2e-evm | ||
| LCPD-17118 | P3-Medium | Kernel MMC/SD user’s guide incorrectly refers to OMAP-HSMMC | Connectivity | MMCSD | am57xx-evm, dra7xx-evm | None | |
| LCPD-16590 | P3-Medium | am335x: usb bus power lost after system suspend resume | Connectivity | usb | am335x-evm, am335x-sk, beaglebone-black | ||
| LCPD-16406 | P3-Medium | Seeing “e1000#0: ERROR: Hardware Initialization Failed” sometimes when do dhcp via pcie-eth | Connectivity | am654x-idk | |||
| LCPD-16029 | P3-Medium | AM65: icssg: PRU ethernet links might be unstable with new PHY package | Connectivity | PRUSS-Ethernet | am654x-evm, am654x-idk, am654x-hsevm | ||
| LCPD-15952 | P3-Medium | DCAN Documentation incorrect | Connectivity | am335x-evm | None | ||
| LCPD-15885 | P3-Medium | Uboot usb start trigger the board resetting with one usb stick | Connectivity | k2hk-evm | |||
| LCPD-15787 | P3-Medium | Power suspend fails due to USB (scsi_bus_suspend) failure when HDD is in use | Connectivity | am335x-evm | |||
| LCPD-15737 | P3-Medium | AM65x: MMC OTAPDLY values must match values in the Data Manual | Connectivity | MMCSD | am654x-evm, am654x-idk | ||
| LCPD-15660 | P3-Medium | pcie sata or usb drive no device node being created | Connectivity | k2g-evm | |||
| LCPD-15649 | P3-Medium | Uboot: sata could not be detected | Connectivity | am57xx-evm | |||
| LCPD-15540 | P3-Medium | uvc-gadget results in segmentation fault | Connectivity | am57xx-evm, am654x-evm, dra71x-evm, dra7xx-evm | |||
| LCPD-15515 | P3-Medium | PCI: Endpoint: MSIX interrupts do not work on AM654 | Connectivity | PCIe | am654x-evm | ||
| LCPD-15405 | P3-Medium | DFU: could not update eMMC bootloaders when using dfu_alt_info_emmc set in uboot env | Connectivity | am57xx-evm, dra71x-evm, dra7xx-evm | |||
| LCPD-15365 | P3-Medium | warning dump in fs/nfs/inode.c seen sometimes | Connectivity | CPSW | am654x-evm | ||
| LCPD-14855 | P3-Medium | omap_i2c_prepare_recovery() function can Lock System | Connectivity | I2C | am335x-evm, am335x-ice, am335x-sk | ||
| LCPD-14842 | P3-Medium | musb: unplug usb-serial device cause console lockup | Connectivity | USB | am335x-evm, am335x-sk, beaglebone-black | ||
| LCPD-14511 | P3-Medium | AM65x: Soft reset fails when booting from eMMC | Connectivity | MMCSD | am654x-evm, am654x-idk | ||
| LCPD-14497 | P3-Medium | PCIe Gen3 problems on AM654x | Connectivity | am654x-evm, am654x-idk | |||
| LCPD-14460 | P3-Medium | am654x-idk failed to boot to kernel prompt occasionally | Connectivity | am654x-idk | |||
| LCPD-14171 | P3-Medium | Failed to read uboot from SD card 1/1000 times | Connectivity | am57xx-evm, dra7xx-evm | |||
| LCPD-13936 | P3-Medium | Uboot dhcp timeout 1 of 100 times | Connectivity | am654x-evm | |||
| LCPD-13720 | P3-Medium | SPI DMA TX Mode Halts During Continuous 16/32/64 bit Transfers | Connectivity | beaglebone-black | |||
| LCPD-13452 | P3-Medium | USB Gadget Camera Capture - guvcview causes kernel oops | Connectivity | k2g-evm | |||
| LCPD-13445 | P3-Medium | Seldom kernel oops triggered by prueth_netdev_init | Connectivity | am654x-evm | |||
| LCPD-11952 | P3-Medium | AM57x: disabling USB super-speed phy in DT causes kernel crash | Connectivity | USB | am571x-idk, dra72x-evm | ||
| LCPD-11564 | P3-Medium | AM57xx-evm: eth1 1G connection failure to netgear switch | Connectivity | CPSW, ETHERNET, PHYIF | am57xx-evm | ||
| LCPD-10974 | P3-Medium | am43xx-gpevm - usb camera gadget shows halting frames | Connectivity | USB | am43xx-gpevm | None | |
| LCPD-9905 | P3-Medium | AM437x: UART: Implement workaround for Advisory 27 - Spurious UART interrupts when using EDMA | Connectivity | UART | am43xx-gpevm | ||
| LCPD-9366 | P3-Medium | PCIe USB drive sometimes could not be enumerated | Connectivity | PCIe | k2g-evm | ||
| LCPD-7623 | P3-Medium | Seeing SPI transfer failed error sometimes on k2hk when using rt kernel | Connectivity | SPI | k2hk-evm | ||
| LCPD-1106 | P3-Medium | Connectivity:PCIe-SATA ext2 1G write performance is poor due to ata failed command | Connectivity | PCIe | am57xx-evm, dra71x-evm, dra71x-hsevm, dra72x-evm, dra72x-hsevm, dra7xx-evm, dra7xx-hsevm | None | |
| LCPD-17673 | P3-Medium | No software documentation for the Timer module | Baseport | Timers | am335x-evm, am43xx-gpevm, am571x-idk, am572x-idk, am574x-idk, am57xx-evm, am654x-evm, beaglebone-black, dra71x-evm, dra72x-evm, dra7xx-evm, j721e-evm | ||
| LCPD-17422 | P3-Medium | Disabling IRQ #64 message observed sometimes | Baseport | am654x-evm, am654x-hsevm | |||
| LCPD-16845 | P3-Medium | OPP freq update in DT impacts only cluster0 | Baseport | am654x-evm, am654x-idk | |||
| LCPD-14191 | P3-Medium | IPSec hardware-based throughput is 30% lower than 2018.03 | Baseport | am335x-evm, am57xx-evm | |||
| LCPD-16642 | P3-Medium | omapdrm: in some cases, DPI output width does not need to be divisible by 8 | Audio & Display | Display | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm, dra71x-evm, dra71x-hsevm, dra72x-evm, dra72x-hsevm, dra76x-evm, dra76x-hsevm, dra7xx-evm, dra7xx-hsevm | ||
| LCPD-15819 | P3-Medium | tidss: the driver should reject dual-display setup, as it is not supported | Audio & Display | Display | am654x-evm | ||
| LCPD-15518 | P3-Medium | omapdrm: WB M2M: Headless mode is not working | Audio & Display | Writeback | am571x-idk, am572x-idk, am574x-idk, am574x-hsidk, am57xx-evm, am57xx-beagle-x15, am57xx-hsevm, dra71x-evm, dra71x-hsevm, dra72x-evm, dra72x-hsevm, dra76x-evm, dra76x-hsevm, dra7xx-evm, dra7xx-hsevm | ||
| LCPD-15402 | P4-Low | rpmsg-rpc: test application does not bail out gracefully upon error recovery | IPC | DSP_remoteproc, IPU_remoteproc | am571x-idk, am572x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15, dra71x-evm, dra72x-evm, dra76x-evm, dra7xx-evm | ||
| LCPD-15400 | P4-Low | remoteproc/omap: System suspend fails for IPU1 domain without any remoteprocs loaded | IPC | IPU_remoteproc | am571x-idk, am572x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15, dra71x-evm, dra72x-evm, dra76x-evm, dra7xx-evm | ||
| LCPD-10455 | P4-Low | remoteproc/keystone: Hang observed while running RPMSG_PROTO example app | IPC | DSP_remoteproc | k2g-evm, k2g-ice, k2hk-evm, k2l-evm | ||
| LCPD-9481 | P4-Low | Sometime the system hangs while loading the rpmsg rpc modules | IPC | RPMSG-RPC | am571x-idk, am572x-idk, am57xx-evm, am57xx-hsevm | ||
| LCPD-7495 | P4-Low | Sometimes a Kernel Warning + Oops is seen when removing keystone_remoteproc module | IPC | k2hk-evm | |||
| LCPD-4855 | P4-Low | [rpmsg 2015 LTS] J6Eco: IPC: Board hangs when an MMU fault occurs in the first message | IPC | am572x-idk, dra72x-evm | |||
| LCPD-4699 | P4-Low | [rpmsg 2015 LTS] rpmsg-rpc: kernel crash during error recovery with dynamic debug traces enabled | IPC | am571x-idk, am572x-idk, am57xx-evm, dra72x-evm, dra7xx-evm | |||
| LCPD-17116 | P4-Low | AM335x rmii2_crs_dv is not being muxed in due to SMA rmii2_crs_dv_sel not set | Connectivity | am335x-evm | |||
| LCPD-16437 | P4-Low | Nand with prefetch dma: read perf drop ~20% comparing to 2018 | Connectivity | am335x-evm | |||
| LCPD-15648 | P4-Low | Uboot mmc performance decreased | Connectivity | am335x-evm | |||
| LCPD-12783 | P4-Low | Missing instruction for pcie-ep config on k2g-evm for 4.19 kernel | Connectivity | k2g-evm | |||
| LCPD-12392 | P4-Low | USBhost video: higher resolution tests fail with some cameras | Connectivity | am335x-evm | |||
| LCPD-6075 | P4-Low | BUG: using smp_processor_id() in preemptible [00000000] code during remoteproc suspend/resume | Baseport, IPC | am572x-idk, am57xx-evm, dra7xx-evm | |||
| LCPD-9098 | P4-Low | Writeback: error prints seen when doing wb capture | Audio & Display | Capture, Display, Writeback | am571x-idk, am572x-idk, am57xx-evm, dra71x-evm, dra71x-hsevm, dra72x-evm, dra72x-hsevm, dra7xx-evm, dra7xx-hsevm |
2.1.7.7. RT Linux Kernel Known Issues¶
| Record ID | Priority | Title | Component | Platform | Workaround |
|---|---|---|---|---|---|
| LCPD-6663 | P3-Medium | [RT] Kmemleak is buggy and boot is crashed randomly | Baseport | ||
| LCPD-7623 | P3-Medium | Seeing SPI transfer failed error sometimes on k2hk when using rt kernel | Connectivity | k2hk-evm | |
| LCPD-11586 | P3-Medium | dhcp failed to get IP address after reboot for K2G-ICE non-RT linux | Baseport | k2g-ice |
Installation and Usage
The Software Developer’s Guide provides instructions on how to setup up your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications and Code Composer Studio.
Host Support
The Processor SDK is developed, built and verified on Ubuntu 16.04 and 18.04. Details on how to create a virtual machine to load Ubuntu are described in this page.
Note
Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines