6.2.6. Taking the C66x Out Of Reset with Linux Running on the ARM A15¶
How to take the C66x DSP out of reset with Linux running on A15
This document describes the procedure to bring the C66x core out of reset after booting Linux, or at the u-boot prompt. These steps are necessary in to order to load an application on the C66x core, without interfering with the operation of Linux running on the A15.
NOTE Prior to proceeding with the below instructions, please ensure that the latest Emulation package is downloaded/installed through CCS. This will ensure the GEL files in your machine has the reset routines described below.
- Once Linux has booted, launch the target configuration.
![../../../_images/Outofreset_4_lali.png](../../../_images/Outofreset_4_lali.png)
![../../../_images/Outofreset_5_lali.png](../../../_images/Outofreset_5_lali.png)
![../../../_images/Outofreset_6_lali.png](../../../_images/Outofreset_6_lali.png)
![../../../_images/Outofreset_7_lali.png](../../../_images/Outofreset_7_lali.png)
NOTE Once the DSP core is connected following the above out of reset routine, the DDR and PLL settings done by u-boot would be overwritten by what’s in the GEL. In order to avoid this, please ensure that the gel is NOT preloaded on the DSP core in the ccxml by leaving the initialization script blank.