3.4. Filesystem¶
Introduction
Filesystem Images
There are four filesystem images provided in the SDK. You’ll find them at the SDK Installation directory/filesystem folder.
arago-base-tisdk-image
tisdk-rootfs-image
This is the complete filesystem image, that contains standard Linux commands and features. This also contains the TI component libraries, binaries and out of box examples. For keystone devices (e.g., K2H/K2K, K2E, K2L, and K2G), two filesystem tarballs are provided due to size limit of the rootfs ubi image:
- tisdk-server-rootfs-image-k2g-evm.tar.gz: base filesystem image used to create the ubi image.
- tisdk-server-extra-rootfs-image-k2g-evm.tar.gz: complete filesystem image that can be used with NFS and/or SD card (K2G only).
tisdk-docker-rootfs-image
This is a minimal image with support for Docker. See Docker Linux Container Runtime for more information.
arago-tiny-image
This is the absolute minimal filesystem. The boot files are omitted from this image and systemd has been replaced with sysvinit.