3.1.2.7. UART
This section documents how to use the UART to load files to boot the board into U-Boot. After that the user is expected to know how they want to continue loading files.
3.1.2.7.1. Booting U-Boot from the console UART
In some cases we support loading SPL and U-Boot over the console UART.
You will need to use the tiboot3.bin, tispl.bin and u-boot.img files to boot.
As per the TRM, the file is to be loaded via the X-MODEM
protocol at 115200 baud 8 stop bits no parity (same as using it for
console). SPL in turn expects to be sent u-boot.img at the same rate
but via Y-MODEM. An example session from the host PC, assuming console
is on ttyUSB0 and already configured would be and the lrzsz package
is installed
In K3 based platforms, ROM supports booting from MCU_UART0 via X-Modem protocol. The entire UART-based boot process up to U-Boot (proper) prompt goes through different stages and uses different UART peripherals as follows:
WHO |
Loading WHAT |
HW Module |
Protocol |
|---|---|---|---|
Boot ROM |
tiboot3.bin |
MCU_UART0 |
X-Modem |
R5 SPL |
sysfw.itb |
MCU_UART0 |
Y-Modem |
R5 SPL |
tispl.bin |
MAIN_UART0 |
Y-Modem |
A53/A72 SPL |
u-boot.img |
MAIN_UART0 |
Y-Modem |
UART_BOOT_MAIN_UART and UART_BOOT_MCU_UART should be set to serial ports such as /dev/ttyUSBx.
$ sb --xmodem $OUT_R5/tiboot3.bin > $UART_BOOT_MCU_UART < $UART_BOOT_MCU_UART
$ sb --ymodem $SYSFW_ITB > $UART_BOOT_MCU_UART < $UART_BOOT_MCU_UART
$ sb --ymodem $OUT_AXX/tispl.bin > $UART_BOOT_MAIN_UART < $UART_BOOT_MAIN_UART
$ sb --ymodem $OUT_AXX/u-boot.img > $UART_BOOT_MAIN_UART < $UART_BOOT_MAIN_UART