3.6.3.2. RPMsg¶
3.6.3.2.1. Introduction¶
RPMsg is a method of passing messages and data between the PRU cores and the ARM core running Linux. RPMsg is enabled by a combination of remoteproc and the virtio framework.
3.6.3.2.1.1. Supported Devices¶
Linux ARM to PRU RPMsg communication is supported on these processors:
AM335x
AM437x
AM572x
AM65x
K2G
3.6.3.2.1.2. Supported SDK Versions¶
Linux RPMsg communication with PRU cores is supported up through TI’s Linux kernel 5.4 releases (Linux Processor SDK 7.x). Linux RPMsg communication with PRU cores was not implemented on Linux Processor SDK 8.0.
RPMsg
RPMsg is a message passing mechanism that requests resources through remoteproc and builds on top of the virtio framework. Shared buffers are requested through the resource_table and provided by the remoteproc module during PRU firmware loading (as shown in the remoteproc procedure above). The shared buffers are contained inside a vring data structure in DDR memory. There are two vrings provided per PRU core, one vring is used for messages passed to the ARM and the other vring is used for messages received from the ARM. System level mailboxes are used to notify cores (ARM or PRU) when new messages are waiting in the shared buffers.
There are two RPMsg software implementations provided in the Linux Processor SDK. On the ARM Linux side, RPMsg communication is received in kernel space. An interface module is provided (rpmsg_pru) that creates a character device in user space so that users can write/read to/from a character device in the file system to send/receive messages to/from the PRUs. On the PRU side, an RPMsg library is provided in the PRU Software Support Package that aims to abstract the communication to a point where a user’s code can just call the pru_rpmsg_receive and pru_rpmsg_send functions in order to communicate with the ARM core. Source code for the PRU RPMsg library is provided in the support package along with the ability to rebuild the library if changes are desired.
ARM to PRU
The diagram to the right shows the process that occurs when the ARM sends a message to the PRU. These steps are shown for illustrative purposes as the provided software in the SDK hides them in an abstraction layer.
ARM Host Steps
Step 1a: Allocate a new buffer -or-
Step 1b: Get a Used buffer from the slave Vring
Step 2: Copy data to be transferred into the buffer from Step 1
Step 3: Add the newly filled buffer to the Available list in the slave Vring
Step 4: Kick the slave Vring by writing its index (1) into a message in Mailbox 2
PRU Steps
Step 5: A Kick is discovered in Mailbox 2 with the index of the Kicked Vring (1). This indicates to the PRU that data is available for receive
Step 6: Get the Available buffer from the slave Vring
Step 7: Copy data to be received out of the buffer from Step 2
Step 8: Add the now empty buffer to the Used list in the slave Vring
Step 9: Kick the slave Vring by writing its index (1) into a message in Mailbox 3
PRU to ARM
The diagram to the right shows the process that occurs when the PRU sends a message to the ARM. These steps are shown for illustrative purposes as the provided software in the SDK hides them in an abstraction layer.
PRU Steps
Step 1: Get an Available buffer from the host Vring
Step 2: Copy data to be transferred into the buffer from Step 1
Step 3: Add the newly filled buffer to the Used list in the host Vring
Step 4: Kick the host Vring by writing its index (0) into a message in Mailbox 3
ARM Host Steps
Step 5: An interrupt signals that Mailbox 3 was kicked with the index of Vring (0). This indicates to the ARM Host that data is available for receive
Step 6: Get the Used buffer from the host Vring
Step 7: Copy data to be received out of the buffer from Step 2
Step 8: Add the now empty buffer to the Available list in the host Vring
Step 9: Kick the host Vring by writing its index (0) into a message in Mailbox 2
RPMsg PRU Code Example
Next Steps
To get started quickly with remoteproc and RPMsg you can use the RPMsg Quick Start Guide.
For Hands-on Labs that work with the BeagleBone Black and a PRU Cape take a look at PRU Hands-on Labs.