2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the yocto-build/configs/processor-sdk-linux
directory.
Config File |
Description |
Supported machines |
---|---|---|
processor-sdk-linux-08_00_00.txt |
Processor SDK Linux 08_00_00 Release |
am65xx-evm |