2.4. CoreSDK Linux Migration Guide¶
Overview
This page covers migration information for applications built on top of the Processor SDK for Linux.
2.4.1. Processor CoreSDK 08.xx Releases¶
2.4.1.1. Processor CoreSDK 08.00¶
This is the first release in the 2021 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch.`
First release on 5.10 kernel and 2021.01 U-boot
ATF 2.5
OPTEE 3.12
Yocto Dunfell/3.1
Platforms Supported : AM654x , J721E, J7200, AM64xx
Memory layout of bootloaders in eMMC and OSPI have been changed for J7200