3.6.3.5. PRU-ICSSG PWM¶
Introduction
The PRU_ICSSG subsystem integrates one PWM module, which uses IEP0 and IEP1 compare events to generates PWM outputs.
The PRU_ICSSG PWM module is supported as of in Processor SDK Linux v6.2 for AM65x. The linux PRU PWM driver models the PWM module as two pwmchips, each supports up to 12 PWMs through PRU-ICSSG GPIO pins. The PWM function is implemented in PRU firmware.
PRU PWM Features
Up to 24 PWMs are supported per PRU-ICSSG with the following features:
- Each pwmchip (IEP) supports up to 12 PWMs
- support Single-Ended mode
- PWM period range: 40us ~ 2sec
- PWM duty-cycle range: 400ns ~ (period - 400ns)
PRU PWM Unsupported Features
The following features are not supported in PRU PWM:
- Complementary mode
- Invert polarity (Active Low)
PRU PWM driver Kernel Config
The PRU PWM Linux kernel driver depends on the PRU-ICSS kernel driver. So the following kernel Kconfig options should be enabled to use the PRU PWM module.
Device Drivers --->
SOC (System On Chip) specific Drivers --->
[*] TI SOC drivers support --->
<M> TI PRU-ICSS Subsystem Platform drivers
Device Drivers --->
Pulse-Width Modulation (PWM) Support --->
PRU-ICSS PWM support
PRU PWM Sysfs Usage
The PRU PWM Linux kernel driver is integrated in the kernel PWM framework, so user space application can access the PWMs via the Linux sysfs entries. For details of the usage, please refer to PWM Driver Usage.
Notes
The 12 PWMs within a pwmchip (IEP) share the common PWM period setting. So only the PWM which first sets the PWM period (period ownner) has the permission to modify the PWM period setting. Other PWMs within the same pwmchip cannot modify the PWM period until the application deallocated the “period owner” PWM.