2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.

To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :

  • Platform/board-support software and configuration files for Linux

  • U-Boot and Kernel sources and configuration files

  • An ARM cross-compiling toolchain as well as other host binaries and components

  • A Yocto/OE compliant filesystem and sources for example applications

  • A variety of scripts and Makefiles to automate certain tasks

  • Other components needed to build an embedded system that don’t fit neatly into one of the above buckets

  • Reference Examples, benchmarks

This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide

2.1.2. Release versioning scheme

Processor SDK releases follow the 5-duplet versioning scheme YY.RR.EE.CC.SS, where:

  • YY - Yearly baseline. Increments with each new LTS baseline.

  • RR - Release index within the yearly baseline. Each yearly baseline includes many stable releases.

  • EE - Extended release index within a stable baseline.

  • CC - Release Candidate for common foundational BSP components such as Linux, U-Boot, ATF, OPTEE, Firmware and OE manifest including meta-ti, meta-arago.

  • SS - SDK Release identifier for Distro layers (Yocto meta-tisdk, Armbian, Buildroot) with OOB Demos and Installers.

2.1.3. Licensing

Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.

2.1.4. Software Bill of Materials (SBOM)

Processor SDK AM64x releases include Software Bill of Materials (SBOM) files in SPDX 3.0 format by default. SBOMs for all released artifacts are bundled into a single archive and can be found on the AM64x-SDK-Download-page. For more refer Working with SBOM.

2.1.5. Release 12.00.00.07.04

Released on Apr 2026

2.1.5.1. What’s new

Processor SDK Linux AM64X Release has following new features:

  • First 2026 LTS Reference Release Including RT combined branch model

  • Important Bug Fixes on top of Processor SDK 11.02.08.02 Release

  • Review Issue Tracker Section for the new fixes.

  • Security: ATF and OPTEE memory firewall for isolation from Linux

Key Release References:

Component version:

  • Kernel 6.18.13

  • U-Boot 2026.01

  • Toolchain GCC 15.2

  • ATF 2.14+

  • OPTEE 4.9.0+

  • TIFS Firmware v12.00.02 (Click on the link for more information)

  • Yocto Master

  • Security: Post Quantum Cryptography using Module Lattice (ML) Key Encapsulation Mechanism (KEM) or ML-KEM, ML Digital Signature Algorithm (DSA) or ML-DSA, and Stateless Hash-Based (SLH) DSA or SLH-DSA - Post Quantum Cryptography

2.1.6. Build Information

2.1.6.1. Arago (Yocto/OE)

Component

Branch Info

Tag Info

Config Info

U-Boot

ti-u-boot-2026.01

12.00.00.07

Build Config

TF-A

master

v2.14+

OPTEE

master

4.9.0+

k3-am64x

Linux Firmware

ti-linux-firmware

12.00.00.07

Linux Kernel

ti-linux-6.18.y

12.00.00.07

non-RT , RT

meta-ti

master

12.00.00.07

am64xx-evm

meta-arago

master

12.00.00.07

meta-tisdk

master

12.00.00.07.04

2.1.6.2. Debian (Armbian)

Component

Branch Info

Tag Info

Config Info

U-Boot

ti-u-boot-2026.01

12.00.00.07

Build

TF-A

master

v2.14+

Build

OPTEE

master

4.9.0+

Build

Linux Firmware

ti-linux-firmware

12.00.00.07

Git Clone

Linux Kernel

ti-linux-6.18.y

12.00.00.07

non-RT, RT

Armbian Build

2026.04-release

12.00.00.07.04

Board: SK-AM64B

2.1.7. Issues Tracker

Note

  • Release Specific Issues including details will be published through Software Incident Report (SIR) portal

  • Further Information can be found at SIR Portal <https://sir.ext.ti.com/>

2.1.7.1. Errata Resolved

Record ID

Title

EXT_EP-12122

USB2 PHY locks up due to short suspend

EXT_EP-12123

USART: Erroneous clear/trigger of timeout interrupt

EXT_EP-12114

MMCSD: HS200 and SDR104 Command Timeout Window Too Small

2.1.7.2. Issues Resolved

Record ID

Title

EXT_EP-13313

PRUETH: 100M Link fails if auto negotiation disabled

EXT_EP-13131

MMCSD: PHY DLL frequency is setting incorrectly for any clock < 200MHz

2.1.7.3. Issues Open

Record ID

Title

EXT_EP-13331

am64x: incorrect device id in icssg0_mdio devicetree node

EXT_EP-12051

AM64x: DFU Boot hangs on repetitive test

EXT_EP-13306

ICSSG: HSR packet out of order

EXT_EP-13309

U-Boot binman does not have the provision of SWREV for Board Configurations

EXT_EP-13310

Docs: Incorrect secure boot flow description

EXT_EP-12819

AM64x CICD does not test PRU

EXT_EP-12818

PRU RPMsg swaps which message is sent to which core

EXT_EP-12749

cdns: device mode: Linux hangs when USB cable is disconnected

EXT_EP-12060

AM64x: Lower core count on variant devices no supported