2.2. Yocto Layer ConfigurationΒΆ

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>


The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File Description Supported machines/platforms
processor-sdk-08.00.00.21-config.txt Processor SDK 08.00.00.21 Release am64xx-evm