4. Building Buildroot Packages
This document provides a step-by-step guide to building a Buildroot package. There are two ways you can build a package in buildroot.
Add existing Buildroot Packages
Add custom Packages
4.1. Adding Existing Buildroot Packages
4.1.1. Set Up Your Environment
Ensure you have the Buildroot repository and the buildroot-external-TI tree set up as described here Setting up the External Tree.
4.1.2. Enable Packages in the Buildroot Configuration
Run make menuconfig to enable the packages you have added in the Buildroot configuration.
$ make menuconfig
Navigate to the relevant package categories and enable the desired packages. For nano and htop, you would typically find them under the Target packages menu.
Go to Target packages.
Navigate to Text editors and viewers and enable nano.
Navigate to System tools and enable htop.
Save and exit the menuconfig interface.
4.1.3. Build the Image
With the packages configured, you can now build the image. Buildroot will download, compile, and include the specified packages in the build process.
$ make
The build process can take some time, depending on your system’s resources and the complexity of the configuration.
4.1.4. Verify the Packages
After the build process is complete, verify that the packages are included in the output image. You can check the presence of the package binaries in the root filesystem.
$ find output/target -name nano
$ find output/target -name htop
You should see the paths to your package binaries, indicating that they were successfully included in the build.
By following these steps, you can add existing Buildroot packages. This approach allows you to leverage the extensive package repository of Buildroot.
4.2. Adding Custom Packages
4.2.1. Set Up Your Environment
Ensure you have the Buildroot repository and the buildroot-external-TI tree set up as described here Setting up the External Tree.
4.2.2. Understand the Package Directory Structure
In Buildroot, packages are typically organized into categories under the
package/directory. When using an external tree, you can add new packages
under the package/directory of the external tree.
4.2.3. Create the Package Directory
Inside the buildroot-external-TI directory, create a new directory for your package. For example, if you want to add a package named myapp:
$ cd buildroot-external-TI/
$ mkdir -p package/myapp
4.2.4. Create the Package Files
In the myapp directory, you need to create several files:
Config.in: Describes the configuration options for the package.
myapp.mk: Contains the build instructions for the package.
Example Config.in:
config BR2_PACKAGE_MYAPP
bool "myapp"
help
MyApp is an example application.
Example myapp.mk
MYAPP_VERSION = 1.0
MYAPP_SITE = http://example.com/downloads
MYAPP_SOURCE = myapp-$(MYAPP_VERSION).tar.gz
define MYAPP_BUILD_CMDS
$(MAKE) -C $(@D)
endef
define MYAPP_INSTALL_TARGET_CMDS
$(INSTALL) -D -m 0755 $(@D)/myapp $(TARGET_DIR)/usr/bin/myapp
endef
$(eval $(generic-package))
4.2.5. Add the Package to Buildroot Configuration
Edit the Config.in file in the buildroot-external-TI directory to include your new package. Add the following line:
$ source "$BR2_EXTERNAL_TI_PATH/package/myapp/Config.in"
Also edit external.mk to include package mk file
$ include $(sort $(wildcard $(BR2_EXTERNAL_TI_PATH)/package/*/*.mk))
4.2.6. Enable the Package in the Configuration
Run make menuconfig in the buildroot directory to enable your new package in the Buildroot configuration.
$ cd buildroot/
$ make menuconfig
Navigate to your package in the External Options menu and enable it. Save and exit the menuconfig interface.
4.2.7. Build the Package
With your package configuration set, build the image. Buildroot will download, compile, and include your new package in the build process.
$ make
4.2.8. Verify the Package
After the build process completes, verify that your package is included in the output image. You can check the presence of your package’s binaries in the root filesystem.
$ find output/target -name myapp
You should see the path to your package’s binary, indicating that it was successfully included in the build.
By following these steps, you can add and build custom packages in Buildroot using the buildroot-external-TI tree. This method provides a structured way to extend the functionality of Buildroot-based systems while keeping customizations organized and separate from the main Buildroot source.
For more detailed information and advanced package options, refer to the Buildroot manual. Buildroot manual.