2.1. Release Notes
2.1.1. Overview
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM62x installer provides everything needed as discussed below to create the embedded system from “scratch” :
Platform/board-support software and configuration files for Linux
U-Boot and Kernel sources and configuration files
An ARM cross-compiling toolchain as well as other host binaries and components
A Yocto/OE compliant filesystem and sources for example applications
A variety of scripts and Makefiles to automate certain tasks
Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
Reference Examples, benchmarks
This release supports High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Licensing
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
Linux Manifest:
<PSDK_PATH>/manifest/software_manifest.htm
2.1.3. Release 11.01.05.03
Released on July 2025
2.1.3.1. What’s new
Processor SDK Linux AM62X Release has following new features:
Second 2025 LTS Reference Release Including RT combined branch model
Add support for AM62SIP, which is an example of using AM62x with 512MiB of RAM
Falcon mode through R5 SPL U-Boot Falcon Mode
Important Bug Fixes on top of Processor SDK 11.00.09.04 Release
Review Issue Tracker Section for the new fixes.
Key Release References:
RT Kernel : Real-Time Linux Interrupt Latency numbers here - RT Interrupt Latencies
Out-of-Box TI Apps Launcher Application with Qt6 Framework - TI Apps Launcher
Snagfactory Support - Snagfactory Tool
Support for M2 CC33xx cards on Debian - How to Enable M.2-CC33x1 in Linux
How to Enable PRU RPMsg - Read FAQ
How standby power mode works - CPUIdle Documentation
Component version:
Kernel 6.12.35
U-Boot 2025.01
Toolchain GCC 13.4
ATF 2.13+
OPTEE 4.6.0
Graphics DDK 24.2
TIFS Firmware / SYSFW v11.01.02 (Click on the link for more information)
DM Firmware 11.01.00.05
Yocto scarthgap 5.0
2.1.4. Build Information
2.1.4.1. U-Boot
2.1.4.2. TF-A
2.1.4.3. OP-TEE
2.1.4.4. ti-linux-firmware
2.1.4.5. Kernel
2.1.4.6. Yocto
meta-ti
meta-arago
meta-tisdk
2.1.5. Issues Tracker
Note
Release Specific Issues including details will be published through Software Incident Report (SIR) portal
Further Information can be found at SIR Portal
2.1.5.1. Errata Resolved
Record ID |
Title |
|---|---|
USB2 PHY locks up due to short suspend |
|
USART: Erroneous clear/trigger of timeout interrupt |
|
BCDMA: RX Channel can lockup in certain scenarios |
|
i2327: RTC: Hardware wakeup event limitation |
|
MMCSD: HS200 and SDR104 Command Timeout Window Too Small |
2.1.5.2. Issues Resolved
Record ID |
Title |
|---|---|
Yocto Documentation: AM6x: SDK: Build Instruction missing steps for building K3R5 baremetal toolchain |
|
SDK Docs: Broken URL in How To Guides > EVM Setup |
|
PRUSS should be disabled for AM62 LP SK board |
|
AM62x: Make Debugging SPL doc specific to AM62x |
|
Yocto: meta-ti*: kernel source has uncommited changes |
|
Null dereference on fdinfo when not bound to a render task |
|
AM62x: 6.12 LTS Regression: PRU IPC Failure due to driver missing |
2.1.5.3. Issues Open
Record ID |
Title |
|---|---|
CPSW ptp4l PDELAY_REQ and DELAY_REQ without timestamp messages |
|
Fixup A53 CPU Frequency by Speed Grade Problem |
|
CSI-2 Rx driver shall support frame width that is not 16-byte-aligned |
|
PRU RPMsg swaps which message is sent to which core |
|
misleading GPMC message in kernel log |
|
Cyclictest performance degradation on AM62x/AM64x/AM62A |
|
UDP Ingress failing |
|
Suspend-to-RAM failure: tps65219: device creates a circular dependency and device fails to enter suspend |
|
beagleplay: Segmentation-Fault: SD Boot failure and needs bootcmd update |