3.5.4. Flash via Ethernet

Ethernet is used for peripheral boot and then to flash the files to on-chip memory using DHCP server and TFTP.

3.5.4.1. Important files

Environment variable text files are located at

<TI_SDK_PATH>/bin/Ethernet_flash/am62xx-evm/

Note

This documentation note is applicable only for am62xx-evm.

3.5.4.2. Requirements on host PC

Set up Ethernet boot. For details of Ethernet boot refer Booting over Ethernet (Ethernet RGMII).

3.5.4.3. Building bootloader binaries for flashing and Ethernet Boot

First you need to override the bootcmd command to send the environment variable text file.

CONFIG_BOOTCOMMAND="dhcp <name of your uEnv.txt file>; env import -t ${loadaddr} $filesize; run user_commands;"

Add above line to am62x_evm_a53_defconfig file

3.5.4.4. Getting ready to flash

Make sure that the bootloader binaries for flashing and Ethernet boot is built for the EVM and place them in the TFTP directory.

Place the files to be flashed to TFTP directory.

Make sure to set up Ethernet boot.

For connection refer Booting over Ethernet (Ethernet RGMII).

3.5.4.5. Environment variable text file for flashing

It will be used to set environment variables in U-Boot for flashing. Create a new uEnv.txt file by using existing uEnv files as reference

It assigns U-Boot commands to run the list of commands specified by user to variable user_commands. Ex. for transfer to eMMC following commands are assigned to variable user_commands.

user_commands=echo Flashing_on_emmc; run command_list;

To add new U-Boot commands, assign them to a variable in text file. For example

example_command1=echo Flash
example_command2=mmc list

Now add the variables to command_list to run them. By this way you can add or remove commands as per your choice.

command_list=run example_command1; run example_command2;

Also make sure to replace file names in text files with the actual names of files to be flashed. Ex. to transfer tiboot3.bin over TFTP to EVM

#Enter your filename in place of tiboot3.bin
cmd_3=dhcp tiboot3.bin

Flash to eMMC

Use uEnv_ethernet_emmc_am62xx-evm.txt file as reference.

Flash to OSPI NOR

Use uEnv_ethernet_ospi-nor_am62xx-evm.txt file as reference.