3.11. Machine Learning

The Machine Learning toolkit brings machine learning to the edge by enabling machine learning inference on Sitara devices. It is provided as part of TI’s Processor SDK Linux, free to download and use. The Machine Learning toolkit consists of below modules. All the modules have been validated with examples available in EdgeAI TIDL Tools. Refer the documentation available here for more details on usage and examples

ML inference Library

Version

Delegate / Execution provider

Python API

C/CPP API

TensorFlow Lite

2.8.0

XNNPACK, ARMNN (1)

YES

YES

ONNX Runtime

1.7.0

CPU

YES

YES

  1. ARMNN delegate libraries for TFLite are not part of SDK filesystem, this has been validated with the examples and scripts available at EdgeAI TIDL Tools.