3.2.2.12. PWM

Introduction

Linux has support for Enhanced Pulse Width Modulator (ePWM) and Auxiliary Pulse Width Modulator (APWM) modules. APWM is Enhanced Capture (eCAP) module configured in PWM mode. These devices are part of the Pulse-Width Modulation Subsystem (PWMSS).

PWMSS software architecture

../../../../_images/AM335X_PWM-SS_arch.JPG

Kernel Configuration

Enable the eHRPWM driver

Device Drivers --->
   <*> Pulse Width Modulation(PWM) Support --->
      <*> eHRPWM PWM support

Enable the eCAP driver

Device Drivers --->
   <*> Pulse Width Modulation(PWM) Support --->
      <*> eCAP PWM support

Note

  • eHRPWM modules provide two PWM output channels per instance.

  • eCAP modules provide a single PWM output channel pre instance when configured in APWM mode.

Driver Usage

Using PWM with the sysfs interface

The PWMs can be used from the userspace with a simple sysfs interface exposed at /sys/class/pwm/. Each probed PWM controller/chip will be exported as pwmchipN, where N is the base of the PWM chip. The following attributes are available for each pwmchipN:

  • npwm

The number of PWM channels this chip supports.

  • export

Exports a PWM channel for use with sysfs.

  • unexport

Unexports a PWM channel from sysfs.

The PWM channels are numbered per-chip from 0 to npwm-1. When a PWM channel is exported a pwmX directory will be created in the pwmchipN directory, where X is the number of the channel that was exported. The following attributes will then be available in the pwmX directory:

  • period

The total period of the PWM signal in nanoseconds.

  • duty_cycle

The active time of the PWM signal in nanoseconds. Must be less than the period.

  • polarity

Changes the polarity of the PWM signal. The value written is the string “normal” or “inversed”.

  • enable

Enable/disable the PWM signal.

  • 0 - disabled

  • 1 - enabled

Example

List the available PWM controllers.

$ ls /sys/class/pwm/
pwmchip0  pwmchip1  pwmchip2  pwmchip3  pwmchip5  pwmchip7

The number of channels per controller is reported in the npwm attribute.

$ cat /sys/class/pwm/pwmchip5/npwm
2

The pwmchip5 controller is a 2 channel ePWM. Export the second channel (EPWM_B, channel 1).

$ echo 1 > /sys/class/pwm/pwmchip5/export

Verify pwm1 directory exists in the pwmchip5 directory.

$ ls /sys/class/pwm/pwmchip5/
device  export  npwm  power  pwm1  subsystem  uevent unexport

Note

The PWM period and duty cycle must be configured before enabling any channel.

Set a period of 100 milliseconds with 30% duty cycle. The values are in nanoseconds.

$ echo 100000000 > /sys/class/pwm/pwmchip5/pwm1/period
$ echo 30000000 > /sys/class/pwm/pwmchip5/pwm1/duty_cycle

Set the PWM signal polarity to “inversed” (or “normal”) if required.

$ echo "inversed" > /sys/class/pwm/pwmchip5/pwm1/polarity
$ cat /sys/class/pwm/pwmchip5/pwm1/polarity
inversed

Enable the PWM channel.

$ echo 1 > /sys/class/pwm/pwmchip5/pwm1/enable

Using PWM with kernel PWM API

A few examples of kernel drivers using the kernel PWM API:

Troubleshooting the PWM setup

The current PWM settings for ePWM and eCAP(APWM) can be monitored from the debugfs pwm entry.

$ cat /sys/kernel/debug/pwm
platform/23020000.pwm, 2 PWM devices
 pwm-0   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
 pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal

platform/23010000.pwm, 2 PWM devices
 pwm-0   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
 pwm-1   (sysfs               ): requested enabled period: 100000000 ns duty: 50000000 ns polarity: inverse

platform/23000000.pwm, 2 PWM devices
 pwm-0   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
 pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal

platform/23120000.pwm, 1 PWM device
 pwm-0   ((null)              ): period: 0 ns duty: 0 ns polarity: normal

platform/23110000.pwm, 1 PWM device
 pwm-0   ((null)              ): period: 0 ns duty: 0 ns polarity: normal

platform/23100000.pwm, 1 PWM device
 pwm-0   ((null)              ): period: 0 ns duty: 0 ns polarity: normal