3.8.1. Introduction

AM62x device is enabled with 3D graphics accelerator based on the A-Series AXE-1-16M from Imagination Technologies Inc. It enables the support of 3D graphics rendering using OpenGL® ES API’s. The OpenGL® ES API’s up to and including version 3.1 with render surfaces upto 4k and input textures upto 8k sizes are supported by the hardware. It also supports Vulkan ® up to API version 1.2.

The following extensions are supported:

Table 3.6 EGL client extensions

EGL_EXT_client_extensions

EGL_EXT_device_base

EGL_EXT_device_enumeration

EGL_EXT_device_query

EGL_EXT_platform_base

EGL_KHR_client_get_all_proc_addresses

EGL_KHR_debug EGL_EXT_platform_device

EGL_EXT_platform_wayland

EGL_KHR_platform_wayland

EGL_MESA_platform_gbm

EGL_KHR_platform_gbm

EGL_MESA_platform_surfaceless

Table 3.7 EGL extensions

EGL_ANDROID_native_fence_sync

EGL_EXT_buffer_age

EGL_EXT_create_context_robustness

EGL_EXT_image_dma_buf_import

EGL_EXT_image_dma_buf_import_modifiers

EGL_EXT_image_gl_colorspace

EGL_EXT_swap_buffers_with_damage

EGL_EXT_yuv_surface

EGL_IMG_context_priority

EGL_KHR_cl_event2

EGL_KHR_config_attribs

EGL_KHR_create_context

EGL_KHR_fence_sync

EGL_KHR_get_all_proc_addresses

EGL_KHR_gl_colorspace

EGL_KHR_gl_renderbuffer_image

EGL_KHR_gl_texture_2D_image

EGL_KHR_gl_texture_3D_image

EGL_KHR_gl_texture_cubemap_image

EGL_KHR_image_base

EGL_KHR_no_config_context

EGL_KHR_partial_update

EGL_KHR_reusable_sync

EGL_KHR_surfaceless_context

EGL_KHR_swap_buffers_with_damage

EGL_EXT_pixel_format_float

EGL_KHR_wait_sync

EGL_MESA_configless_context

EGL_MESA_drm_image

EGL_MESA_image_dma_buf_export

EGL_WL_bind_wayland_display

EGL_WL_create_wayland_buffer_from_image

EGL_IMG_cl_image

Table 3.8 GL extensions

GL_APPLE_texture_format_BGRA8888

GL_EXT_blend_minmax

GL_EXT_buffer_storage

GL_EXT_clip_control

GL_EXT_color_buffer_float

GL_EXT_color_buffer_half_float

GL_EXT_compressed_ETC1_RGB8_sub_texture

GL_EXT_conservative_depth

GL_EXT_copy_image

GL_EXT_discard_framebuffer

GL_EXT_draw_buffers

GL_EXT_draw_buffers_indexed

GL_EXT_draw_elements_base_vertex

GL_EXT_EGL_image_array

GL_EXT_float_blend

GL_EXT_gpu_shader5

GL_EXT_memory_object

GL_EXT_memory_object_fd

GL_EXT_multi_draw_arrays

GL_EXT_multisampled_render_to_texture

GL_EXT_multisampled_render_to_texture2

GL_EXT_occlusion_query_boolean

GL_EXT_polygon_offset_clamp

GL_EXT_read_format_bgra

GL_EXT_robustness

GL_EXT_separate_shader_objects

GL_EXT_shader_framebuffer_fetch

GL_EXT_shader_group_vote

GL_EXT_shader_implicit_conversions

GL_EXT_shader_io_blocks

GL_EXT_shader_non_constant_global_initializers

GL_EXT_shader_pixel_local_storage

GL_EXT_shader_pixel_local_storage2

GL_EXT_shader_texture_lod

GL_EXT_shadow_samplers

GL_EXT_sparse_texture

GL_EXT_sRGB_write_control

GL_EXT_texture_border_clamp

GL_EXT_texture_buffer

GL_EXT_texture_cube_map_array

GL_EXT_texture_format_BGRA8888

GL_EXT_texture_format_sRGB_override

GL_EXT_texture_rg

GL_EXT_texture_shadow_lod

GL_EXT_texture_sRGB_decode

GL_EXT_texture_sRGB_R8

GL_EXT_texture_sRGB_RG8

GL_EXT_YUV_target

GL_IMG_framebuffer_downsample

GL_IMG_multisampled_render_to_texture

GL_IMG_program_binary

GL_IMG_read_format

GL_IMG_shader_binary

GL_IMG_texture_format_BGRA8888

GL_IMG_texture_npot

GL_KHR_blend_equation_advanced

GL_KHR_blend_equation_advanced_coherent

GL_KHR_debug

GL_KHR_robustness

GL_OES_compressed_ETC1_RGB8_texture

GL_OES_depth24

GL_OES_depth_texture

GL_OES_draw_buffers_indexed

GL_OES_draw_elements_base_vertex

GL_OES_EGL_image

GL_OES_EGL_image_external

GL_OES_EGL_image_external_essl3

GL_OES_EGL_sync

GL_OES_element_index_uint

GL_OES_fragment_precision_high

GL_OES_get_program_binary

GL_OES_gpu_shader5

GL_OES_mapbuffer

GL_OES_packed_depth_stencil

GL_OES_required_internalformat

GL_OES_rgb8_rgba8

GL_OES_sample_shading

GL_OES_sample_variables

GL_OES_shader_image_atomic

GL_OES_shader_io_blocks

GL_OES_shader_multisample_interpolation

GL_OES_standard_derivatives

GL_OES_surfaceless_context

GL_OES_texture_border_clamp

GL_OES_texture_buffer

GL_OES_texture_cube_map_array

GL_OES_texture_float

GL_OES_texture_half_float

GL_OES_texture_npot

GL_OES_texture_stencil8

GL_OES_texture_storage_multisample_2d_array

GL_OES_vertex_array_object

GL_OES_vertex_half_float

Table 3.9 Vulkan instance extensions

VK_KHR_device_group_creation

v1

VK_KHR_external_fence_capabilities

v1

VK_KHR_external_memory_capabilities

v1

VK_KHR_external_semaphore_capabilities

v1

VK_KHR_get_physical_device_properties2

v2

VK_KHR_get_surface_capabilities2

v1

VK_KHR_surface

v25

VK_KHR_wayland_surface

v6

VK_KHR_xcb_surface

v6

VK_KHR_xlib_surface

v6

VK_EXT_debug_report

v10

VK_EXT_debug_utils

v2

For more information about the supported OpenGL® ES and EGL® extensions see:

Note

OpenCL® libraries are currently provided without support at https://git.ti.com

The OpenGL® ES and EGL® libraries are packaged with the Processor SDK Linux AM62x and are used by graphics stacks such as Wayland/Weston. The drivers run on an ARM core and programs the firmware running inside a GPU core with rendering commands submitted by the user applications.

Other features of the Rogue series of GPUs include bilinear and trilinear filtering.

Support for the following pixel formats:

Table 3.14 Supported surface pixel formats

ARGB8888

BGRA8888

RGB565

Table 3.15 Supported texture pixel formats

ARGB4444

ARGB8888

BGRA8888

RGB565

RGBA5551

YUV420

YUYV

NV12

Support for Ericsson Texture Compression (ETC1 and ETC2) on input textures. For an example toolkit to interact with these texture compression mechanisms, see the Khronos KTX-Software project.

Support for up to 2Kx2K render surfaces.

Support for OS controlled Active Power Management, enabled by default.

Support for OS suspend and resume functions. See How to Suspend to RAM (Deep Sleep) on AM62x for more info.

The rest of this page will cover the following topics:

  • Software architecture of Graphics

  • Instructions on how to run graphics demos

  • Instructions on how to run DSS application

  • Instructions on how launch Weston

  • Instructions on how to run PVR tools

3.8.2. Software Architecture

The picture below shows the software architecture of Graphics in Processor SDK Linux AM62x.

../../../_images/rogue-graphics-software-stack.png

Fig. 3.4 PSDK Linux Rogue Graphics Software Stack

Please note that RGX-KM in this context refers to the pvrsrvkm kernel module, which is currently provided at: https://git.ti.com/cgit/graphics/ti-img-rogue-driver

This is included by default in the SDK. The kernel module is located at:

# /lib/modules/$(uname -r)/extra/pvrsrvkm.ko

3.8.3. Graphics Demos

Along with the graphics driver and userspace libraries, the SDK also includes example applications. Some of the demos are based on the IMG Native_SDK examples.

The following demos are available to run under the Wayland windowing system.

# /usr/bin/SGX/demos/Wayland/OpenGLESDeferredShading
# /usr/bin/SGX/demos/Wayland/OpenGLESGaussianBlur
# /usr/bin/SGX/demos/Wayland/OpenGLESImageBasedLighting
# /usr/bin/SGX/demos/Wayland/OpenGLESIntroducingPVRCamera
# /usr/bin/SGX/demos/Wayland/OpenGLESIntroducingPVRUtils
# /usr/bin/SGX/demos/Wayland/OpenGLESIntroducingUIRenderer
# /usr/bin/SGX/demos/Wayland/OpenGLESNavigation2D
# /usr/bin/SGX/demos/Wayland/OpenGLESNavigation3D
# /usr/bin/SGX/demos/Wayland/OpenGLESParticleSystem

Additionally demos using the Null Window System / KMS / DRM / EGLFS are provided with Qt. By default EGLFS will use the eglfs_kms backend.

# /usr/share/qt5/examples/opengl/hellogles3/hellogles3 -platform eglfs
# /usr/share/qt5/examples/opengl/2dpainting/2dpainting -platform eglfs
# /usr/share/qt5/examples/opengl/paintedwindow/paintedwindow -platform eglfs

The default eglfs_kms configuration file for Qt5 is located at:

# /etc/qt5/eglfs_kms_cfg.json

For more information about Qt’s EGLFS and using Qt5 in embedded applications see:

3.8.4. Display

TI SoC’s are equipped with Display SubSystem (DSS) hardware to provide hardware acceleration for alpha blending of overlays and color conversion. The DSS hardware is exposed to the software drm API available through libdrm module. Through this drm interface, a user space program can perform mode setting of the display.

The drm module models the display hardware as a series of abstract hardware blocks and manages them through the API. The blocks are:

  • CRTC1: represents a scanout engine that generates video timing signal from the data pointed to by the scanout buffer

  • Connector: represents where the video timing signal is sent across to the display

  • Encoder: transforms the video timing signal from CRTC to a format that is suitable for sending across the connector

  • Plane: represents the overlay buffer that a CRTC can be fed with

A utility application modetest can be used to get the list of available drm blocks. All the information available for the device can be displayed by using it.

3.8.4.1. Finding Connector ID

Run the below modetest command:

Look for the display device for which the connector ID is required - such as HDMI, LCD etc.

Connectors:
id      encoder status          type    size (mm)       modes   encoders
4       3       connected       HDMI-A  480x270         20      3
  modes:
        name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
  1920x1080 60 1920 2008 2052 2200 1080 1084 1089 1125 flags: phsync, pvsync; type: preferred, driver
...
16      15      connected       unknown 0x0             1       15
  modes:
        name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
  800x480 60 800 1010 1040 1056 480 502 515 525 flags: nhsync, nvsync; type: preferred, driver

The modes displayed are the various resolutions supported by the connected display.

3.8.4.2. Finding Plane ID

To find the Plane ID, run the modetest command:

which should show something like below:

Planes:
id      crtc    fb      CRTC x,y        x,y     gamma size
19      0       0       0,0             0,0     0
 formats: RG16 RX12 XR12 RA12 AR12 XR15 AR15 RG24 RX24 XR24 RA24 AR24 NV12 YUYV UYVY
 props:
 ...
20      0       0       0,0             0,0     0
 formats: RG16 RX12 XR12 RA12 AR12 XR15 AR15 RG24 RX24 XR24 RA24 AR24 NV12 YUYV UYVY
 props:
 ...

3.8.5. Wayland/Weston

The supported Wayland/Weston version brings in the multiple display support in extended desktop mode and the ability to drag-and-drop windows from one display to the other.

3.8.5.1. Starting Weston with Systemd

Starting with Weston 10, the preferred way to start Weston is with the weston user using the systemd service. If you need to interact with this instance using any other user then make sure that user is in the wayland or root group and direct them to interact with that instance using the global socket at /run/wayland-0.

This global socket is special in that it will automatically launch Weston when a GUI application attempts to connect to it. A profile script in /etc/profile.d will automatically set the WAYLAND_DISPLAY environment variable if the user has sufficient permission to interact with the socket.

To start the systemd service manually, do the following:

# systemctl start weston

To inspect the systemd service and socket status, do the following:

# systemctl status weston.service weston.socket

3.8.5.2. Starting Weston Manually

To launch Weston manually, do the following:

On the target console:

# unset WAYLAND_DISPLAY

On the default display:

# weston --tty=1 --display=<default connector-id>

On the secondary display:

# weston --tty=1 --display=<secondary connector-id>

On all connected displays (LCD and HDMI):

# weston --tty=1

By default, the screensaver timeout is configured to 300 seconds. The user can change the screensaver timeout using a command line option:

--idle-time=<number of seconds>

For example, to set timeout of 10 minutes and Weston configured to display on all connectors, use the below command:

weston --tty=1 --idle-time=600

To disable the screen timeout and to configure Weston to display on all connectors, use the below command:

weston --tty=1 --idle-time=0

If you face any issues with the above procedure, please refer to the upstream weston documentation for troubleshooting tips.

The filesystem comes with a preconfigured weston.ini file which will be located in

/etc/xdg/weston/weston.ini

3.8.5.3. Running Weston clients

Weston client examples can run from the command line on a serial port console or an SSH console. After launching Weston, the user should be able to use the keyboard and the mouse for various controls.
# /usr/bin/weston-flower
# /usr/bin/weston-clickdot
# /usr/bin/weston-cliptest
# /usr/bin/weston-dnd
# /usr/bin/weston-editor
# /usr/bin/weston-eventdemo
# /usr/bin/weston-image /usr/share/weston/terminal.png
# /usr/bin/weston-resizor
# /usr/bin/weston-simple-egl
# /usr/bin/weston-simple-shm
# /usr/bin/weston-simple-touch
# /usr/bin/weston-smoke
# /usr/bin/weston-info
# /usr/bin/weston-terminal

3.8.5.4. Running multimedia with Wayland sink

The GStreamer video sink for Wayland is the waylandsink. To use this video-sink for video playback:

# gst-launch-1.0 playbin uri=file://<path-to-file-name> video-sink=waylandsink

3.8.5.5. Exiting Weston

Terminate all Weston clients before exiting Weston. If you have invoked Weston from the serial console, exit Weston by pressing Ctrl-C.

If Weston was started automatically by the init system then it can be stopped with:

# systemctl stop weston

It is also possible to invoke Weston from the native console, exit Weston by pressing Ctrl-Alt-Backspace.

3.8.5.6. Using IVI shell feature

The SDK also has support for configuring Weston ivi-shell. The default shell that is configured in the SDK is the desktop-shell.

To change the shell to ivi-shell, the user will have to add the following lines into the /etc/xdg/weston/weston.ini.

To switch back to the desktop-shell can be done by commenting these lines in the /etc/xdg/weston/weston.ini (comments begin with a ‘#’ at the start of line).

[core]
shell=ivi-shell.so

After the above configuration is completed, we can restart Weston by running the following command

# systemctl restart weston

Note

When Weston starts with ivi-shell, the default background is black, this is different from the desktop-shell that brings up a window with background.

With ivi-shell configured for Weston, Wayland client applications use ivi-application protocol to be managed by a central HMI window management.

Applications must support the ivi_application Wayland protocol to be managed by the HMI central controller with an unique numeric ID.

Some important references to Weston IVI-shell can be found at the following link:

3.8.5.6.1. Running QT applications with IVI shell

To run the QT application with ivi-shell, set the QT_WAYLAND_SHELL_INTEGRATION environment variable to ivi-shell.

# export QT_WAYLAND_SHELL_INTEGRATION=ivi-shell

3.8.6. Using the PowerVR Tools

The suite of PowerVR Tools is designed to enable rapid graphics application development. It targets a range of areas including asset exporting and optimization, PC emulation, prototyping environments, on-line and off-line performance analysis tools and many more. Please refer to PowerVR-SDK for additional details on the tools and detailed documentation.

There are a number of useful tools available in the Imagination PowerVR SDK that are compatible with our devices. Two of the most useful tools available are PVRTune and PVRCarbon, which can be used for to profiling and tracing GFX activities.

Previously these were included in the target’s rootfs, but these were removed due to tight version dependencies between the target and host tools. Imagination has moved to packaging the target binaries with their host installer, so we recommend using those binaries directly for guaranteed compatibility.

3.8.6.1. PVRTune

The PVRTune utility is a real-time GPU performance analysis tool. It captures hardware timing data and counters which facilitate the identification of performance bottlenecks. PVRPerfServer should be used along with the PVRTune running on the PC to gather data on the SGX loading and activity threads. The target binaries can be found in the host’s PVRTune installation directory under PVRPerfServer.

For more information please refer to Imagination’s upstream documentation on PVRTune and PVRPerfServer.

https://docs.imgtec.com/tools-manuals/pvrtune-manual/topics/introduction.html

3.8.6.2. PVRCarbon

The PVRCarbon is an OpenGL® ES and Vulkan ® API recording and analysis utility. PVRCarbon GUI provides off-line tools to inspect captured data, identify redundant calls, highlight costly shaders and many more. This tool can capture traces on target and then play them back on multiple different devices by introducing shim libraries in place of the standard offering for that API.

This requires a little bit of setup on the target though. Please refer to Imagination’s upstream target setup guide for the most recent instructions.

https://docs.imgtec.com/tools-manuals/pvrcarbon-manual/topics/pvrcarbon-recorder/opengl-es/linux.html

1

CRTC stands for cathode-ray tube controller, a throw back to the old cathode-ray tubes TV’s which had a controller that generated video timings based on the data it is being fed by a buffer.