3.1.1.2. Build
3.1.1.2.1. Build U-Boot
Note
The following commands are intended to be run from the root of the U-Boot tree unless otherwise specified. The root of the U-Boot tree is the top-level directory and can be identified by looking for the “MAINTAINERS” file.
Note
Note about HSM Rearchitecture
After HSM rearchitecture in bootloader, loading of remote cores with firmware will be supported at A72 SPL stage only and not at R5 SPL stage. Early loading of remote core firmware in R5 SPL requires core reset functionality. As part of HSM rearchitecture, this functionality has moved into the DM service which requires SPL to re-implement device and clock control. This support is not present in Uboot R5 SPL due to memory constraints on the existing 64-bit TI devices.
Note
As of Processor SDK 9.0, compilation of bootloader images will no longer require different defconfigs for GP and HS devices. The same build commands will generate images for GP, HS-SE and HS-FS devices.
Prebuilt Images
Several prebuilt images are required from the TI Processor SDK for building U-Boot on K3 based platforms.
TF-A (BL-31): Refer to ARM Trusted Firmware-A for more information
OP-TEE (TEE): Refer to OP-TEE for more information
ti-linux-firmware (BINMAN_INDIRS): Prebuilt binaries for DM and SYSFW available here.
All of these binaries are available in the SDK at <path to tisdk>/board-support/prebuilt-images>
Compiling R5 and ARM64 images
Use the following table to determine what defconfig to use to configure with:
Note
BINMAN_INDIRS is used to fetch the DM binary from board-support/prebuilt-images/ti-dm/ and SYSFW binaries from board-support/prebuilt-images/ti-sysfw/. If not using the SDK, BINMAN_INDIRS can point to either ti-linux-firmware or any folder where DM is located in <path to folder>/ti-dm/ and SYSFW binaries are present in <path to folder>/ti-sysfw/. Please make sure to use the absolute path.