3.4.7. Post-quantum cryptography

3.4.7.1. Introduction

Post-Quantum Cryptography (PQC) refers to cryptographic algorithms built to resist attacks by quantum computers. Classical asymmetric algorithms such as RSA and Elliptic Curve Cryptography (ECC) are vulnerable to polynomial-time quantum factoring algorithms running on a sufficiently powerful quantum computer.

The National Institute of Standards and Technology (NIST) has standardized three PQC algorithms:

  • Federal Information Processing Standards (FIPS) 203: Module Lattice (ML) Key Encapsulation Mechanism (KEM) or ML-KEM, based on CRYSTALS-Kyber

  • FIPS 204: Module Lattice (ML) Digital Signature Algorithm (DSA) or ML-DSA, based on CRYSTALS-Dilithium

  • FIPS 205: Stateless Hash-Based (SLH) Digital Signature Algorithm (DSA) or SLH-DSA, based on SPHINCS+

The SDK includes OpenSSL 3.5.x, which provides native support for all NIST-standardized PQC algorithms through its default provider. You do not need external libraries or patches.

3.4.7.2. Verifying post-quantum support

To confirm the OpenSSL version and available PQC algorithms on the target board:

root@<machine>:~# openssl version
OpenSSL 3.5.5 27 Jan 2026 (Library: OpenSSL 3.5.5 27 Jan 2026)

List supported KEM algorithms:

root@<machine>:~# openssl list -kem-algorithms | grep -i ml
  { 2.16.840.1.101.3.4.4.1, id-alg-ml-kem-512,  ML-KEM-512,  MLKEM512  } @ default
  { 2.16.840.1.101.3.4.4.2, id-alg-ml-kem-768,  ML-KEM-768,  MLKEM768  } @ default
  { 2.16.840.1.101.3.4.4.3, id-alg-ml-kem-1024, ML-KEM-1024, MLKEM1024 } @ default
  X25519MLKEM768    @ default
  X448MLKEM1024     @ default
  SecP256r1MLKEM768 @ default
  SecP384r1MLKEM1024 @ default

List supported signature algorithms:

root@<machine>:~# openssl list -signature-algorithms | grep -i -E 'ml-dsa|slh-dsa'
  { 2.16.840.1.101.3.4.3.17, id-ml-dsa-44, ML-DSA-44, MLDSA44 } @ default
  { 2.16.840.1.101.3.4.3.18, id-ml-dsa-65, ML-DSA-65, MLDSA65 } @ default
  { 2.16.840.1.101.3.4.3.19, id-ml-dsa-87, ML-DSA-87, MLDSA87 } @ default
  { 2.16.840.1.101.3.4.3.20, id-slh-dsa-sha2-128s,  SLH-DSA-SHA2-128s  } @ default
  { 2.16.840.1.101.3.4.3.21, id-slh-dsa-sha2-128f,  SLH-DSA-SHA2-128f  } @ default
  { 2.16.840.1.101.3.4.3.22, id-slh-dsa-sha2-192s,  SLH-DSA-SHA2-192s  } @ default
  { 2.16.840.1.101.3.4.3.23, id-slh-dsa-sha2-192f,  SLH-DSA-SHA2-192f  } @ default
  { 2.16.840.1.101.3.4.3.24, id-slh-dsa-sha2-256s,  SLH-DSA-SHA2-256s  } @ default
  { 2.16.840.1.101.3.4.3.25, id-slh-dsa-sha2-256f,  SLH-DSA-SHA2-256f  } @ default
  { 2.16.840.1.101.3.4.3.26, id-slh-dsa-shake-128s, SLH-DSA-SHAKE-128s } @ default
  { 2.16.840.1.101.3.4.3.27, id-slh-dsa-shake-128f, SLH-DSA-SHAKE-128f } @ default
  { 2.16.840.1.101.3.4.3.28, id-slh-dsa-shake-192s, SLH-DSA-SHAKE-192s } @ default
  { 2.16.840.1.101.3.4.3.29, id-slh-dsa-shake-192f, SLH-DSA-SHAKE-192f } @ default
  { 2.16.840.1.101.3.4.3.30, id-slh-dsa-shake-256s, SLH-DSA-SHAKE-256s } @ default
  { 2.16.840.1.101.3.4.3.31, id-slh-dsa-shake-256f, SLH-DSA-SHAKE-256f } @ default

3.4.7.3. Supported algorithms

3.4.7.3.1. Key encapsulation

ML-KEM is a KEM used to securely establish a shared secret between two parties. It replaces classical Elliptic Curve Diffie-Hellman (ECDH) or RSA key exchange in protocols such as Transport Layer Security (TLS).

Security levels reference Advanced Encryption Standard (AES) bit equivalence as a baseline:

Algorithm

NIST Security Level

Use Case

ML-KEM-512

Level 1 (~AES-128)

Constrained environments

ML-KEM-768

Level 3 (~AES-192)

General purpose

ML-KEM-1024

Level 5 (~AES-256)

High-security applications

Hybrid KEM variants combine classical and PQC algorithms, providing protection even if an attacker breaks one:

  • X25519MLKEM768: X25519 + ML-KEM-768 (recommended for TLS)

  • X448MLKEM1024: X448 + ML-KEM-1024

  • SecP256r1MLKEM768: ECDH P-256 + ML-KEM-768

  • SecP384r1MLKEM1024: ECDH P-384 + ML-KEM-1024

3.4.7.3.2. Digital signatures

ML-DSA is a lattice-based DSA replacing classical RSA or Elliptic Curve Digital Signature Algorithm (ECDSA) signatures.

Algorithm

NIST Security Level

Key Size (approx.)

ML-DSA-44

Level 2

~1.3 KB

ML-DSA-65

Level 3

~2.0 KB

ML-DSA-87

Level 5

~2.6 KB

3.4.7.3.3. Hash-based signatures

SLH-DSA is a stateless hash-based signature scheme with minimal security assumptions (only hash function security). It is available in SHA-2 and Secure Hash Algorithm-3 (SHA-3) extendable-output (SHAKE) variants, each with small (s) and fast (f) tradeoffs:

  • s variants: smaller signatures, slower signing

  • f variants: larger signatures, faster signing

3.4.7.4. Usage examples

3.4.7.4.1. Generating keys and signing

Generate an ML-DSA key pair:

root@<machine>:~# openssl genpkey -algorithm ML-DSA-65 -out ml-dsa.key
root@<machine>:~# openssl pkey -in ml-dsa.key -pubout -out ml-dsa.pub

Sign a file:

root@<machine>:~# echo "hello pqc" > file.txt
root@<machine>:~# openssl pkeyutl -sign -inkey ml-dsa.key -in file.txt -out file.sig

Verify the signature:

root@<machine>:~# openssl pkeyutl -verify -pubin -inkey ml-dsa.pub -in file.txt -sigfile file.sig
Signature Verified Successfully

3.4.7.4.2. Hash-based key signing

root@<machine>:~# openssl genpkey -algorithm SLH-DSA-SHA2-128s -out slh-dsa.key
root@<machine>:~# openssl pkeyutl -sign -inkey slh-dsa.key -in file.txt -out file.sig

3.4.7.4.3. Self-signed certificate

Generate a self-signed certificate with ML-DSA for testing:

root@<machine>:~# openssl req -x509 -newkey ml-dsa-65 \
    -keyout server.key -out server.crt \
    -days 365 -nodes -subj '/CN=my-device'

3.4.7.5. Testing the key exchange

ML-KEM is a KEM primitive. It does not have a standalone encrypt or decrypt command. ML-KEM serves only as the key exchange mechanism inside a TLS 1.3 handshake (replacing ECDH). Both client and server must advertise the same group to negotiate it.

3.4.7.5.1. Generating a certificate

The TLS server requires a certificate. Use ML-DSA for a fully PQC setup:

root@<machine>:~# openssl req -x509 -newkey ml-dsa-65 \
    -keyout /tmp/server.key -out /tmp/server.crt \
    -days 1 -nodes -subj '/CN=test'

3.4.7.5.2. Starting the server

root@<machine>:~# openssl s_server \
    -cert /tmp/server.crt \
    -key /tmp/server.key \
    -groups X25519MLKEM768 \
    -port 4433 -www &

3.4.7.5.3. Connecting the client

root@<machine>:~# openssl s_client \
    -connect localhost:4433 \
    -groups X25519MLKEM768 \
    </dev/null 2>&1 | grep -E 'group|Cipher|Protocol'

Expected output confirming ML-KEM negotiation:

Negotiated TLS1.3 group: X25519MLKEM768
New, TLSv1.3, Cipher is TLS_AES_256_GCM_SHA384
Protocol  : TLSv1.3

3.4.7.5.4. Handshake walkthrough

The verbose handshake (-msg flag) reveals the full PQC key exchange flow:

root@<machine>:~# openssl s_client \
    -connect localhost:4433 \
    -groups X25519MLKEM768 \
    -msg </dev/null 2>&1

Annotated handshake sequence:

>>> ClientHello
    Client advertises X25519MLKEM768 in supported_groups + key_share.
    Sends its ML-KEM public key (encapsulation key) to the server.

<<< ServerHello  [length ~0x4ba]
    Server selects X25519MLKEM768.
    Encapsulates using client's ML-KEM public key.
    Sends the ML-KEM ciphertext (~1200 bytes) back. This is the
    key encapsulation happening over the wire.

<<< Certificate
    Server's certificate using ML-DSA-65 signature (15616-bit key).

<<< CertificateVerify
    Proves server holds the private key, signed with ML-DSA-65.

<<< Finished  /  >>> Finished
    Both sides confirm the handshake using the derived shared secret.

Negotiated TLS1.3 group: X25519MLKEM768
Protocol  : TLSv1.3
Cipher    : TLS_AES_256_GCM_SHA384

The full session uses PQC at every asymmetric operation. Bulk encryption uses AES-256 in Galois Counter Mode (GCM):

TLS Role

Algorithm

Standard

Key exchange

X25519MLKEM768

Hybrid (classical + FIPS 203)

Server certificate

ML-DSA-65

FIPS 204

Bulk encryption

AES-256-GCM

Symmetric (not PQC-relevant)

Note

The X25519MLKEM768 hybrid is the recommended choice for TLS. It provides classical security from X25519 in addition to PQC security from ML-KEM-768. If either algorithm is ever broken, the other still protects the session.

3.4.7.6. Notes

  • ML-KEM requires TLS 1.3. You cannot use it with TLS 1.2 or earlier.

  • SLH-DSA signatures are large (8-50 KB depending on variant). Use ML-DSA for TLS certificates where size matters.

  • All algorithms above are available in the OpenSSL default provider. You do not need additional provider configuration.

3.4.7.7. See also