Processor SDK Linux for AM62Ax
10_00_00
1. Overview
2. Release Specific
3. Foundational Components
4. Edge AI user guide
5. RTOS/NO-RTOS [MCU+ SDK]
6. How to Guides
6.1. Developer Notes
6.1.1. Connect to an EVM via Telnet
6.1.2. How to Setup a Samba Server
6.1.3. Moving Files to the Target System
6.1.4. SDK File System Optimization/Customization
6.1.5. How to Enable M.2-CC33x1 in Linux
6.1.6. How to enable MCAN in Linux
6.1.7. How to enable DT overlays in linux
6.1.8. How to playback audio over HDMI
6.1.9. How to Use K3Conf Tool
6.1.10. Real-Time Linux on TI SoCs
6.1.11. Boot Time Optimizations
6.1.12. Unlocking Runtime Debug on a Secure Device (HS) via the Secure Access Point
6.1.13. How to check some device tree information from user-space of Linux?
6.1.14. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM62Ax?
6.1.15. How to Build a Ubuntu Linux host under VMware
6.1.16. K3 Resource Partitioning Tool
6.1.17. Enabling and Parsing SYSFW Trace
6.2. Hardware EVM Setup
7. Applications
Processor SDK Linux for AM62Ax
»
6.
How to Guides
»
6.1.
Developer Notes
»
6.1.12.
Unlocking Runtime Debug on a Secure Device (HS) via the Secure Access Point
6.1.12.
Unlocking Runtime Debug on a Secure Device (HS) via the Secure Access Point
Refer to
Secure Debug User Guide
available in the
System Firmware Documentation
.