3.2.2.8.3.2.2.4. IET¶
3.2.2.8.3.2.2.4.1. Introduction¶
CPSW h/w support Intersperse Express Traffic (IET, defined in P802.3br/D2.0 spec which later is included in IEEE 802.3 2018) Frame preemption (FPE) feature and also to allow MAC layer to Verify if the peer supports IET MAC merge layer or not. MAC merge layer is responsible for preempting the transmission of frame from a preemptible queue if there is frame waiting for transmission at a higher priority Express queue. The h/w sends an initial segment of the frame satisfying min fragment size requirement and then schedule frame from the Express queue for transmission. Finally when no more frames available at the Express queue, it will resume transmission of remaining segments of the frame of the preemptible queue which was preempted. At the peer end, the segments are re-assembled and delivered to the MAC interface.
IET FPE feature is configured for a port through ethtool –set-priv-flags command. Note that this is a temporary interface to allow configure IET FPE in CPSW2g driver and is not approved by netdev subsystem maintainers in Linux Kernel Mailing List (LKML) and may change in the future. Driver configures IET FPE for a port when network device is opened (ndo_open()) if user has turned ON the iet-frame-preemption priv flag. Note that since IET is a common feature applicable to all slave ports, this has to be done before the network ports of the CPSW2g are brought up. The user may also turn ON the iec-mac-verify flag if the peer device connected to CPSW2g port is also capable of verifying MAC merge/FPE capability. For this, driver schedules a worker thread to do the MAC/Verify process as soon as the Link is up and iec-mac-verify priv flag is set. It resets the LINKFAIL bit and check if the Verify succeeds or not. On failure, the MAC Verify state machine is reset by toggling LINKFAIL bit and process repeats for 20 times before bailing out. If iec-mac-verify priv flag is not set, driver assumes that peer is capable of supporting FPE, but not able to do MAC Verify. So it configures the device into force mode. User needs to verify that peer device is capable of supporting IET FPE to use force mode.
Driver assumes highest priority h/w Queue as the express Queue and configures lower queues (Q0-QN-2, where N is the maximum number of queues configured) as preemptible queues by programming the PN_REG_IET_CTRL register if the MAC Verify succeeds or if the force mode is enabled. p0-rx-ptype-rrobin flag should be turned off before using IET feature. i.e CPSW2g h/w should be programmed into strict priority mode for IET to work.
To enable IET FPE with MAC Verify, do
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
To enable IET FPE with no MAC Verify (Force mode)
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
To disable IET FPE and restore rrobin mode
ethtool --set-priv-flags eth0 iet-frame-preemption off
ethtool --set-priv-flags eth0 iet-mac-verify off
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin on
Example session to enable IET FPE with MAC Verify.
Assume 2 AM65x IDKs are connected back to back over MCU Ethernet port (typically eth0 interface. Example assumes 2 h/w queues configured. Q1 will be express queue and Q0 the preemption queue in this configuration.
root@evm:~# ip link set dev eth0 down
[ 169.798571] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
root@evm:~# ethtool -L eth0 tx 2
root@evm:~# ethtool -l eth0
Channel parameters for eth0:
Pre-set maximums:
RX: 1
TX: 8
Other: 0
Combined: 0
Current hardware settings:
RX: 1
TX: 2
Other: 0
Combined: 0
@evm:~# ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
root@evm:~# ethtool --set-priv-flags eth0 iet-frame-preemption on
root@evm:~# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : off
iet-frame-preemption: on
iet-mac-verify : off
root@evm:~# ethtool --set-priv-flags eth0 iet-mac-verify on
root@evm:~# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : off
iet-frame-preemption: on
iet-mac-verify : on
root@evm:~# ip link set dev eth0 up
root@evm:~#
root@evm:~# [ 267.393967] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 267.400353] am65-cpsw-nuss 46000000.ethernet eth0: Starting IET/FPE MAC Verify
[ 267.465086] am65-cpsw-nuss 46000000.ethernet eth0: IET/FPE MAC Verify Success
[ 267.472276] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
Example session to enable IET FPE with no MAC Verify (Force mode)
root@evm:~# ip link set dev eth0 down
[ 394.590576] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
root@evm:~# ethtool --set-priv-flags eth0 iet-frame-preemption on
#if iet-mac-verify was enabled before, turn it of
root@evm:~# ethtool --set-priv-flags eth0 iet-mac-verify off
root@evm:~# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : off
iet-frame-preemption: on
iet-mac-verify : off
root@evm:~#
root@evm:~# ip link set dev eth0 up
root@evm:~# ip addr add 192.168.100.20/24 dev eth0
[ 500.502660] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
root@evm:~# [ 500.516232] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
root@evm:~# [ 552.738077] am65-cpsw-nuss 46000000.ethernet eth0: IET Enable Force mode
[ 552.744839] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 552.753434] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
IET FPE example
Highest priority Queue is Express queue. I.e if there are 8 queues configured through ethtool -L command, Q7 will be express and Q0-Q6 will be preemptible. Similarly if 4 queues are configured then Q3 will be express queue and Q0-Q2 will be preemptible queues. See below an example on how to verify preemption is happening in the hardware. Setup requires 2 IDKs (Example AM65x) connected over MCU Ethernet/CPSW2g port. Assume that IET is enabled on both IDKs as in previous sections and either Force mode or MAC Verify mode is enabled. As soon as the Link comes up, the IET FPE gets enabled. The test requires MQPRIO qdisc to be configured at the Talker DUT’s eth0 port and enable classifier to map UDP frames with specific port to be to a given traffic class. Traffic class is used as the index to direct traffic to the specific h/w queue. CPSW2g stats module provide a statistics counter for following that can be used to verify the IET FPE is functional:-
- iet_rx_assembly_ok - Increments at the receiver if re-assembly of MAC fragments are successful.
- iet_rx_frag - Incremenets at the receiver if MAC fragments are received due to preemption
- iet_tx_frag - Increments at the sender side if fragments are created due to frame preemption.
So to test, need to have traffic at the preemption queue as well as at the express queue and use the above statistics counters to verify if fragmentation happens at the sender side and re-assembly at the receiver side. Below logs provide some example usage.
# At the Talker side
# Set up mqprio qdisc at eth0 - 2 Queues configured. Q0 - preemption queue and Q1 express queue
root@evm:~# tc qdisc replace dev eth0 handle 100: parent root mqprio num_tc 2 map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@0
1@1 hw 0
root@evm:~# tc -g class show dev eth0
+---(100:ffe1) mqprio
| +---(100:2) mqprio
|
+---(100:ffe0) mqprio
+---(100:1) mqprio
# Enable classifier at net core
root@evm:~# tc qdisc add dev eth0 clsact
# Add tc filter rule to mark packet priority based on destination UDP port number - Port 5002 mapped to prio 2
# From above mqprio settings, TC at index 2 is 0. So this TC packets go to Q0
root@evm:~# tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
[ 285.576105] u32 classifier
[ 285.578910] input device check on
[ 285.582640] Actions configured
# Add tc filter rule to map packets with UDP port number - Port 5003 to prio 3
# From above mqprio settings, TC at index 3 is 1. So this TC packets go to Q1
root@evm:~# tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
root@evm:~#
root@evm:~# ip addr add 192.168.100.20/24 dev eth0
# At the Listener DUT, setup ip address and run iperf3 server session listening to port 5002 and 5003.
# ip addr add 192.168.100.30/24 dev eth0
root@evm:~# iperf3 -s -i30 -p5002&
[1] 1224
root@evm:~# iperf3 -s -i30 -p5003&
-----------------------------------------------------------
Server listening on 5002
-----------------------------------------------------------
[2] 1225
-----------------------------------------------------------
Server listening on 5003
-----------------------------------------------------------
root@evm:~#
# At Listener DUT start iperf3 client session to port 5002 and 5003
root@evm:~# iperf3 -c 192.168.100.30 -u -b200M -l1472 -u -t30 -i30 -p5002&
[1] 1050
root@evm:~# iperf3 -c 192.168.100.30 -u -b50M -l1472 -u -t30 -i30 -p5003&
[2] 1051
root@evm:~#
root@evm:~# warning: UDP block size 1472 exceeds TCP MSS 1448, may result in fragmentation / drops
warning: UDP block size 1472 exceeds TCP MSS 1448, may result in fragmentation / drops
Connecting to host 192.168.100.30, port 5003
Connecting to host 192.168.100.30, port 5002
[ 5] local 192.168.100.20 port 60646 connected to 192.168.100.30 port 5003
[ 5] local 192.168.100.20 port 39515 connected to 192.168.100.30 port 5002
# Now at the Talker DUT, dump statistics counter for Q0 and Q1 as well as IET statistics
root@evm:~# ethtool -S eth0 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 24869
tx_pri1_bcnt: 37722660
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@evm:~# ethtool -S eth0 | grep 'tx_pri0'
p0_tx_pri0: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 100271
tx_pri0_bcnt: 152067960
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 159
root@evm:~# ethtool -S eth0 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 27718
tx_pri1_bcnt: 42047442
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@evm:~# ethtool -S eth0 | grep 'tx_pri0'
p0_tx_pri0: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 111637
tx_pri0_bcnt: 169320030
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 175
# As seen, iet_tx_frag statistics counter increments at the Talker showing fragmentation at the Talker
# Also dump the statistics at the listener DUT
ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 248
iet_rx_smd_err: 0
iet_rx_frag: 248
iet_tx_hold: 0
iet_tx_frag: 0
root@evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 252
iet_rx_smd_err: 0
iet_rx_frag: 252
iet_tx_hold: 0
iet_tx_frag: 0
root@evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 252
iet_rx_smd_err: 0
iet_rx_frag: 252
iet_tx_hold: 0
iet_tx_frag: 0
# As seen, iet_rx_frag and iet_rx_assembly_ok statistics counter increments at the Listener showing re-assembly at the Listener
Using IET together with EST
Express and preemption queues/Gates may be used as part of the EST schedule. If only Preemption queues are in a schedule entry, preceding an entry with Express queue, the guard band requirement reduces to 2048 nsec (0x100 = 256 * 8) so that packets don’t spill over to the next sched-entry. Otherwise, the guard band required is as explained in the EST section.
3.2.2.8.3.2.2.4.2. Warning: IET with Fixed-Link Interface¶
If one of the interfaces which takes part in IET is in fixed-link mode, then do NOT enable MAC verify for IET on either of the devices connected to each other directly by the LAN cable. This is because, in the case of fixed-link, the link state cannot be detected by interfaces on either side of the link. The process of IET MAC Verification depends on the link state being toggled, with the verification starting immediately after the link comes up and lasting for 1 second. Thus, unless this process starts roughly simultaneously on both interfaces connected over the link (Which would happen in the non fixed-link case), IET MAC Verification would fail with a Timeout message, thereby causing frame fragmentation to fail.
Thus, if either of the interfaces that are directly connected by a LAN cable, is in fixed-link mode, then do NOT enable MAC verify on BOTH the interfaces. Simply enable IET Frame Preemption on both devices and IET will work. The rest of the steps are the same as documented in the upcoming sectionss.
IET MAC Verification in ethtool corresponds to:
iet-mac-verify
IET Frame Preemption in ethtool corresponds to:
iet-frame-preemption
3.2.2.8.3.2.2.4.3. IET in MAC mode¶
3.2.2.8.3.2.2.4.3.1. AM625-SK fragments frames and J7VCL assembles them¶
Connect eth0 of AM625-SK to eth1 of J7VCL.
Steps:
- Create and run the following script on J7VCL:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth1 up
sleep 5
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
- Create and run the following script on AM625-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
tc qdisc replace dev eth0 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth0
tc qdisc add dev eth0 clsact
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
ip addr add 192.168.100.20/24 dev eth0
sleep 2
- On J7VCL, run the following command:
ifconfig eth1 192.168.100.30
- Now, run the following commands on AM625-SK:
iperf3 -c 192.168.100.30 -u -b200M -l1472 -u -t30 -i30 -p5002&
iperf3 -c 192.168.100.30 -u -b50M -l1472 -u -t30 -i30 -p5003&
Results:
On AM625-SK (Sender):
root@am62xx-evm:~/IET# ethtool -S eth0 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 127400
tx_pri1_bcnt: 193357542
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth0 | grep 'tx_pri0'
p0_tx_pri0: 67
p0_tx_pri0_bcnt: 10496
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 509608
tx_pri0_bcnt: 773438547
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 63
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 120056
On J7VCL (Receiver):
root@j7200-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 32334
iet_rx_smd_err: 1
iet_rx_frag: 120056
iet_tx_hold: 0
iet_tx_frag: 0
Explanation:
On AM625-SK, the higher priority traffic preempts the lower priority
traffic, thereby resulting in the fragmentation of frames of lower
priority. This can be seen in the iet_tx_frag statistic on AM625-SK.
Similarly, on J7VCL, the received fragmented frames can be observed
in the iet_rx_frag statistic, while the assembled frames can be seen
in the iet_rx_assembly_ok statistic.
3.2.2.8.3.2.2.4.3.2. J7VCL fragments frames and AM625-SK assembles them¶
Connect eth1 of J7VCL to eth0 of AM625-SK.
Steps:
- Create and run the following script on AM625-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
- Create and run the following script on J7VCL:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth1 up
sleep 5
tc qdisc replace dev eth1 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth1
tc qdisc add dev eth1 clsact
tc filter add dev eth1 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
tc filter add dev eth1 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
ip addr add 192.168.100.20/24 dev eth1
sleep 2
- Run the following command on AM625-SK:
ifconfig eth0 192.168.100.30
- Next, run the following commands on J7VCL:
iperf3 -c 192.168.100.30 -u -b200M -l1472 -u -t30 -i30 -p5002&
iperf3 -c 192.168.100.30 -u -b50M -l1472 -u -t30 -i30 -p5003&
Results:
On J7VCL (Sender):
root@j7200-evm:~/IET# ethtool -S eth1 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 254787
tx_pri1_bcnt: 386711048
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth1 | grep 'tx_pri0'
p0_tx_pri0: 110
p0_tx_pri0_bcnt: 16002
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 1019126
tx_pri0_bcnt: 1546856078
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 36
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 42
On AM625-SK (Receiver):
root@am62xx-evm:~/IET# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 29
iet_rx_smd_err: 1
iet_rx_frag: 42
iet_tx_hold: 0
iet_tx_frag: 0
Explanation:
On J7VCL, the higher priority traffic preempts the lower priority
traffic, thereby resulting in the fragmentation of frames of lower
priority. This can be seen in the iet_tx_frag statistic on J7VCL.
Similarly, on AM625-SK, the received fragmented frames can be observed
in the iet_rx_frag statistic, while the assembled frames can be seen
in the iet_rx_assembly_ok statistic.
3.2.2.8.3.2.2.4.4. IET in Switch mode¶
3 Devices are connected: Sender, Switch and Receiver.
3 Cases:
- Frame is preempted on Sender and Assembled on Switch Ingress Port.
- Frame is preempted on Switch Egress Port and Assembled on Receiver.
- Frame is preempted on Sender and Assembled on Switch Ingress Port, and also, frame is preempted on Switch Egress Port and Assembled on Receiver.
Devices Used:
- AM625-SK (As Switch/Sender)
- J7VCL (As Switch/Sender)
- AM64-SK (As Receiver)
3.2.2.8.3.2.2.4.4.1. CASE-1: Frame is preempted on Sender and Assembled on Switch Ingress Port¶
3.2.2.8.3.2.2.4.4.1.1. Preemption on AM625-SK (Sender) and Assembly on J7VCL (Switch) Ingress Port and sent to AM64-SK (Receiver)¶
Connect eth0 of AM625-SK to eth1 of J7VCL and eth0 of AM64-SK to eth2 of J7VCL.
Steps:
- On J7VCL, create and run the following script:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth1 up
ifconfig eth2 up
sleep 5
devlink dev param set platform/c000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth1 up
ip link set dev eth2 up
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 1 pvid untagged self
- On AM625-SK, create and run the following script:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
tc qdisc replace dev eth0 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth0
tc qdisc add dev eth0 clsact
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
ifconfig eth0 192.168.100.20 netmask 255.255.255.0
sleep 2
- On AM64-SK, run the following commands:
ifconfig eth0 192.168.100.30
iperf3 -s -i30 -p5002& \
iperf3 -s -i30 -p5003&
- Then, on AM625-SK, run the following commands:
iperf3 -c 192.168.100.30 -u -b200M -l1472 -u -t30 -i30 -p5002& \
iperf3 -c 192.168.100.30 -u -b50M -l1472 -u -t30 -i30 -p5003&
Results:
On AM625-SK (Sender):
root@am62xx-evm:~/IET# ethtool -S eth0 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 127395
tx_pri1_bcnt: 193357336
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth0 | grep 'tx_pri0'
p0_tx_pri0: 165
p0_tx_pri0_bcnt: 34444
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 509721
tx_pri0_bcnt: 773459795
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 128
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 114
On J7VCL (Switch):
root@j7200-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 108
iet_rx_smd_err: 1
iet_rx_frag: 114
iet_tx_hold: 0
iet_tx_frag: 0
3.2.2.8.3.2.2.4.4.1.2. Preemption on J7VCL (Sender) and Assembly on AM625-SK (Switch) Ingress Port and sent to AM64-SK (Receiver)¶
Connect eth1 of J7VCL to eth0 of AM625-SK and eth0 of AM64-SK to eth1 of AM625-SK.
Steps:
- On AM625-SK, create and run the following script:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
ifconfig eth1 up
sleep 5
devlink dev param set platform/8000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 up
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 1 pvid untagged self
- On J7VCL, create and run the following script:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth1 up
sleep 5
tc qdisc replace dev eth1 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth1
tc qdisc add dev eth1 clsact
tc filter add dev eth1 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
tc filter add dev eth1 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
ifconfig eth1 192.168.100.20 netmask 255.255.255.0
sleep 2
- On AM64-SK, run the following commands:
ifconfig eth0 192.168.100.30
iperf3 -s -i30 -p5002& \
iperf3 -s -i30 -p5003&
- Then, on J7VCL, run the following commands:
iperf3 -c 192.168.100.30 -u -b200M -l1472 -u -t30 -i30 -p5002& \
iperf3 -c 192.168.100.30 -u -b50M -l1472 -u -t30 -i30 -p5003&
Results:
On J7VCL (Sender):
root@j7200-evm:~/IET# ethtool -S eth1 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 127396
tx_pri1_bcnt: 193356005
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth1 | grep 'tx_pri0'
p0_tx_pri0: 76
p0_tx_pri0_bcnt: 14563
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 509604
tx_pri0_bcnt: 773435752
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 10
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 77331
On AM625-SK (Switch):
root@am62xx-evm:~/IET# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 11
iet_rx_assembly_ok: 20790
iet_rx_smd_err: 1092
iet_rx_frag: 77300
iet_tx_hold: 0
iet_tx_frag: 0
3.2.2.8.3.2.2.4.4.2. CASE-2: Frame is preempted on Switch Egress Port and Assembled on Receiver¶
Note
For the following tests, all interfaces which are a part of the test need to be a part of the same VLAN, since the switch needs to receive priority of the frames in order to perform preemption.
In addition to the Sender, the Switch’s Host Port also transmits traffic of lower priority to the receiver. This is done to ensure a higher chance of frame preemption and therefore frame fragmentation on the Switch’ Egress Port.
3.2.2.8.3.2.2.4.4.2.1. Highest priority frame sent by AM625-SK with preemption on J7VCL’s (Switch) Egress Port and Assembly on AM64-SK¶
Connect eth0 of AM625-SK to eth1 of J7VCL and eth0 of AM64-SK to eth2 of J7VCL.
Steps:
- Create and run the following script on J7VCL:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth2 tx 2
ethtool --set-priv-flags eth2 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth2 iet-frame-preemption on
ethtool --set-priv-flags eth2 iet-mac-verify on
ifconfig eth1 up
ifconfig eth2 up
sleep 5
tc qdisc replace dev eth2 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth2
devlink dev param set platform/c000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth1 up
ip link set dev eth2 up
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
sleep 2
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 100 pvid tagged self
bridge vlan add dev eth1 vid 100 master
bridge vlan add dev eth2 vid 100 master
sleep 2
ip link add link br0 name br0.100 type vlan id 100
ip link set br0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 2
tc qdisc add dev br0.100 clsact
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
sleep 2
- Create and run the following script on AM64-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
ip link add link eth0 name eth0.100 type vlan id 100
sleep 5
ifconfig eth0.100 192.168.100.30
iperf3 -s -i30 -p5001&
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
- Create and run the following script on AM625-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ifconfig eth0 up
sleep 5
ip link add link eth0 name eth0.100 type vlan id 100
ip link set eth0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 5
tc qdisc add dev eth0.100 clsact
tc filter add dev eth0.100 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
ifconfig eth0.100 192.168.100.20 netmask 255.255.255.0
sleep 2
- Run the following commands on J7VCL:
ifconfig br0.100 192.168.100.10
sleep 10
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5001&
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5002&
- Now, run the following command on AM625-SK:
iperf3 -c 192.168.100.30 -u -b50M -l1472 -t30 -i30 -p5003&
Results:
On J7VCL (Switch):
root@j7200-evm:~/IET# ethtool -S eth2 | grep 'tx_pri0'
p0_tx_pri0: 173
p0_tx_pri0_bcnt: 31039
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 85135
tx_pri0_bcnt: 129274224
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth2 | grep 'tx_pri2'
p0_tx_pri2: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri2_drop: 0
p0_tx_pri2_drop_bcnt: 0
tx_pri2: 84932
tx_pri2_bcnt: 129237975
tx_pri2_drop: 0
tx_pri2_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth2 | grep 'tx_pri3'
p0_tx_pri3: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri3_drop: 0
p0_tx_pri3_drop_bcnt: 0
tx_pri3: 3775
tx_pri3_bcnt: 5717026
tx_pri3_drop: 0
tx_pri3_drop_bcnt: 0
root@j7200-evm:~/IET# ethtool -S eth2 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 2
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 107
On AM64-SK (Receiver):
root@am64xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 1
iet_rx_assembly_ok: 94
iet_rx_smd_err: 72
iet_rx_frag: 106
iet_tx_hold: 0
iet_tx_frag: 0
3.2.2.8.3.2.2.4.4.2.2. Highest priority frame sent by J7VCL with preemption on AM625-SK’s (Switch) Egress Port and Assembly on AM64-SK¶
Connect eth1 of J7VCL to eth0 of AM625-SK and eth0 of AM64-SK to eth1 of AM625-SK.
Steps:
- On AM625-SK, create and run the following script:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth0 up
ifconfig eth1 up
sleep 5
tc qdisc replace dev eth1 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth1
devlink dev param set platform/8000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 up
sleep 2
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 100 pvid tagged self
bridge vlan add dev eth0 vid 100 master
bridge vlan add dev eth1 vid 100 master
sleep 2
ip link add link br0 name br0.100 type vlan id 100
ip link set br0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 2
tc qdisc add dev br0.100 clsact
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
sleep 2
- On AM64-SK, create and run the following script:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
ip link add link eth0 name eth0.100 type vlan id 100
sleep 5
ifconfig eth0.100 192.168.100.30
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
- On J7VCL, create and run the following script:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth1 up
sleep 5
tc qdisc replace dev eth1 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth1
ip link add link eth1 name eth1.100 type vlan id 100
ip link set eth1.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 5
tc qdisc add dev eth1.100 clsact
tc filter add dev eth1.100 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
ifconfig eth1.100 192.168.100.20 netmask 255.255.255.0
sleep 2
- Run the following commands on AM625-SK:
ifconfig br0.100 192.168.100.10
sleep 10
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5001& \
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5002&
- Now, on J7VCL, run the following command:
iperf3 -c 192.168.100.30 -u -b50M -l1472 -t30 -i30 -p5003&
Results:
On AM625-SK (Switch):
root@am62xx-evm:~/IET# ethtool -S eth1 | grep 'tx_pri0
p0_tx_pri0: 228
p0_tx_pri0_bcnt: 44010
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 792
tx_pri0_bcnt: 938162
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth1 | grep 'tx_pri2'
p0_tx_pri2: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri2_drop: 0
p0_tx_pri2_drop_bcnt: 0
tx_pri2: 706
tx_pri2_bcnt: 1047447
tx_pri2_drop: 0
tx_pri2_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth1 | grep 'tx_pri3'
p0_tx_pri3: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri3_drop: 0
p0_tx_pri3_drop_bcnt: 0
tx_pri3: 127393
tx_pri3_bcnt: 193865046
tx_pri3_drop: 0
tx_pri3_drop_bcnt: 0
root@am62xx-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 54
On AM64-SK (Receiver):
root@am64xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 23
iet_rx_smd_err: 120
iet_rx_frag: 54
iet_tx_hold: 0
iet_tx_frag: 0
3.2.2.8.3.2.2.4.4.3. CASE-3: Frame is preempted on both Sender and Switch Egress Port¶
Note
For the following tests, all interfaces which are a part of the test need to be a part of the same VLAN, since the switch needs to receive priority of the frames in order to perform preemption.
In addition to the Sender, the Switch’s Host Port also transmits traffic of lower priority to the receiver. This is done to ensure a higher chance of frame preemption and therefore frame fragmentation on the Switch’ Egress Port.
CASE-3 is the same as CASE-1 and CASE-2 combined.
3.2.2.8.3.2.2.4.4.3.1. Frame sent by AM625-SK with preemption on AM625-SK Egress Port and Assembled on J7VCL’s (Switch) Ingress Port followed by preemption on J7VCL’s (Switch) Egress Port and Assembled on AM64-SK¶
Connect eth0 of AM625-SK to eth1 of J7VCL and eth0 of AM64-SK to eth2 of J7VCL.
Steps:
- Create and run the following script on J7VCL:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ethtool -L eth2 tx 2
ethtool --set-priv-flags eth2 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth2 iet-frame-preemption on
ethtool --set-priv-flags eth2 iet-mac-verify on
ifconfig eth1 up
ifconfig eth2 up
sleep 5
tc qdisc replace dev eth2 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth2
devlink dev param set platform/c000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth1 up
ip link set dev eth2 up
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
sleep 2
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 100 pvid tagged self
bridge vlan add dev eth1 vid 100 master
bridge vlan add dev eth2 vid 100 master
sleep 2
ip link add link br0 name br0.100 type vlan id 100
ip link set br0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 2
tc qdisc add dev br0.100 clsact
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
sleep 2
- Create and run the following script on AM64-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
ip link add link eth0 name eth0.100 type vlan id 100
sleep 5
ifconfig eth0.100 192.168.100.30
iperf3 -s -i30 -p5001&
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
iperf3 -s -i30 -p5004&
iperf3 -s -i30 -p5005&
- Create and run the following script on AM625-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
ip link add link eth0 name eth0.100 type vlan id 100
ip link set eth0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 5
tc qdisc add dev eth0.100 clsact
tc filter add dev eth0.100 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 2
tc filter add dev eth0.100 egress protocol ip prio 1 u32 match ip dport 5004 0xffff action skbedit priority 3
ifconfig eth0.100 192.168.100.20 netmask 255.255.255.0
sleep 2
- Run the following commands on J7VCL:
ifconfig br0.100 192.168.100.10
sleep 10
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5001& \
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5002&
- Now, run the following commands on AM625-SK:
iperf3 -c 192.168.100.30 -u -b100M -l1472 -t30 -i30 -p5003& \
iperf3 -c 192.168.100.30 -u -b50M -l1472 -t30 -i30 -p5004& \
iperf3 -c 192.168.100.30 -u -b100M -l1472 -t30 -i30 -p5005&
Results:
On AM625-SK (Sender):
root@am62xx-evm:~/IET# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 63
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 4
On J7VCL (Switch):
root@j7200-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 4
iet_rx_smd_err: 1
iet_rx_frag: 4
iet_tx_hold: 0
iet_tx_frag: 0
root@j7200-evm:~/IET# ethtool -S eth2 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 1
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 127
On AM64-SK (Receiver):
root@am64xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 68
iet_rx_smd_err: 34
iet_rx_frag: 127
iet_tx_hold: 0
iet_tx_frag: 0
3.2.2.8.3.2.2.4.4.3.2. Frame sent by J7VCL with preemption on J7VCL Egress Port and Assembled on AM625-SK’s (Switch) Ingress Port followed by preemption on AM625-SK’s (Switch) Egress Port and Assembled on AM64-SK¶
Connect eth1 of J7VCL to eth0 of AM625-SK and eth0 of AM64-SK to eth1 of AM625-SK.
Steps:
- Create and run the following script on AM625-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth0 up
ifconfig eth1 up
sleep 5
tc qdisc replace dev eth1 handle 100: parent root mqprio \
num_tc 2 \
map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 \
hw 0
tc -g class show dev eth1
devlink dev param set platform/8000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 up
sleep 2
ip link set dev br0 type bridge vlan_filtering 1
bridge vlan add dev br0 vid 100 pvid tagged self
bridge vlan add dev eth0 vid 100 master
bridge vlan add dev eth1 vid 100 master
sleep 2
ip link add link br0 name br0.100 type vlan id 100
ip link set br0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 2
tc qdisc add dev br0.100 clsact
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
sleep 2
- Create and run the following script on AM64-SK:
#!/bin/sh
ifconfig eth0 down
ifconfig eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
ifconfig eth0 up
sleep 5
ip link add link eth0 name eth0.100 type vlan id 100
sleep 5
ifconfig eth0.100 192.168.100.30
iperf3 -s -i30 -p5001&
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
iperf3 -s -i30 -p5004&
iperf3 -s -i30 -p5005&
- Create and run the following script on J7VCL:
#!/bin/sh
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth1 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth1 iet-frame-preemption on
ethtool --set-priv-flags eth1 iet-mac-verify on
ifconfig eth1 up
sleep 5
ip link add link eth1 name eth1.100 type vlan id 100
ip link set eth1.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
sleep 5
tc qdisc add dev eth1.100 clsact
tc filter add dev eth1.100 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 2
tc filter add dev eth1.100 egress protocol ip prio 1 u32 match ip dport 5004 0xffff action skbedit priority 3
ifconfig eth1.100 192.168.100.20 netmask 255.255.255.0
sleep 2
- Run the following commands on AM625-SK:
ifconfig br0.100 192.168.100.10
sleep 10
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5001& \
iperf3 -c 192.168.100.30 -u -b100M -l1472 t30 -i30 -p5002&
- Now, run the following commands on J7VCL:
iperf3 -c 192.168.100.30 -u -b100M -l1472 -t30 -i30 -p5003& \
iperf3 -c 192.168.100.30 -u -b50M -l1472 -t30 -i30 -p5004& \
iperf3 -c 192.168.100.30 -u -b100M -l1472 -t30 -i30 -p5005&
Results:
On J7VCL (Sender):
root@j7200-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 55
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 220
On AM625-SK (Switch):
root@am62xx-evm:~/IET# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 106
iet_rx_smd_err: 4
iet_rx_frag: 220
iet_tx_hold: 0
iet_tx_frag: 0
root@am62xx-evm:~/IET# ethtool -S eth1 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 212
On AM64-SK (Receiver):
root@am64xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 148
iet_rx_smd_err: 109
iet_rx_frag: 212
iet_tx_hold: 0
iet_tx_frag: 0