3.3.3.24. MMCSD
3.3.3.24.1. Introduction
The multimedia card secure digital (MMCSD) host controller provides an interface between a local host (LH) such as a microprocessor unit (MPU) or digital signal processor (DSP) and either embedded multimedia card (eMMC), secure digital (SD), or secure digital input/output (SDIO) devices. The MMCSD host controller handles MMCSD and SDIO protocol with minimal LH intervention.
Main features of the MMCSD host controllers:
Full compliance with MMCSD command/response sets as defined in the Specification.
Support:
4-bit transfer mode specifications for SD and SDIO cards
8-bit transfer mode specifications for eMMC
Built-in 1024-byte buffer for read or write
32-bit-wide access bus to maximize bus throughput
Single interrupt line for multiple interrupt source events
Two slave DMA channels (1 for TX, 1 for RX)
Designed for low power and programmable clock generation
Maximum operating frequency of 48MHz
MMCSD card hot insertion and removal
The following image shows the MMCSD Driver Architecture:
3.3.3.24.2. References
3.3.3.24.3. Features
The SD driver supports the following features:
The driver is built in-kernel (part of vmlinux)
SD cards including SD High Speed and secure digital high capacity (SDHC) cards
Uses block bounce buffer to aggregate scattered blocks
3.3.3.24.4. Supported ultra high speed (UHS) modes
Platform |
SDR104 |
DDR50 |
SDR50 |
SDR25 |
SDR12 |
|---|---|---|---|---|---|
DRA74-EVM |
Y |
Y |
Y |
Y |
Y |
DRA72-EVM |
Y |
Y |
Y |
Y |
Y |
DRA71-EVM |
Y |
Y |
Y |
Y |
Y |
DRA72-EVM-REVC |
Y |
Y |
Y |
Y |
Y |
AM57XX-EVM |
N |
N |
N |
N |
N |
AM57XX-EVM-REVA3 |
N |
N |
N |
N |
N |
AM572X-IDK |
N |
N |
N |
N |
N |
AM571X-IDK |
N |
N |
N |
N |
N |
AM654-SR2-EVM |
Y |
Y |
Y |
Y |
Y |
Note
In AM654-SR1-EVM none of the UHS modes are supported.
Important Info: Certain UHS cards do not enumerate. The list of functional UHS cards is given in the following tables
FUNCTIONAL UHS CARDS |
|---|
ATP 32GB UHS CARD AF32GUD3 |
STRONTIUM NITRO 466x UHS CARD |
SANDISK EXTREME UHS CARD |
SANDISK ULTRA UHS CARD |
SAMSUNG EVO+ UHS CARD |
SAMSUNG EVO UHS CARD |
KINGSTON UHS CARD (DDR mode) |
TRANSCEND PREMIUM 400X UHS CARD (Non fatal error and then it re-enumerates in UHS mode) |
FUNCTIONAL (WITH LIMITED CAPABILITY) UHS CARD |
|---|
SONY UHS CARD - Voltage switching fails and enumerates in high speed |
GSKILL UHS CARD - Voltage switching fails and enumerates in high speed |
PATRIOT 8G UHS CARD - Voltage switching fails and enumerates in high speed |
Known Workaround: For cards that don’t enumerate in UHS mode, removing the PULLUP resistor in CLK line and changing the GPIO to PULLDOWN increases the frequency that the card enumerates in UHS modes.
Platform |
DDR |
HS200 |
|---|---|---|
DRA74-EVM |
Y |
Y |
DRA72-EVM |
Y |
Y |
DRA71-EVM |
Y |
Y |
DRA72-EVM-REVC |
Y |
Y |
AM57XX-EVM |
Y |
N |
AM57XX-EVM-REVA3 |
Y |
N |
AM572X-IDK |
Y |
N |
AM571X-IDK |
Y |
N |
AM654-SR2-EVM |
Y |
Y |
3.3.3.24.5. Driver configuration
The default kernel configuration enables support for MMCSD(built-in to kernel).
The selection of MMCSD/SDIO driver can be modified using the linux kernel configuration tool. Launch it by the following command:
$ make menuconfig ARCH=arm
Building into Kernel
Ensure that the following config options are set to ‘y’: * CONFIG_MMC * CONFIG_MMC_BLOCK * CONFIG_MMC_SDHCI * CONFIG_MMC_SDHCI_OMAP (for DRA7XX and AM57XX devices) * CONFIG_MMC_OMAP (for AM335X and AM437X devices)
Building as Loadable Kernel Module
Depending on your configuration, any of the above options can be set to ‘m’ to build them as a module. Use the following command to install all modules tp your filesystem.
$ sudo -E make modules_install ARCH=arm INSTALL_MOD_PATH=path/to/filesystem
Boot the kernel up-to kernel prompt and use modprobe to insert the driver module and all its dependencies.
$ modprobe sdhci-omap # for DRA7XX and AM57XX devices
$ modprobe omap_hsmmc # for AM335X and AM437X devices
If udev is running and the SD card is already inserted, the required modules will be loaded and any valid filesystem will be automatically mounted if they exist on the card.
Enabling eMMC Card Background operations support
eMMC cards need to occasionally spend some time cleaning up garbage and perform cache/buffer related operations. These are strictly on the card side and do not involve the host. They occur at one of the three levels based on the importance/severity of the operation:
Normal
Important
Critical
If an operation is delayed for too long, it becomes critical, taking priority over the regular read/write from host. This can cause host operations to be delayed or take more time than expected. To avoid such issues the multimedia card (MMC) HW and core driver provide a framework that can check for pending background operations and give the card some time to service them before they become critical. This feature is already part of the framework and to start using it the User needs to enable: EXT_CSD : BKOPS_EN [163] BIT 0.
This can be done using the “mmc-utils” tool from user space or using the “mmc” command in U-boot.
Command to enable bkops from userspace using mmc-utils, assuming eMMC instance to be mmcblk0
root@<machine>:mmc bkops enable /dev/mmcblk0
You can find the instance of eMMC by reading the ios timing spec from debug filesystem (debugfs):
root@<machine>:~# cat /sys/kernel/debug/mmc0/ios
----
timing spec: 9 (mmc HS200)
---
or by looking for boot partitions, eMMC has two boot partitions mmcblk<x>boot0 and mmcblk<x>boot1
root@<machine>:/# ls /dev/mmcblk*boot*
/dev/mmcblk0boot0 /dev/mmcblk0boot1
3.3.3.24.6. MMC support in Linux
There is no missing MMC support for AM57X devices device.
3.3.3.24.7. Steps for working around SD card issues in Linux
Steps for working around SD card issues in Linux documentation is pending for AM57X devices please reach out to: Help e2e for additional information.
3.3.3.24.8. Listing MMC devices from Linux
eMMC and SD cards register with the MMC subsystem and are available as a block device
as /dev/mmcblkn. To find the device index n corresponding to an eMMC device,
check which device includes mmcblknboot0 and mmcblknboot1. Here,
mmcblk0* is in eMMC.
root@<machine>:~# ls -l /dev/mmcblk*
brw-rw---- 1 root disk 179, 0 Jan 1 00:10 /dev/mmcblk0
brw-rw---- 1 root disk 179, 32 Jan 8 2025 /dev/mmcblk0boot0
brw-rw---- 1 root disk 179, 64 Jan 8 2025 /dev/mmcblk0boot1
brw-rw---- 1 root disk 179, 1 Jan 1 00:14 /dev/mmcblk0p1
crw------- 1 root root 239, 0 Jan 1 00:00 /dev/mmcblk0rpmb
brw-rw---- 1 root disk 179, 96 Jan 8 2025 /dev/mmcblk1
brw-rw---- 1 root disk 179, 97 Jan 1 00:00 /dev/mmcblk1p1
brw-rw---- 1 root disk 179, 98 Jan 8 2025 /dev/mmcblk1p2
The disk partitions for each MMC device are displayed as /dev/mmcblknpx.
To check existing or mounted disk partitions for an eMMC device, use the
command lsblk, such as:
root@<machine>:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
mmcblk0boot0 179:32 0 31.5M 1 disk
mmcblk0boot1 179:64 0 31.5M 1 disk
mmcblk1 179:96 0 14.8G 0 disk
|-mmcblk1p1 179:97 0 128M 0 part /run/media/boot-mmcblk1p1
`-mmcblk1p2 179:98 0 1.9G 0 part /
Use the mount and umount commands to mount and unmount formatted disk partitions, usually to virtual file allocation table (vfat) or fourth extended file system (ext4) types.
3.3.3.24.9. Create partitions in eMMC UDA
In eMMC, the user data area (UDA) HW partition is the primary storage space generally used
to flash the root filesystem (rootfs). To create disk partitions in UDA, use the fdisk command.
For ex: fdisk /dev/mmcblkn in which n is typically 0 or 1. In the previous example,
eMMC is fdisk /dev/mmcblk0.
For documentation on using fdisk command, go to: fdisk how-to.
Erase eMMC UDA
In Linux, before creating disk partitions, we can optionally erase eMMC UDA by using dd command:
root@<machine>:~# umount /dev/mmcblk0*
root@<machine>:~# dd if=/dev/zero of=/dev/mmcblk0 bs=1M count=n
where n should be determined according to the following formula: count = total size UDA (bytes) / bs.
3.3.3.24.9.1. Create “boot” partition
In this example create a “boot” partition of size 400 MiB which can be formatted to vfat type and will store the boot loader binaries.
root@<machine>:~# fdisk /dev/mmcblk0
Welcome to fdisk (util-linux 2.39.3).
Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.
Command (m for help): n
Partition type
p primary (0 primary, 0 extended, 4 free)
e extended (container for logical partitions)
Select (default p):
Using default response p.
Partition number (1-4, default 1):
First sector (2048-31080447, default 2048):
Last sector, +/-sectors or +/-size{K,M,G,T,P} (2048-31080447, default 31080447): +400M
Created a new partition 1 of type 'Linux' and of size 400 MiB.
Partition #1 contains a vfat signature.
Do you want to remove the signature? [Y]es/[N]o: y
The signature will be removed by a write command.
Command (m for help): a
Selected partition 1
The bootable flag on partition 1 is enabled now.
Command (m for help): t
Selected partition 1
Hex code or alias (type L to list all): c
Changed type of partition 'Linux' to 'W95 FAT32 (LBA)'.
Command (m for help): w
The partition table has been altered.
[ 644.818358] mmcblk0: p1
Calling ioctl() to re-read partition table.
Syncing disks.
Make sure bootable flag is set for “boot” partition, ROM might not boot from this partition if bootable flag is not set.
3.3.3.24.9.2. Create “root” partition
In this example create a “root” partition which can be formatted to ext4 type and will store Linux kernel Image, DTB, and the rootfs.
root@<machine>:~# fdisk /dev/mmcblk0
Welcome to fdisk (util-linux 2.39.3).
Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.
This disk is currently in use - repartitioning is probably a bad idea.
It's recommended to umount all file systems, and swapoff all swap
partitions on this disk.
Command (m for help): n
Partition type
p primary (1 primary, 0 extended, 3 free)
e extended (container for logical partitions)
Select (default p):
Using default response p.
Partition number (2-4, default 2):
First sector (821248-31080447, default 821248):
Last sector, +/-sectors or +/-size{K,M,G,T,P} (821248-31080447, default 31080447):
Created a new partition 2 of type 'Linux' and of size 14.4 GiB.
Command (m for help): t
Partition number (1,2, default 2): 2
Hex code or alias (type L to list all): 83
Changed type of partition 'Linux' to 'Linux'.
Command (m for help): w
The partition table has been altered.
Syncing disks.
3.3.3.24.10. Formatting eMMC partitions from Linux
After creating a partition/s, the partition can be formatted with the mkfs command.
For ex: mkfs -t ext4 /dev/mmcblkn where mmcblk{n} is the MMC device with the new
disk partitions to format. The general syntax for formatting disk partitions in Linux is:
mkfs.vfat [OPTIONS] TARGET [BLOCKS]
mkfs.ext4 [-c|-l filename] [-b block-size] [-C cluster-size]
3.3.3.24.10.1. Format to vfat
In this example, format the “boot” partition to type vfat.
root@<machine>:~# mkfs.vfat -F 32 -n "boot" /dev/mmcblk0p1
3.3.3.24.10.2. Format to ext4
In this example, format the “root” partition to type ext4.
root@<machine>:~# mkfs.ext4 -L "root" /dev/mmcblk0p2
Verify partitions
Verify setup of
mmcblk0p1andmmcblk0p2with lsblk command.root@<machine>:~# lsblk -o name,mountpoint,label,size,uuid NAME MOUNTPOINT LABEL SIZE UUID mmcblk0 14.8G |-mmcblk0p1 boot 400M E4D4-4879 `-mmcblk0p2 root 14.4G 74d40075-07e4-4bce-9401-6fccef68e934 mmcblk0boot0 31.5M mmcblk0boot1 31.5M mmcblk1 29.7G |-mmcblk1p1 /run/media/boot-mmcblk1p1 boot 128M 681F-55DD `-mmcblk1p2 / root 8.7G ead4c8bb-fa37-4c4d-9ba3-47a1f3824764
3.3.3.24.11. Flash eMMC for MMCSD boot
In this example, we show one simple method for flashing to eMMC for MMCSD boot from eMMC UDA in filesystem (FS) mode. Know this is not the only method for flashing the eMMC for this boot mode.
This example assumes the current boot mode is MMCSD boot from SD (FS mode)
3.3.3.24.11.1. Flash to eMMC “boot” partition
root@<machine>:~# umount /run/media/*
root@<machine>:~# mkdir /mnt/eboot /mnt/sdboot
root@<machine>:~# mount /dev/mmcblk0p1 /mnt/eboot
root@<machine>:~# mount /dev/mmcblk1p1 /mnt/sdboot
Verify the partitions are mounted to the correct folders by using lsblk command in the
column labeled MOUNTPOINTS.
root@<machine>:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
|-mmcblk0p1 179:1 0 400M 0 part /mnt/eboot
`-mmcblk0p2 179:2 0 14.4G 0 part
mmcblk0boot0 179:32 0 31.5M 1 disk
mmcblk0boot1 179:64 0 31.5M 1 disk
mmcblk1 179:96 0 29.7G 0 disk
|-mmcblk1p1 179:97 0 128M 0 part /mnt/sdboot
`-mmcblk1p2 179:98 0 8.7G 0 part /
Now we can copy boot loader binaries to eMMC and umount the partitions when writes finish.
root@<machine>:~# ls /mnt/sdboot/
tiboot3.bin tispl.bin u-boot.img uEnv.txt
root@<machine>:~# cp /mnt/sdboot/* /mnt/eboot/
root@<machine>:~# sync && umount /mnt/*
3.3.3.24.11.2. Flash to eMMC “root” partition
root@<machine>:~# umount /run/media/*
root@<machine>:~# mkdir /mnt/eroot /mnt/sdroot
root@<machine>:~# mount /dev/mmcblk0p2 /mnt/eroot
[69229.982452] EXT4-fs (mmcblk0p2): mounted filesystem 74d40075-07e4-4bce-9401-6fccef68e934 r/w with ordered data mode. Quota mode: none.
root@<machine>:~# mount /dev/mmcblk1p2 /mnt/sdroot
Verify the partitions are mounted to the correct folders by using lsblk command in the
column labeled MOUNTPOINTS.
root@<machine>:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
|-mmcblk0p1 179:1 0 400M 0 part
`-mmcblk0p2 179:2 0 14.4G 0 part /mnt/eroot
mmcblk0boot0 179:32 0 31.5M 1 disk
mmcblk0boot1 179:64 0 31.5M 1 disk
mmcblk1 179:96 0 29.7G 0 disk
|-mmcblk1p1 179:97 0 128M 0 part
`-mmcblk1p2 179:98 0 8.7G 0 part /mnt/sdroot
/
Now we can copy rootfs to eMMC (either from SD rootfs or from tar file) and umount the partitions when writes finish.
From SD
root@<machine>:~# ls /mnt/sdroot
bin dev home lost+found mnt proc run srv tmp var
boot etc lib media opt root sbin sys usr
root@<machine>:~# cp -r -a /mnt/sdroot/* /mnt/eroot
root@<machine>:~# sync
root@<machine>:~# umount /mnt/*
[70154.205154] EXT4-fs (mmcblk0p2): unmounting filesystem 74d40075-07e4-4bce-9401-6fccef68e934.
From tar file
This sections requires for tisdk-base-image-<soc>evm.rootfs.tar.xz to have been previously copied to the SD card rootfs.
root@<machine>:~# ls
tisdk-base-image-<soc>-evm.rootfs.tar.xz
root@<machine>:~# tar -xpf tisdk-base-image-<soc>-evm.rootfs.tar.xz -C /mnt/eroot
root@<machine>:~# sync
root@<machine>:~# umount /mnt/*