Processor SDK Linux for AM57X Logo
11_01
  • 1. Overview
  • 2. Release Specific
  • 3. Foundational Components
  • 4. Industrial Protocols
  • 5. Examples and Demos
  • 6. How to Guides
    • 6.1. Host
    • 6.2. Target
    • 6.3. Hardware EVM Setup
    • 6.4. Linux Porting Guide for AM571x/AM570x Speed Grades
Processor SDK Linux for AM57X
  • 6. How to Guides
  • Edit on GitHub

6. How to Guides

  • 6.1. Host
    • 6.1.1. How to Build a Ubuntu Linux host under VMware
    • 6.1.2. Connect to an EVM via Telnet
    • 6.1.3. How to Setup a Samba Server
    • 6.1.4. Boot Sequence
    • 6.1.5. Moving Files to the Target System
    • 6.1.6. How to Flash from U-boot Shell
    • 6.1.7. Customizing the SDK Splash Screen
    • 6.1.8. How to Develop with 3D Graphics
    • 6.1.9. How to Develop accelerated Multimedia using GStreamer on AM57xx
    • 6.1.10. Preventing BeagleBone board reset on JTAG Connect
    • 6.1.11. Processor SDK IPC Quick Start Guide
    • 6.1.12. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux
  • 6.2. Target
    • 6.2.1. SDK File System Optimization/Customization
      • 6.2.1.1. The Basics of OPKG
        • 6.2.1.1.1. List all available options of opkg
        • 6.2.1.1.2. Show all installed packages
        • 6.2.1.1.3. Show package contents
        • 6.2.1.1.4. Find a file owner
        • 6.2.1.1.5. Show packages which require the package as dependency
        • 6.2.1.1.6. Removing Packages or Deinstallation
        • 6.2.1.1.7. Install local packages
    • 6.2.2. How to add a JVM
    • 6.2.3. Update U-Boot Environment Variables stored in SPI Flash from Linux
    • 6.2.4. How to change dtb files
    • 6.2.5. How to Set Display for AM572x GP EVM
    • 6.2.6. How to Fix Y2K38 Issue
      • 6.2.6.1. What is the Y2K38 Issue?
      • 6.2.6.2. Building a Y2K38-friendly Image
  • 6.3. Hardware EVM Setup
    • 6.3.1. AM572x GP EVM Hardware Setup
    • 6.3.2. TMDXIDK5728 Hardware Setup
  • 6.4. Linux Porting Guide for AM571x/AM570x Speed Grades
Previous Next

© Copyright 1995-2025 Texas Instruments Incorporated, CC-BY-SA-4.0. Revision 255eaaca. Last updated on Oct 28, 2025.